Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
Next revision
Previous revision
resources:eval:ad9208-3000ebz [09 Jul 2018 15:11]
Amrutha_Anantha [Preface]
resources:eval:ad9208-3000ebz [25 Jul 2018 14:48]
UmeshJ [Preface]
Line 15: Line 15:
 | <fc #​9400d3>​AD9689-2000EBZ</​fc> ​   | <fc #​9400d3>​Evaluation board for AD9689-2000</​fc> ​    | <fc #​9400d3>​9689CE02C</​fc> ​    | | <fc #​9400d3>​AD9689-2000EBZ</​fc> ​   | <fc #​9400d3>​Evaluation board for AD9689-2000</​fc> ​    | <fc #​9400d3>​9689CE02C</​fc> ​    |
    
-Note: ADS8-V1 does not support lane rates below 2Gbps. Hence, the following modes will not give a valid FFT.+Note: The FPGA image in ADS8-V1 does not support lane rates below 2Gbps. Hence, the following modes will not give a valid FFT. All modes listed below use a 3GHz sample clock.
   LMF=411 and LMF=412 for a decimation ratio of 8   LMF=411 and LMF=412 for a decimation ratio of 8
   LMF=811 and LMF=812 for a decimation ratio of 4   LMF=811 and LMF=812 for a decimation ratio of 4
Line 54: Line 54:
   * [[>​resources/​tools-software/​ace>​|ACE]] (Analysis | Control | Evaluation) ​   * [[>​resources/​tools-software/​ace>​|ACE]] (Analysis | Control | Evaluation) ​
 ====== Design and Integration Files ====== ====== Design and Integration Files ======
-  * {{:​resources:​eval:​ad9208_3000ebz_files.zip|Schematic,​ Gerber layout and BOM}}+  * {{ :​resources:​eval:​ad9208_3000ebz_files.zip |Schematic, Gerber layout and BOM}} 
 +  ​
 //Note : The AD9208-3000EBZ,​ AD9689-2600EBZ and the AD9689-2000EBZ use the same design files. The only difference is in the ADC choice// //Note : The AD9208-3000EBZ,​ AD9689-2600EBZ and the AD9689-2000EBZ use the same design files. The only difference is in the ADC choice//
 ====== Equipment Needed ====== ====== Equipment Needed ======
resources/eval/ad9208-3000ebz.txt · Last modified: 25 Jul 2018 14:48 by UmeshJ