This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:ad9083 [22 Mar 2021 16:35] – added trigger section Alex Arrants | resources:eval:ad9083 [05 Jan 2022 16:45] (current) – change Gerber layout files to layout files Brigid Duggan | ||
---|---|---|---|
Line 26: | Line 26: | ||
===== Board Design and Integration Files ===== | ===== Board Design and Integration Files ===== | ||
* {{: | * {{: | ||
- | * {{: | + | * {{: |
* {{: | * {{: | ||
Line 224: | Line 224: | ||
//Figure 9. AD9083EBZ Precision Time Domain Mode Typical FFT // | //Figure 9. AD9083EBZ Precision Time Domain Mode Typical FFT // | ||
===== External Trigger ===== | ===== External Trigger ===== | ||
- | SMA connector J2 on the ADS8v3 | + | SMA connector J2 on the ADS8v3 |
To enable the external trigger: | To enable the external trigger: | ||
Line 231: | Line 231: | ||
2. Click on the " | 2. Click on the " | ||
- | {{: | + | {{: |
3. Click on the " | 3. Click on the " | ||
+ | {{: | ||
4. Click "Apply Changes" | 4. Click "Apply Changes" | ||
Line 239: | Line 241: | ||
SMA connector J3 is normally used as a system ready indicator. It indicates that the FPGA is ready to accept an external trigger. | SMA connector J3 is normally used as a system ready indicator. It indicates that the FPGA is ready to accept an external trigger. | ||
+ | To capture data, click on "Run Once" as normal. Capture will begin once 1.8V is detected on connector J2 of the ADS8v3. | ||
===== Troubleshooting Notes ===== | ===== Troubleshooting Notes ===== |