This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:ad9083 [22 Mar 2021 21:18] – [External Trigger] Alex Arrants | resources:eval:ad9083 [05 Jan 2022 16:45] (current) – change Gerber layout files to layout files Brigid Duggan | ||
---|---|---|---|
Line 26: | Line 26: | ||
===== Board Design and Integration Files ===== | ===== Board Design and Integration Files ===== | ||
* {{: | * {{: | ||
- | * {{: | + | * {{: |
* {{: | * {{: | ||
Line 224: | Line 224: | ||
//Figure 9. AD9083EBZ Precision Time Domain Mode Typical FFT // | //Figure 9. AD9083EBZ Precision Time Domain Mode Typical FFT // | ||
===== External Trigger ===== | ===== External Trigger ===== | ||
- | SMA connector J2 on the ADS8v3 can used as an optional trigger so that the data capture start time can be controlled. The trigger requires | + | SMA connector J2 on the ADS8v3 can be used as an optional trigger so that the data capture start time can be controlled. The trigger requires |
To enable the external trigger: | To enable the external trigger: | ||
Line 235: | Line 235: | ||
3. Click on the " | 3. Click on the " | ||
{{: | {{: | ||
+ | |||
4. Click "Apply Changes" | 4. Click "Apply Changes" | ||
{{: | {{: |