This is an old revision of the document!
EVALUATING THE AD6674 IF DIVERSITY RECEIVER
Preface
This user guide describes the AD6674 evaluation board AD6674-1000EBZ which provides all of the support circuitry required to operate the ADC in its various modes and configurations. The application software used to interface with the devices is also described. The user guide wiki applies to the follow evaluation boards:
Evaluation Board Part Number | Description | Board Revision |
AD6674-1000EBZ | Evaluation board for AD6674-1000; Full Bandwidth | 9680CE04B |
AD6674-750EBZ | Evaluation board for AD6674-750; Full Bandwidth | 9680CE04B |
AD6674-500EBZ | Evaluation board for AD6674-500; Full Bandwidth | 9680CE04B |
AD6674-LF1000EBZ | Evaluation board for AD6674-1000; up to 1GHz Input Bandwidth | 9680CE02B |
AD6674-LF750EBZ | Evaluation board for AD6674-750; up to 1GHz Input Bandwidth | 9680CE02B |
AD6674-LF500EBZ | Evaluation board for AD6674-500; up to 1GHz Input Bandwidth | 9680CE02B |
The AD6674 data sheet provides additional information and should be consulted when using the evaluation board. All documents and software tools are available at www.analog.com/hsadcevalboard. For additional information or questions, send an email to highspeed.converters@analog.com.
AD6674 Evaluation Board
Figure 1. AD6674 Evaluation Board for full 2GHz Input Bandwidth
Figure 2. AD6674 Low Frequency Evaluation Board up to 1GHz Input Bandwidth
Figure 3 below compares the bandwidth available on the AD6674 normal evaluation boards and the “LF” boards
Figure 3. Comparison of Bandwidth on the Normal and the “LF” boards
Typical Measurement Setup
Features
Helpful Documents
Software Needed
Design and Integration Files
Equipment Needed
Getting Started
This section provides quick start procedures for using the evaluation board for AD6674.
Configuring the Board
Before using the software for testing, configure the evaluation board as follows:
-
Connect one 12V, 6.5A switching power supply (such as the CENB1080A1251F01 supplied) to P4 on the
ADS7-V2EBZ/
ADS7-V1EBZ board. Connect the Standard-B
USB port of the
ADS7-V2EBZ/
ADS7-V1EBZ board to the PC with the supplied
USB cable.
-
-
If the Device Manager does not show the
ADS7-V2EBZ/
ADS7-V1EBZ listed, unplug all
USB devices from the PC, uninstall and re-install SPIController and VisualAnalog and restart the hardware setup from step 1.
On the ADC evaluation board, provide a clean, low jitter 1GHz clock source to connector J801 and set the amplitude to 14dBm. This is the ADC Sample Clock.
On the ADC evaluation board, provide a clean, low jitter clock source to connector J804 and set the amplitude to 10dBm. This is the Reference Clock for the gigabit transceivers in the FPGA. The REFCLK frequency can be calculated using the following empirical formulae:
bps/lane, where
(Default Nprime = 16)
On the ADC evaluation board, use a clean signal generator with low phase noise to provide an input signal for channel A to P200. Use a shielded, RG-58, 50 Ω coaxial cable to connect the signal generator output to the ADC Evaluation Board. For best results, use a narrow-band, band-pass filter with 50 Ω terminations and an appropriate center frequency. (
ADI uses TTE, Allen Avionics, and
K & L band-pass filters.)
On the ADC evaluation board, use a clean signal generator with low phase noise to provide an input signal for channel B to P202. Use a shielded, RG-58, 50 Ω coaxial cable to connect the signal generator output to the ADC Evaluation Board. For best results, use a narrow-band, band-pass filter with 50 Ω terminations and an appropriate center frequency. (
ADI uses TTE, Allen Avionics, and
K & L band-pass filters.)
Visual Analog Setup
Click Start
All Programs
Analog Devices
VisualAnalog
VisualAnalog
On the VisualAnalog “New Canvas” window, click
ADCDualAD6674
Figure 5. Selecting the AD6674 canvas
At this point, VisualAnalog will automatically detect the evaluation board and the FPGA data capture board and ask if it can program the FPGA with the appropriate bin file. This is shown in figure 6.
If VisualAnalog opens with a collapsed view, click on the “Expand Display” icon (see figure 5)
Figure 7. Expanding Display in VA
Click the
Settings button in the
ADC Data Capture block as shown in Figure 8
Figure 8. Changing the ADC Capture Settings
On the
General tab make sure the clock frequency is set to
1000MHz (or other clock frequency). The FFT capture length may be changed to 131072 (128k) or 262144 (256k) per channel. The ADS7-V2 and ADS7-V1 FPGA software supports up to 2M FFT capture (1M per channel)
Figure 9. Setting the clock frequency and Capture length
If the board did not Auto-program click on the Capture Board tab and browse to the ad9680_ads7v1.bin file. Click the Program button. The FPGA_DONE LED should illuminate on the ADS7-V1 board indicating that the FPGA has been correctly programmed.
On the Device tab. Make sure that Enable Alternate REFCLK option is unchecked.
Click OK
SPIController Setup
Click Start
All Programs
Analog Devices
SPIController
SPIController
Select the appropriate configuration file when prompted.
In the
Global tab, under the
Generic Read/Write section, write 0x81 to register 0x000. This issues a Soft reset for the DUT.
Figure 10. Sending a Soft Reset to the AD6674
The JESD204B quick configuration and Lane Rate registers are available in the
ADCBase3 tab. Set the Lane Rate setting register 0x56E to
Low Lane Rate Mode
Figure 11. Setting the JESD204B Lane Rate
Set the JESD204B Quick Configuration register 0x570. For 1000MSPS operation with with default conditions (
Noise Shaped Requantizer (NSR) Mode), the values for
L.M.F are
4.2.1
Figure 12. Setting the JESD204B Quick Configuration Register
After the quick configuration setting is completed, the
PLL Lock Detect register 0x56F will read 0x80 to denote a lock. The SPIController interface will show a “1” to denote a lock.
Toggle the JESD204B link by checking and then unchecking the JESD204B Serial Transmit Power Down box
Individual Channel control for
ADC A and
ADC B are done using the Device Index Register (0x008) in the Global tab.
Figure 13. Device Index for ADC Channel A and Channel B
Under ADC A and ADC B tabs the options for Channel A and B are listed. Default settings have been programmed to ensure optimal performance for the input bandwidth and sample rate. Only the following options need to be operated with:
Chip Configuration Register (2): This option allows the channel to be powered on
Buffer Current Setting (18): This option allows the buffer current to change to enable better harmonic performance at different frequencies. At high analog input frequencies, the buffer current may need to be increased to optimize harmonic distortion performance (HD2, HD3). Keep in mind that at high frequencies, the performance is also jitter limited. So increasing the buffer currents may lead to diminishing returns with higher power consumption. Refer to the datasheet to understand the relationship between IAVDD3 and Buffer Current Setting.
Analog Input Differential Termination (16): This sets the input termination. Recommended settings are 500, 200, 100, 50 ohms. At lower termination settings, the harmonic distortion performance may show improvement, but the analog input signal amplitude will be reduced.
Input Full Scale Range (25): At high input frequencies, in order to preserve the linearity of the input buffer, it may be beneficial to reduce the input full-scale range in order to get more harmonic distortion performance. This in turn may negatively affect the SNR of the ADC.
Device Setup - NSR Mode
The default Chip Application Mode for the AD6674-750/AD6674-1000 is NSR with a chip decimation ratio of 2 (the AD6674-500 also defaults to NSR mode but with decimation disabled).
Figure 14. Default Application Mode - NSR/Decimation by 2
The NSR mode settings are configured in the ADCA and ADCB tabs. The NSR defaults to 21% bandwidth mode with a tuning word of 0. Decimate by 2 is enabled by default also on the AD6674-750 and AD6674-1000 (and cannot be disabled in NSR mode).
Figure 15. Channel A and Channel B NSR Settings
Obtaining an FFT - NSR Mode
The first item to configure in Visual Analog is the input clock frequency. This is the frequency of the input clock and NOT the decimated sample rate (if using decimation). Click in the ADC Data Capture block to open the settings. In this example, 750MHz is the input clock frequency.
Figure 16. AD6674-750 FFT Data Capture Settings
In order to obtain an FFT with NSR enabled, Visual Analog must be configured correctly. Click on the settings button on the FFT Analysis block and configure the settings in Visual Analog to match the NSR settings that have been programmed into the AD6674. Under Advanced Calculation, click the Enable box, select AD6674 NSR, and then select the appropriate bandwidth mode and tuning word. Make sure to set the Bandwidth to match the mode. When finished, click the Apply button and then the OK button to apply the settings.
Figure 17. AD6674-750 FFT Analysis NSR Settings
In this example, with an input clock of 750MHz, the output sample rate is 375MSPS. The default JESD204B lane configuration is 4.2.1 (L.
M.F). The required REFCLK frequency is 187.5MHz (refer to step 7 in the section “Configuring the Board”).
Click the Run button in Visual Analog and you should see the capture data similar to the plot below.
Figure 18. AD6674-750 FFT with NSR Enabled
Adjust the amplitude of the input signal so that the fundamental is at the desired level. (Examine the
Fund Power reading in the left panel of the VisualAnalog FFT window.) NSR imposes a ~3dB loss in the signal, but does not impact the dynamic range. A -1.0
dBFS input signal will show as -4.0
dBFS in the FFT in Visual Analog.
To save the FFT plot do the following
Click on the Float Form button in the FFT window
Figure 19. Floating the FFT window
Click on File
Save Form As button and save it to a location of choice
Figure 20. Saving the FFT
Device Setup - VDR Mode
The default Chip Application Mode for the AD6674-750/AD6674-1000 is NSR with a chip decimation ratio of 2 (the AD6674-500 also defaults to NSR mode but with decimation disabled). The settings in the ADCBase0 tab must be changed to configure the AD6674 into VDR mode. To set up the AD6674 for VDR mode change the Chip Application Mode in register 0x200 to Variable Dynamic Range (VDR) Mode and set the Chip Decimation Ratio in register 0x201 to Full Sample Rate.
Figure 21. Set Application Mode to VDR
The VDR mode tuning word can be configured in the ADC A and ADC B tabs. VDR defaults to 25% bandwidth complex mode with a tuning word of 0. The tuning word can be changed using the VDR Tuner Frequency selection (register 0x434). See the AD6674 data sheet for more details on the available bandwidth modes and tuning words.
Figure 22. Channel A and Channel B VDR Settings
Using the default lane configuration in the AD6674 (L.
M.F = 4.2.1) the JESD204B lane rate will be 7.5
Gbps which means the
PLL must be set to Maximum Lane Rate Mode (0x56E) int he ADCBase3 tab in SPIController.
Figure 23. PLL Encode Settings
Obtaining an FFT - VDR Mode
The first item to configure in Visual Analog is the input clock frequency. This is the frequency of the input clock and NOT the decimated sample rate (if using decimation). Click in the ADC Data Capture block to open the settings. In this example, 750MHz is the input clock frequency.
Figure 24. AD6674-750 FFT Data Capture Settings
In this example, with an input clock of 750MHz, the output sample rate is 750MSPS. The default JESD204B lane configuration is 4.2.1 (L.
M.F). The required REFCLK frequency is 375MHz (refer to step 7 in the section “Configuring the Board”).
Click the Run button in Visual Analog and you should see the capture data similar to the plot below.
Figure 25. AD6674-750 FFT with VDR Enabled
Adjust the amplitude of the input signal so that the fundamental is at the desired level. (Examine the
Fund Power reading in the left panel of the VisualAnalog FFT window.) VDR imposes no loss on the input signal so a -1.0
dBFS input signal will show as -1.0
dBFS in the FFT in Visual Analog.
To save the FFT plot do the following
Click on the Float Form button in the FFT window
Figure 26. Floating the FFT window
Click on File
Save Form As button and save it to a location of choice
Figure 27. Saving the FFT
Setting up SPIController to Use Control Bits as VDR Punish Bits and the VDR High/Low Resolution Bit - VDR Mode
The first step go to the ADCBase2 tab in SPIController to set up the control bits to select the VDR indicator bits. In this example Control Bit 2 is set to VDR Punish Bit 1, Control Bit 1 is set to VDR Punish Bit 0, and Control Bit 0 is set to the VDR High/Low resolution bit.
Figure 28. SPIController ADCBase2 Settings for VDR Indicators in the Control Bits
Next go to the ADCBase4 tab to set up the control bits to select the VDR indicator bits. In this example three control bits are sent per sample. In order to accommodate three control bits, the converter resolution (N) must be set to 13 bits (there are 16 available bits in the JESD204B data word and if three are used for control bits there are 13 bits available for the converter sample - in this example this means there will only be 13 bits available instead of the 14 bits of converter resolution.
Figure 29. SPIController ADCBase4 Settings for Enabling the Control Bits
Viewing the VDR Punish Bits and the VDR High/Low Resolution Bit - VDR Mode
The first step is to open a new Logic canvas in VisualAnalog. In the Logic canvas configure the Input Formatter to set the Resolution to 16 bits and the Alignment to 18 bits. This will create the space such that all three control bits can be visible in the Logic canvas.
Figure 30. Input Formatter Settings for VDR Indicators in the Control Bits
Next configure the Logic Analysis block for the data alignement. Set the High Bit to 15 and the low bit to 0. This will align the canvas such that all three control bits can be visible in the Logic canvas.
Figure 31. Logic Analysis Settings for Bit Alignment
These settings will create the space in the Logic Canvas display so that all three control bits available in the JESD204B data stream will be visible.
Figure 32. Logic Canvas Display Showing Available Control Bits
Once a signal is input that will trigger VDR to operate the VDR punish bits [1:0] and the VDR High/Low resolution bit can be seen in the Logic Canvas display. In this case control bit 2 is VDR punish bit 1, control bit 1 is VDR punish bit 0, and control bit 0 is the VDR High/Low resolution bit.
Figure 33. Logic Canvas Display Showing Control Bits [2:0] Indicating VDR Status
Note that the data alignment from the FPGA to VisualAnalog will fill in the control bits starting from the
LSB location in the Logic Canvas display. In this example data bit two is control bit 2, data bit 1 is control bit 1, and data bit 0 is control bit 0. If only using control bit 2 then this would reside in the data bit 0 location in the Logic Canvas display.
Figure 34. Logic Canvas Display Showing Control Bit 2 Only
Device Setup - 2 ADCs, 2DDCs, Real Mode Decimate by 2
The default Chip Application Mode for the AD6674-750/AD6674-1000 is NSR with a chip decimation ratio of 2 (the AD6674-500 also defaults to NSR mode but with decimation disabled). The settings in the ADCBase0 tab must be changed to configure the AD6674 to use the DDCs. In this example the AD6674 is set up to use two DDCs (one per ADC channel) with real outputs and a decimation ratio of two. Set the Chip Application Mode in register 0x200 to Two Digital Down Converters and select the Only Real (I) Selected checkbox. Set the Chip Decimation Ratio in register 0x201 to Decimate by 2 Ratio.
Figure 35. Set Application Mode to 2 DDCs Real Mode Decimate by 2
The DDC settings must be configured in ADCBase1, but first, the tuning step, translation frequency, and DDC Phase Increment must be calculated.
The tuning step is equal to the output sample rate divided by 4096.
tuning step = 375MSPS/4096 = 91552.734375
The translation frequency is equal to the output sample rate divided by 4*(decimation ratio).
translation frequency = 375MSPS/(4*2) = 46875000
The DDC Phase Increment is equal to the translation frequency divided by the tuning step.
DDC Phase Increment = 46875000/91552.734375 = 512
Under DDCO CTRL and DDC1 CTRL in the ADCBase1 tab configure the DDCs to select 6dB Gain, Variable IF Mode, Real(I) Decimate by 2 Filter Selection, Both Input Sample Selections to Channel A for DDC0 and Channel B for DDC1, and the DDC Phase Increment to the calculated value of 512
After changing DDC selections, perform a soft reset of the DDCs by checking and unchecking the box for DDC Soft Reset under the DDC Synchronization CTRL Reg (300).
Figure 36. Channel A and Channel B DDC Settings
Using the default lane configuration in the AD6674 (L.
M.F = 4.2.1) the JESD204B lane rate will be 3.75Gbps which means that the
PLL needs to be set to Low Lane Rate Mode (0x56E) in the ADCBase3 tab in SPIController. This is the default setting so no change is needed.
Obtaining an FFT - 2 ADCs, 2DDCs, Real Mode Decimate by 2
1. The first item to configure in Visual Analog is the input clock frequency. This is the frequency of the input clock and NOT the decimated sample rate (if using decimation). Click in the ADC Data Capture block to open the settings. In this example, 750MHz is the input clock frequency. In addition, the DDC data must be selected under the Output Data section. DDC0 and DDC1 are being used in the AD6674 so this must be selected under the ADC Data Capture Settings.
Figure 37. AD6674-750 FFT Data Capture Settings
In this example, with an input clock of 750MHz, the output sample rate is 375MSPS. The default JESD204B lane configuration is 4.2.1 (L.
M.F). The required REFCLK frequency is 187.5MHz (refer to step 7 in the section “Configuring the Board”).
Click the Run button in Visual Analog and you should see the capture data similar to the plot below.
Figure 38. AD6674-750 FFT with 2 DDCs in Real Mode with Dec2 Enabled
Adjust the amplitude of the input signal so that the fundamental is at the desired level. (Examine the
Fund Power reading in the left panel of the VisualAnalog FFT window.) Real DDC operation imposes ~0.7
dB loss on the input signal but does not impact the dynamic range. A -1.0
dBFS input signal will show as -1.7
dBFS in the FFT in Visual Analog.
To save the FFT plot do the following
Click on the Float Form button in the FFT window
Figure 39. Floating the FFT window
Click on File
Save Form As button and save it to a location of choice
Figure 40. Saving the FFT
Device Setup - 2 ADCs, 1DDC, Complex ZIF Mode Decimate by 2
The default Chip Application Mode for the AD6674 is Noise Shaped Requantizer (NSR) Mode with the Chip Decimation Ratio of 2 (decimation is disabled on the AD6674-500). The settings in the ADCBase0 tab must be changed to configure the AD6674 to use the DDC. In this example the AD6674 will be set up to use one DDCs with a complex ZIF output (NCO bypassed) and a decimation ration of two. Set the Chip Application Mode in register 0x200 to One Digital Down Converter and make sure the Only Real (I) Selected checkbox is
NOT checked. Set the Chip Decimation Ratio in register 0x201 to Decimate by 2 Ratio.
Figure 41. Set Application Mode to 1 DDC Complex ZIF Mode Decimate by 2
The DDC settings must be configured under DDCO CTRL in the ADCBase1 tab configure the DDC to select Complex Mixer Selection, 0 Hz IF Mode, Decimate by 2 Filter Selection, Real (I) Input Sample Selection to Channel A for DDC0, and Complex (Q) Input Sample Selection to Channel B.
After changing DDC selections, perform a soft reset of the DDCs by checking and unchecking the box for DDC Soft Reset under the DDC Synchronization CTRL Reg (300).
Figure 42. DDC Settings for Complex ZIF Mode
Using the default lane configuration in the AD6674 (L.
M.F = 4.2.1) the JESD204B lane rate will be 3.75Gbps which means that the
PLL needs to be set to Low Lane Rate Mode (0x56E) in the ADCBase3 tab in SPIController. This is the default setting so no change is needed.
Obtaining an FFT - 2 ADCs, 1DDC, Complex ZIF Mode Decimate by 2
The first item to configure in Visual Analog is the input clock frequency. This is the frequency of the input clock and NOT the decimated sample rate (if using decimation). Click in the ADC Data Capture block to open the settings. In this example, 750MHz is the input clock frequency. In addition, the DDC data must be selected under the Output Data section. DDC0 is being used in the AD6674 so this must be selected under the ADC Data Capture Settings.
Figure 43. AD6674-750 FFT Data Capture Settings
In this example, with an input clock of 750MHz, the output sample rate is 750MSPS. The default JESD204B lane configuration is 4.2.1 (L.
M.F). The output sample rate is 375MSPS and the required REFCLK frequency is 187.5MHz (refer to step 7 in the section “Configuring the Board”).
In order to exclude the image frequency from the SFDR measurements, configure Visual Analog to remove the image from its calculations. This is done under the FFT Analysis settings. Under the User-Defined tab add a new row by clicking Add. Name it ‘Image’. Use a symbol such as the # and set the Freq to ‘-fund’. Set the Single-Side Band to 3 Bins and set it as ‘Spur, Exclude’. Once done, select the row, and then hit the Move Up button to place this new row just below the row with Fund.
Figure 44. AD6674-750 FFT Analysis Settings for Complex Image
Click the Run button in Visual Analog and you should see the capture data similar to the plot below.
Figure 45. AD6674-750 FFT with 1 DDC in Complex ZIF Mode with Dec2 Enabled
Adjust the amplitude of the input signal so that the fundamental is at the desired level. (Examine the “Fund Power” reading in the left panel of the VisualAnalog FFT window.) Complex DDC operation imposes ~1dB loss in the signal, but does not impact the dynamic range. A -1dBFS input signal will show as -2dBFS in Visual Analog.
To save the FFT plot do the following
Click on the Float Form button in the FFT window
Figure 46. Floating the FFT window
Click on File
Save Form As button and save it to a location of choice
Figure 47. Saving the FFT
Troubleshooting Tips
FFT plot appears abnormal
If you see a normal noise floor when you disconnect the signal generator from the analog input, be sure you are not overdriving the ADC. Reduce input level if necessary.
In VisualAnalog, Click on the Settings button in the Input Formatter block. Check that Number Format is set to the correct encoding (twos compliment by default). Repeat for the other channel.
Issue a
Data Path Soft Reset through SPIController
Global tab as shown in Figure 46
Figure 48. Issuing a data path soft reset through SPIController
The FFT plot appears normal, but performance is poor.
Make sure you are using the appropriate band-pass filter on the analog input.
Make sure the signal generators for the clock and the analog input are clean (low phase noise).
If you are using non-coherent sampling, change the analog input frequency slightly, or use coherent frequencies.
Make sure the
SPI config file matches the product being evaluated.
The FFT window remains blank after the Run button is clicked
Make sure the evaluation board is securely connected to the ADS7-V1.
Make sure the FPGA has been programmed by verifying that the
Config DONE LED is illuminated on the ADS7-V1. If this LED is not illuminated reprogram the FPGA through VisualAnalog. If the LED still does not illuminate disconnect the
USB and power cord for 15 seconds. Connect again and repeat the ADS7-V1 setup process.
Make sure the correct FPGA bin file was used to program the FPGA.
Be sure that the correct sample rate is programmed. Click on the
Settings button in the
ADC Data Capture block in VisualAnalog, and verify that the
Clock Frequency is properly set.
Figure 49. Setting the correct clock frequeency in VisualAnalog
Ensure that the REFCLOCK is ON and set to the appropriate frequency.
Restart SPIController.
VisualAnalog indicates that the “FIFO capture timed out” or “FIFO not ready for read back”
VisualAnalog displays a blank FFT when the RUN button is clicked
Ensure that the clock to the ADC is supplied. Using SPIController
ADCBase0 tab the status of the clock can be read out.
Figure 50. Clock Detection Status Register
Ensure that the ADC's
PLL is locked by checking the status of the
PLL lock detect register 0x56F. This can be done using SPIController.