Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
resources:eval:ad6674-1000ebz [17 Nov 2022 03:22]
John Xavier Toledo [Visual Analog Setup]
resources:eval:ad6674-1000ebz [17 Nov 2022 03:24] (current)
John Xavier Toledo [Troubleshooting Tips]
Line 182: Line 182:
  
 ** The FFT window remains blank after the Run button is clicked ** ** The FFT window remains blank after the Run button is clicked **
-  * Make sure the evaluation board is securely connected to the ADS7-V1+  * Make sure the evaluation board is securely connected to the [[adi>​eval-ads7-v1|ADS7-V1EBZ]]
-  * Make sure the FPGA has been programmed by verifying that the **Config DONE** LED is illuminated on the ADS7-V1.  If this LED is not illuminated reprogram the FPGA through VisualAnalog. If the LED still does not illuminate disconnect the USB and power cord for 15 seconds. Connect again and repeat the ADS7-V1 setup process.+  * Make sure the FPGA has been programmed by verifying that the **Config DONE** LED is illuminated on the [[adi>​eval-ads7-v1|ADS7-V1EBZ]].  If this LED is not illuminated reprogram the FPGA through VisualAnalog. If the LED still does not illuminate disconnect the USB and power cord for 15 seconds. Connect again and repeat the [[adi>​eval-ads7-v1|ADS7-V1EBZ]] ​setup process.
   * Make sure the correct FPGA //bin// file was used to program the FPGA.   * Make sure the correct FPGA //bin// file was used to program the FPGA.
-  * Be sure that the correct sample rate is programmed. Click on the **Settings** button in the **ADC Data Capture** block in VisualAnalog,​ and verify that the **Clock Frequency** is properly set.{{ :​resources:​eval:​ad6674_capture_settings.png?​nolink |}}<WRAP centeralign>//​Figure 49. Setting the correct clock frequeency ​in VisualAnalog//</​WRAP>​+  * Be sure that the correct sample rate is programmed. Click on the **Settings** button in the **ADC Data Capture** block in VisualAnalog,​ and verify that the **Clock Frequency** is properly set.{{ :​resources:​eval:​ad6674_capture_settings.png?​nolink |}}<WRAP centeralign>//​Figure 49. Setting the correct clock frequency ​in VisualAnalog//</​WRAP>​
   * Ensure that the REFCLOCK is ON and set to the appropriate frequency.   * Ensure that the REFCLOCK is ON and set to the appropriate frequency.
   * Restart SPIController.   * Restart SPIController.
resources/eval/ad6674-1000ebz.txt · Last modified: 17 Nov 2022 03:24 by John Xavier Toledo