Wiki

This version is outdated by a newer approved version.DiffThis version (09 Sep 2022 17:14) was approved by Padraic O Reilly.The Previously approved version (09 Sep 2022 10:14) is available.Diff

This is an old revision of the document!


AD4630/AD4030 Evaluation Board User Guide

General Description

The EVAL-AD4630-24FMCZ, EVAL-AD4030-24FMCZ & EVAL-AD4630-16FMCZ evaluation boards enable quick and easy evaluation of the AD4X3X family of 24-bit & 16-bit precision successive approximation register (SAR) analog-to-digital converters (ADCs).
The AD4630-24 & AD4630-16 are 2MSPS per channel, low power, dual channel 24-bit or 16-bit SAR ADCs while the AD4030-24 is a single channel 24-bit precision SAR ADC that supports up to 2 MSPS per channel. The evaluation boards demonstrates the performance of either the AD4630-24, AD4030-24 or AD4630-16 and provides a configurable analog front end (AFE) for a variety of system applications.
The evaluations board are designed for use with the Digilent ZedBoard. The ZedBoard is used to control data capture and buffering. The evaluation board connects to the ZedBoard board via a field-programmable gate array (FPGA) mezzanine card (FMC) low pin count (LPC) connector. The ZedBoard hosts a Xilinx Zynq7000 SoC, which has two processor cores and programmable FPGA fabric. The ZedBoard connects to the PC through USB.
The evaluation board includes:

  • A high precision buffered band gap 5 volt reference (LTC6655).
  • An analog front end (AFE) that provides signal conditioning and drive for the AD4630-24, AD4030-24 & AD4630-16. The AFE can be configured to use either the ADA4896-2 in a dual buffer configuration, or the ADA4945-1, a fully differential amplifier.
  • An optional 100 MHz clock source that provides a reference clock for the FPGA and ADC.
  • Full power supply solution that provides all the necessary voltage rails from a 12 volt supply that is provided from the ZedBoard through the FMC connector.

Full descriptions of these products are available in their respective data sheets, which should be consulted when using the evaluation board.

Features

  • On-board voltage reference, clock source, and ADC drivers
  • Versatile analog signal conditioning circuitry
  • FMC-LPC system board connector
  • ACE PC software for configuration and data analysis (time and frequency domain)
  • Compatible with other off-the-shelf controller boards

Evaluation Board Kit Contents

  • EVAL-AD4630-24FMCZ, EVAL-AD4030-24FMCZ or EVAL-AD4630-16FMCZ evaluation board
  • Micro-SD memory card (with adapter) containing system board boot software and Linux OS
  • Optional - ZedBoard (system controller board )

Equipment Needed

  • PC with Windows 7 or Windows 10 operating system
  • Digilent ZedBoard with 12 V wall adapter power supply
  • Precision signal source
  • SMA Cable(s) (input to evaluation board)
  • Recommended - Band-pass filter centered on test signal frequency.

Quick Start Guide

To avoid potential issues, ensure the VADJ SELECT = 2.5V.

Getting Started

  • Download and install the ACE Software tool from the ACE download page. If ACE is already installed, make sure you have the latest version by using the ‘Check For Updates’ option in the ACE sidebar.

When selecting components to install, please ensure that the 'LibIIO Wrapper' in the 'Precision Converter Components' section is enabled.

The installer can also be run from within ACE by clicking the link found in the 'IIIO Resources' section found in the Help » Application Resources section.

  • Run ACE and select ‘Plug-in Manager’ from the ACE sidebar to install the board plug-in that supports the Product Evaluation Board and select Available Packages. You can use the search field to help filter the list of boards to find the relevant one. An ACE Quickstart guide is available here: ACE Quickstart - Using ACE and Installing Plug-ins

  • Insert the EVAL-SD-KUIPERZ SD card into the SD card slot on the underside of the ZedBoard.

If there is a need to re-image or create a new SD card, instructions are available here: ADI Kuiper Linux with support for ACE Evaluation.

  • Ensure the ZedBoard boot configuration jumpers are set to use the SD card as shown.

To avoid potential damage, ensure the VADJ SELECT jumper is set to the correct voltage for the Product Evaluation Board.

  • Connect the Product Evaluation Board to the FMC connector on the ZedBoard.

There may be additional steps and hardware required for a given Product Evaluation Board, for example, function generators connections and setup. This information may be included with the eval kit or in the User guide for the corresponding Product Evaluation Boards page that can be found by searching Product Evaluation Boards and Kits.

  • Connect the USB cable from the PC to the J13/USB OTG port and the PSU to J20/DC input.

  • Slide SW8/POWER switch to the ON position. The green LD13/POWER LED should turn on, followed by the blue LD12/DONE LED.
  • The red LD7 LED should start blinking ~20-30 seconds later which indicates the boot process is complete.
  • Launch the ACE software from the Analog Devices folder in the Windows Start menu. The Evaluation Board should appear in the ACE Start Tab » Attached Hardware view.

03 Jun 2022 22:08 · Michael Bradley

Evaluation Board Hardware


Figure 1. EVAL-AD4630-XXFMCZ Evaluation System


Figure 2a. EVAL-AD4030-24FMCZ



Figure 2b. EVAL-AD4630-24FMCZ


Figure 2c. EVAL-AD4630-16FMCZ

Setting Up the Evaluation Board

Figure 1 illustrates the evaluation system components. To use the system, connect the evaluation board to the ZedBoard, connect a micro-USB cable to the USB OTG port, apply power to the ZedBoard, open the ACE GUI, and supply an input stimulus to one or both ADC channels.

Each ADC channel has dedicated SMA connectors that support either a singled-ended or differential input. The signals on these inputs are injected to the configurable AFE (see the Analog Front End section below for more details). The digital interface to the system controller board uses level shifters to translate between the VIO supply of the AD4630-16 and the I/O voltage of the Zynq 7000 on the ZedBoard. By default, the evaluation board is powered from the system controller board 12V supply through the FMC connector. The Power Supplies section contains a list of optional on-board connections that can be used to connect external supplies and references to the board.

Power Supplies

The primary 12 volt supply to the EVAL-AD4X30-XXFMCZ comes from the ZedBoard through the FMC connector. 12 volts is regulated down to an intermediate voltage with a switcher and then is post regulated down to the various voltage rails. 12 volts is also used to generate the negative rails for the buffers and final drive amplifiers.

Each of the voltage rails are brought out to turrets so they can be easily measured (see Figure 1). A bench supply can be used to drive these turrets to supply the evaluation board manually. This is useful if a current measurement is required. Each supply is decoupled where it enters the board and at each device. A single ground plane is used on this board to minimize the effect of high frequency interference. The voltage ranges listed in the table below represent the expected ranges for the board. If the user desires to connect external supplies to the board, the amplifier data sheets and the AD4630-24 datasheet, AD4030-24 datasheet or AD4630-16 datasheet should be consulted to ensure that the external supply values comply with the device requirements.

Power Supply Function Min. (V) Max. (V)
+12V 12 volt primary supply via FMC connector N/A N/A
GND Ground connection N/A N/A
+3.3V 3.3 volts for various digital logic 3.26 3.33
+1.8V 1.8 volts for the ADC 1.77 1.81
VIO 1.8 volt supply for the ADC digital I/O 1.8 1.87
+5V 5 volts for the ADC 5.26 5.4
REFIN 5 volt ADC reference input 4.95 5.05
VAMP+ Positive supply for the amplifiers 5.36 5.47
VAMP- Negative supply for the amplifiers -3.5 -3.28
VP1 5.7 volts at the input of the switcher 5.45 5.75
REF 5 volts at the ADC reference output 4.95 5.05
EN 1.8 volts enable signal for the power supplies 1.75 1.85

Table 1. On-Board Power Supplies

Reference Circuit

By default, the on-board LT6655 provides a 5 V reference to the AD4630-24, AD4030-24 & AD4630-16. It drives the REFIN pin of the ADC through an R-C filter (R=100Ω, C=1μF) that reduces the low frequency noise. The REFIN pin is connected to an internal buffer, eliminating the need for an external buffer. However, if the user desires to use an external reference that drives the internal buffer, it can be attached the EXT REF SMA connector (see figure below). R137 should be populated with a zero ohm resistor, and R136 should be open. The internal buffer can be bypassed by attaching an external reference to the REF turret on the board. To reduce the ADC power consumption, the internal reference buffer can be disabled (see respective products data sheet).


Figure 3. EVAL-AD4X30-XXFMCZ Reference circuit (AD4630-24 shown. Configuration applies to all parts)

Clock Circuit

The ZedBoard uses a 100MHz reference clock to generate its internal clocks as well as the sample clock for the AD4630-24, AD4030-24 or AD4630-16. To simplify system operation an on-board 100MHz, low-jitter crystal oscillator (XO) on the EVAL-AD4X30-XXFMCZ board supplies this clock as the default configuration, as shown in the figure below. To use an external clock source, remove R55 and connect an external clock source to J1, the CLK IN SMA. The external clock frequency must be < 100 MHz. The user should take care to use a low jitter clock source to achieve best system performance. The external clock level should be 10 to 12 dBm.


Figure 4. EVAL-AD4X30-XXFMCZ clock circuit (AD4630-24 shown. Configuration applies to all parts)

Analog Front End

The EVAL-AD4X30-XXFMCZ has a flexible driver network that can be configured for a variety topologies. The default network is shown in Figure 5, in which the ADA4945-1 fully differential amplifier is driving the ADC. It can accommodate both single-ended and differential signal sources, and drives the ADC differentially. As populated, it has a unity gain. When using a single-ended source, the unused input should be terminated with the equivalent source impedance. Note: As implemented, the AD4945-1 driver on the evaluation board preserves the differential value of IN+ - IN- (with appropriate gain scaling applied), but inverts the signal polarity that is injected to the ADC. Hence, if a positive DC signal is applied to the input, it should be attached to IN_A/B-, and likewise, a negative DC signal should be attached to IN_A/B+ to preserve the signal polarity.


Figure 5. Differential Driver AFE (default) (AD4630-24 shown. Configuration applies to all parts)

Function: Single ended to differential via differential amplifier
Comments: Best distortion
Required changes from default configuration: No changes required

Table 2. EVAL-AD4620-16FMCZ Default AFE Configuration

A second topology can be seen in Figure 6. This topology consists of a pair of unity gain buffers, the ADA4896-2. It also can be driven by either a singled-ended or differential source. This network is ideal for observing the best noise performance of the AD4630-16, due to the low voltage and current noise of the ADA4896-2 (1 nV/rtHz and 2.8 pA/rtHz, respectively). It also offers a common mode input impedance of 10 MΩ and a wide input common mode voltage range of -4.9V to +4.1V (when using +/- 5V supplies). Note: This driver circuit also inverts the polarity of the input signal. To preserve polarity when measuring DC voltages, connect a positive voltage to IN_A/B-. Likewise, a negative DC voltage should be connected to IN_A/B+.


Figure 6. Dual Buffer AFE (AD4630-24 shown. Configuration applies to all parts)

Function: Differential input using buffer amplifiers
Comments: Best noise & relaxed drive requirement for signal source
Required changes from default configuration: Remove: R10, R12,R119, R120, R121 & R122 (Ch. A); R20, R22, R123, R124, R125 & R126 (Ch. B). Install: R31, R33, R47, & R49 (Ch. A); R60, R62, R75 & R78 (Ch. B)

Table 3. Unity Gain Dual Buffer Configuration

Figure 7 shows a driver network which combines the ADA4896-2 with the ADA4945-1. This circuit is ideal for applications that require a high input impedance along with gain to maximize the input range of the ADC. The gain of the ADA4945-1 can modified by changing either the feedback resistors or input resistors.


Figure 7. High Impedance Buffer with Gain AFE (AD4630-24 shown. Configuration applies to all parts)

Function: High impedance input with gain
Comments: Relaxed drive requirements from signal source plus signal scaling.
Required changes from default configuration: Remove:R120, R121 (Ch. A);R124, R125 (Ch. B). Install: R31, R127, R28, R47, R128 & R43 (Ch. A); R60, R129, R57, R78, R130 & R72 (Ch. B)

Table 4. High Impedance with Gain Configuration

Figure 8 shows an input configuration that allows the AD4630-16 to be directly driven from the SMA connectors. This enables testing with alternative driver configurations mounted on an external PCB.


Figure 8. Direct Driven Inputs (AD4630-24 shown. Configuration applies to all parts)

Function: Direct input path
Comments: Supports evaluation with an alternative driver
Required changes from default configuration: Remove: R10, R12, R119 & R122 (Ch A); R20, R22, R123, R126 (Ch B). Install: R28, R29, R120, R121, R43 & R44 (Ch A); R124, R57, R58, R125, R72 & R73 (Ch B)

Table 5. Direct Drive Configuration

Controller Board

The ZedBoard, which is the system controller board, enables the configuration of the ADC and capture of data from the evaluation board by the PC via USB (or Ethernet). The AD4X30-XX family of parts support a multi-lane serial port interface (SPI) for each data converter channel. The SPI interface for each channel is connected to the ZedBoard via the FMC connector (P1). The ZedBoard™ functions as the communication link between the PC and connected evaluation board. It buffers samples captured from the evaluation board in its DDR3 memory. The ZedBoard board requires power from a 12 volt wall adapter (included with the ZedBoard). It hosts a Xilinx® ZYNQ® 7020 SoC, which contains two ARM® Cortex-A9 Processors and a Series-7 FPGA with 85k Programmable Logic cells. A Linux OS runs on the host processor system. It communicates with the PC through either a USB 2.0 high speed port or a 10/100/1000 Ethernet port. The default software configuration uses USB.

Evaluation Software

GETTING STARTED

The ACE evaluation software controls and configures the evaluation board through the ZedBoard.

SOFTWARE INSTALLATION PROCEDURES

Before connecting the evaluation board to the ZedBoard, take the following steps to set up the AD4630-24, AD4030-24 or AD4630-16 for initial use in the ACE evaluation software:

1. Download the ACE evaluation software package from the ACE software page to start the ACE evaluation software installation.

2. Click on Download ACE Installer to download the file.

3. Run the installer and follow the instructions to complete the software installation process.

During the installation process, be sure to select Precision Converter Components when prompted and enable the LibIIO Wrapper to ensure that all necessary software components are installed.

The LibIIO Wrapper must be installed for ACE to detect the connected hardware. If you need to install the LibIIO Wrapper after ACE has been installed, click the 'Help' button in the main ACE window. In the 'ACE Help' panel that appears expand the 'Application Resources' section, and you will find a link to run a local copy of the LibIIO Wrapper Installer.



Figure 9. Select Precision Converter Components during the ACE installation

When the following prompt appears, be sure to select LibIIO and LibIIODrivers options, then click Install.


Figure 10. Select LibIIO components during ACE installation

EVALUATION HARDWARE SETUP

When the ACE evaluation software installation is complete, take the following steps to set up the ZedBoard and the evaluation board together:

1. Insert the SD card provided with the evaluation board into J12 on the ZedBoard

2. Connect the Evaluation board to the FMC connector of the ZedBoard.

3. Connect the provided power supplies to J20 on the ZedBoard.

4. Connect the USB cable to the USB OTG (J13) on the ZedBoard and to the computer

5. Connect the desired input signal to the appropriate input on the evaluation board (J2-J5)

6. Move SW8 to the ON position to start the ZedBoard

7. Start the ACE evaluation software (see the Software Operation section).

SOFTWARE OPERATION

To start the ACE evaluation software, from the Windows Start menu, click Analog Devices > ACE. The software window opens (see Figure 11) until the software recognizes the AD4630-24, AD4030-24 or AD4630-16 evaluation board. When the software recognizes the board, double-click on the icon in the Start view to open the main window seen in Figure 12. For more detailed information about ACE, refer to the ACE user guide: Analysis | Control | Evaluation - ACE Software

Figure 11. Select Interface Window

MAIN WINDOW

Figure 12. ACE Evaluation Software Main Window

In the main ACE evaluation software window (see Figure 12), the AD4630-16 can be configured. Various settings for the AD4630-24, AD4030-24 or AD4630-16 are available in this window, including the number of SPI data lanes (lane mode), clock mode, data rate, and data mode (sample format).

Lane Mode

Select the number of SPI lanes to use to transmit the data. The options are 1, 2, or 4 lanes per channel.

Clock Mode

Selects between the echo clock mode and the SPI clock mode.

Date Rate

Selects between single data rate (SDR: 1-bit per clock cycle) or dual data rate (DDR: 2-bits per clock cycle). DDR is only available when using Echo clock mode or Master clock mode. Note: The current Linux driver and HDL do not support Master clock mode.

Data Mode

Selects the data output format of the AD4630-24, AD4030-24 or AD4630-16. The available formats are: 24-bit differential data with 8 bit common mode (AD4630-24 & AD4030-24), 24-bit differential data (AD4630-24 & AD4030-24) or 16 bit differential data (AD4630-16), 16-bit differential data and 8 bit common mode, 30-bit averaged data, or a 32-bit programmable test pattern.

Apply Operating mode and reboot

Changes to the operating parameters listed above requires a reboot of the ZedBoard. By clicking Apply Operating mode and reboot, the ACE software will configure the part and load the correct FPGA image. It will also automatically reset the ZedBoard. The specific steps include:

1. After changing any of the operating parameters, click “Apply Operating mode and reboot”.

2. Close any of the following ACE windows that may be open:

  • Analysis
  • AD4630IIO
  • AD4630IIO Board
  • Start
  • System - In this tab, close the subsystem box that contains the components shown in the following figure.


Figure 13. Subsystem view

3. Click on the “Home” icon in the upper portion of the left pane. The AD4630 plug-in should appear. If not, it may be necessary to click Refresh Attached Hardware
4. Double-click on the part plug-in to open the board view and start using the available evaluation functions.

Chip View

Figure 14. Chip View

By clicking on the part in the main ACE evaluation software window (see Figure 12), the chip view will be opened (Figure 14). Settings for the part available in this window include enabling and configuring averaging mode, changing the sample frequency, and changing the gain and offset for each channel. Refer to the data sheet for a detailed explanation of these features.

Operating mode

Selects between normal operating mode and low power mode.

Sample Averaging

Sets the number of samples to be used by the internal block averaging filter of the part. Select OFF to disable averaging, or select the desired number of samples to be averaged by the part. Ensure that the Data Mode is set to 30-bit averaged data when using this feature.

Sampling Frequency

Selects the desired sample frequency from a drop down menu. Note that this is the frequency of the pulse that is applied to the CNV pin. The sampling frequency can be scaled by changing the frequency of the reference clock (see the Clock Circuit section). The sampling rate selected from the menu can be scaled by applying a lower frequency external clock. The effective sampling rate is: selected sampling frequency x fEXT/100 MHz.
If the block averaging filter is enabled, the effective output sample rate is the sampling frequency divided by the selected block average size.

Hardware Gain

This sets the internal digital gain applied to the differential data. The gain can be adjusted independently for each channel.

Offset

This sets the internal digital offset that is applied to the differential data. The offset can be independently set for each channel.

REGISTER MAP

Figure 15. Register Map

By clicking on Proceed to Memory Map in the lower right corner of the Chip view (see Figure 12), the AD4630 register map view will be opened (figure 15). In this view all registers can be read and selected registers can be modified. Changes to the register contents can be written to the part by clicking Apply Changes. Under normal operation no changes are necessary to the register map. Registers that change the operating mode should not be changed in this view.

ANALYSIS VIEW

Figure 16. Analysis View

By clicking on Proceed to Analysis in the lower right corner of the Chip view (see Figure 12), the Analysis view will open (Figure 16). In the CAPTURE pane the desired capture block size is entered in the Sample Count text box. At the bottom of the CAPTURE pane, select Run Once to capture a single block, or select Run Continuously to enable continuous updates. Data will be collected and plotted as a time domain waveform (Figure 17), an FFT (Figure 18), or a histogram (Figure 19) by selecting the desired view on the left side of the CAPTURE pane. The RESULTS pane displays parametric values for the selected display format. The user can pan and zoom on the plot area. Various data sets can be selected in the top right corner of the plot area. The bottom of the RESULTS pane also has buttons that allow the user to import or export sample data.

Figure 17. Time domain waveform

Figure 18. FFT view

Figure 19. Histogram view

System Operational Constraints

Sampling Frequency

The following table illustrates the maximum sampling rates that can be achieved based on the device configuration. Note that the FPGA SPI engine only supports Zone 2 data transfers from the AD4630/AD4030.

Table 3. Maximum sampling rate by device configuration

Clocking Mode Lane Mode (per channel) Data Rate Data format Max sampling rate
SPI 1 Single (SDR) 32-bit 1.75 MSPS (note 1)
SDR 24-bit 2 MSPS
Dual (DDR) 32 or 24-bit 2 MSPS
2 SDR or DDR 32 or 24-bit 2 MSPS
4 SDR or DDR 32 or 24-bit 2 MSPS
Echo Clock 1 SDR 32-bit 1.75 MSPS (note 1)
SDR 24-bit 2 MSPS
DDR 32 or 24-bit 2 MSPS
2 SDR or DDR 32 or 24-bit 2 MSPS
4 SDR or DDR 32 or 24-bit 2 MSPS

Note 1: The sampling rate in Single lane, 32-bit output formats in SDR mode are limited by the FPGA SPI engine. This is not a limitation of the AD4630/AD4030 device.

Software Developers Guide

Analog Devices supports the development of custom applications using the EVAL-AD4X30-XX system and are described in the AD463x and AD403x Developer's Guide

Visit AD463x and AD403x Developer's Guide for an overview of the additional software drivers that are provided with the evaluation system

Evaluation Board Support and Troubleshooting

Technical Support

Technical support for the evaluation board hardware and software can be obtained by posting a question to ADI's EngineerZone technical support community for precision ADCs.

The evaluation board schematic and other board files can be found on the EVAL-AD4630-16FMCZ, EVAL-AD4630-24FMCZ & EVAL-AD0630-24FMCZ web pages.

Troubleshooting

A troubleshooting guide can be found at: Troubleshooting Guide for ADI Kuiper Linux for ACE Evaluation. The latter covers some tips related to ZedBoard startup and the SD card containing the Kuiper Linux image.

resources/eval/ad4630-24-eval-board.1662736463.txt.gz · Last modified: 09 Sep 2022 17:14 by Padraic O Reilly