This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:eval:10-lead-pulsar-adc-evaluation-board [11 Jan 2021 08:37] – Fixed bad link for Evaluation Board Software version 1.1 Ioana Chelaru | resources:eval:10-lead-pulsar-adc-evaluation-board [14 Jan 2021 05:11] (current) – user interwiki links Robin Getz | ||
---|---|---|---|
Line 47: | Line 47: | ||
PMOD compatible hardware is a very simple board which plugs directly into microprocessor and FPGA boards which have PMOD peripherals. | PMOD compatible hardware is a very simple board which plugs directly into microprocessor and FPGA boards which have PMOD peripherals. | ||
- | Complete details about the PulSAR ADC PMOD boards can be found by visiting our [[https:// | + | Complete details about the PulSAR ADC PMOD boards can be found by visiting our [[/ |
- SOFTWARE NOTE: If using the PMOD compatible version of the hardware, please install this version of the software. | - SOFTWARE NOTE: If using the PMOD compatible version of the hardware, please install this version of the software. | ||
- | - HARDWARE NOTE: If using the PMOD compatible version of the hardware, you will need to use the PMOD to SDP interposer board to fully evaluate the system. | + | - HARDWARE NOTE: If using the PMOD compatible version of the hardware, you will need to use the PMOD to SDP interposer board to fully evaluate the system. |
{{ : | {{ : |