Differences
This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |
resources:demo:reference-designs:demo-ad5758-ao8z:introduction [15 Aug 2019 12:33] – [Introduction] Donal O''Sullivan | resources:demo:reference-designs:demo-ad5758-ao8z:introduction [29 Dec 2020 23:03] (current) – fix links Robin Getz |
---|
//Figure 1 - Block diagram of a single channel// | //Figure 1 - Block diagram of a single channel// |
| |
This Board is a demonstration a system level solution where the [[adi>http://www.analog.com/ad5758|AD5758]] and the [[adi>http://www.analog.com/adp1031|ADP1031]] can be used together to implement a compact, eight channel, channel-to-channel isolated, precision analog output (AO) module, while achieving less than 2 W worst case power dissipation over a wide range of operating conditions. | This Board is a demonstration a system level solution where the [[adi>AD5758]] and the [[adi>ADP1031]] can be used together to implement a compact, eight channel, channel-to-channel isolated, precision analog output (AO) module, while achieving less than 2 W worst case power dissipation over a wide range of operating conditions. |
| |
The [[adi>http://www.analog.com/adp1031|ADP1031]] solves the isolation and size challenges and the [[adi>http://www.analog.com/ad5758|AD5758]] provides a low power dissipation, precision, configurable current or voltage output channel. | The [[adi>ADP1031]] solves the isolation and size challenges and the [[adi>AD5758]] provides a low power dissipation, precision, configurable current or voltage output channel. |
| |
This board uses the [[adi>http://www.analog.com/aducm3029|ADUCM3029]] as the system controller to control each channel independently. | This board uses the [[adi>ADUCM3029]] as the system controller to control each channel independently. |
| |
{{:resources:demo:reference-designs:demo-ad5758-ao8z:gui:block_diagram.png|}}\\ | {{:resources:demo:reference-designs:demo-ad5758-ao8z:gui:block_diagram.png|}}\\ |