Both sides previous revisionPrevious revision | Last revisionBoth sides next revision |
resources:demo:reference-designs:demo-ad5758-ao8z:introduction [07 Aug 2019 15:31] – corrected spelling. valerie hamilton | resources:demo:reference-designs:demo-ad5758-ao8z:introduction [15 Aug 2019 12:33] – [Introduction] Donal O''Sullivan |
---|
When designing channel-to-channel isolated analog output modules for process control applications such as programmable logic controller (PLC) or distributed control system (DCS) modules, the main trade-off usually considered is //power dissipation// vs. //channel density//. As module sizes shrink, and channel density increases, the power dissipation budget per channel must decrease to accommodate the maximum power dissipation budget for the module. Higher channel density also means that there is less PCB real estate available for each channel. | When designing channel-to-channel isolated analog output modules for process control applications such as programmable logic controller (PLC) or distributed control system (DCS) modules, the main trade-off usually considered is //power dissipation// vs. //channel density//. As module sizes shrink, and channel density increases, the power dissipation budget per channel must decrease to accommodate the maximum power dissipation budget for the module. Higher channel density also means that there is less PCB real estate available for each channel. |
| |
{{:resources:demo:reference-designs:demo-ad5758-ao8z:01-08-2019_14-52-59.png|}} | {{:resources:demo:reference-designs:demo-ad5758-ao8z:01-08-2019_14-52-59.png|}}\\ |
| //Figure 1 - Block diagram of a single channel// |
This Board is a demonstration a system level solution where the [[adi>http://www.analog.com/ad5758|AD5758]] and the [[adi>http://www.analog.com/adp1031|ADP1031]] can be used together to implement a compact, eight channel, channel-to-channel isolated, precision analog output (AO) module, while achieving less than 2 W worst case power dissipation over a wide range of operating conditions. | This Board is a demonstration a system level solution where the [[adi>http://www.analog.com/ad5758|AD5758]] and the [[adi>http://www.analog.com/adp1031|ADP1031]] can be used together to implement a compact, eight channel, channel-to-channel isolated, precision analog output (AO) module, while achieving less than 2 W worst case power dissipation over a wide range of operating conditions. |
| |
| |
This board uses the [[adi>http://www.analog.com/aducm3029|ADUCM3029]] as the system controller to control each channel independently. | This board uses the [[adi>http://www.analog.com/aducm3029|ADUCM3029]] as the system controller to control each channel independently. |
| |
| {{:resources:demo:reference-designs:demo-ad5758-ao8z:gui:block_diagram.png|}}\\ |
| //Figure 2 - Eight Channel Board// |
| |
---- | ---- |
[[..:ad5758_adp1031|Top]] | [[specifications|Next (Specifications)]] | [[..:ad5758_adp1031|Top]] | [[specifications|Next (Specifications)]] |