Both sides previous revisionPrevious revisionNext revision | Previous revision |
resources:alliances:digilent [16 Jun 2015 19:08] – [FMC] Walt Kester | resources:alliances:digilent [08 Feb 2021 15:16] (current) – Change broken link Iulia Moldovan |
---|
<WRAP column 45%> | <WRAP column 45%> |
[[http://www.digilentinc.com|{{:resources:digilent.png?100 }}]] Digilent Inc. is a leader in the design, manufacture, and world wide distribution of FPGA and microcontroller technologies. Since its founding in 2000, Digilent has grown to the point where our products can now be found in over 1000 universities in more than 70 countries throughout the world. As a multinational company with offices in the US, Taiwan, China and Romania, Digilent is able to provide low-cost, expert quality solutions for a variety of customer needs. | [[http://www.digilentinc.com|{{:resources:digilent.png?100 }}]] Digilent Inc. is a leader in the design, manufacture, and world wide distribution of FPGA and microcontroller technologies. Since its founding in 2000, Digilent has grown to the point where our products can now be found in over 1000 universities in more than 70 countries throughout the world. As a multinational company with offices in the US, Taiwan, China and Romania, Digilent is able to provide low-cost, expert quality solutions for a variety of customer needs. |
* [[http://www.digilentinc.com/Products/Catalog.cfm?Cat=10&FPGA|FPGA Boards]] | * [[https://store.digilentinc.com/digilent-system-boards-and-components/|FPGA Boards]] |
* [[http://www.digilentinc.com/Products/Catalog.cfm?Cat=9|Pmods]] | * [[https://store.digilentinc.com/boards-and-components/expansion-modules/pmods/|Pmods]] |
| |
</WRAP> | </WRAP> |
===== Pmods ===== | ===== Pmods ===== |
| |
ADI products can be found on many boards which use industry standard connectors, such as Pmods and [[http://www.vita.com/fmc.html|FMC]]. | ADI products can be found on many boards which use industry standard connectors, such as Pmods and [[http://www.vita.com/fmc|FMC]]. |
| |
Pmods are small I/O interface boards that offer an ideal way to extend the capabilities of FPGA/CPLD boards. Pmods communicate with system boards using 6 or 12-pin connectors. Pmods include sensors, I/O, data acquisition & conversion, connectors, and more. Popular systems with Pmod connectors can be found at [[http://www.digilentinc.com/Products/Catalog.cfm?Cat=10&FPGA|Digilent]] or [[http://www.xilinx.com/products/boards-and-kits/AES-S6MB-LX9.htm|Avnet]]. | Pmods are small I/O interface boards that offer an ideal way to extend the capabilities of FPGA/CPLD boards. Pmods communicate with system boards using 6 or 12-pin connectors. Pmods include sensors, I/O, data acquisition & conversion, connectors, and more. Popular systems with Pmod connectors can be found at [[http://www.digilentinc.com/Products/Catalog.cfm?Cat=10&FPGA|Digilent]] or [[xilinx>products/boards-and-kits/AES-S6MB-LX9.htm|Avnet]]. |
| |
| |
|< 100% 15% 75% 10% >| | |< 100% 15% 75% 10% >| |
^ Part Number / Purchase ^ Description ^ ADI Parts ^ | ^ Part Number / Purchase ^ Description ^ ADI Parts ^ |
| [[adi>EVAL-AD7960|EVAL-AD7960FMCZ]] | {{:resources:alliances:eval_ad7960_fmc.jpg?150 |}} **Reference Design:** [[/resources/fpga/xilinx/fmc/ad7960|Analog Devices]]\\ \\ The EVAL-AD7960FMCZ board is based on the AD7960, which is an 18-bit, 5 MSPS charge redistribution successive approximation (SAR), analog-to-digital converter (ADC). The SAR architecture allows unmatched performance both in noise and in linearity. The AD7960 contains a low power, high speed, 18-bit sampling ADC, an internal conversion clock and an internal reference buffer. On the CNV± edge, the AD7960 samples the voltage difference between the IN+ and IN- pins. The voltages on these pins swing in opposite phase between 0 V and 4.096 V/5 V. The reference voltage is applied to the part externally. All conversion results are available on a single LVDS self-clocked or echo-clocked serial interface. | [[adi>AD7960]] | | | [[adi>EVAL-AD7960|EVAL-AD7960FMCZ]] | {{:resources:alliances:eval_ad7960_fmc.jpg?150 |}} **Reference Design:** [[/resources/fpga/xilinx/fmc/ad7960|View Reference Design]]\\ \\ The EVAL-AD7960FMCZ board is based on the AD7960, which is an 18-bit, 5 MSPS charge redistribution successive approximation (SAR), analog-to-digital converter (ADC). The SAR architecture allows unmatched performance both in noise and in linearity. The AD7960 contains a low power, high speed, 18-bit sampling ADC, an internal conversion clock and an internal reference buffer. On the CNV± edge, the AD7960 samples the voltage difference between the IN+ and IN- pins. The voltages on these pins swing in opposite phase between 0 V and 4.096 V/5 V. The reference voltage is applied to the part externally. All conversion results are available on a single LVDS self-clocked or echo-clocked serial interface. | [[adi>AD7960]] | |
| [[adi>EVAL-AD7961|EVAL-AD7961FMCZ]] | {{:resources:alliances:eval_ad7960_fmc.jpg?150 |}} **Reference Design:** [[/resources/fpga/xilinx/fmc/ad7961|Analog Devices]]\\ \\ The EVAL-AD7961FMCZ board is based on the AD7961, which is an 16-bit, 5 MSPS charge redistribution successive approximation (SAR), analog-to-digital converter (ADC). The SAR architecture allows unmatched performance both in noise and in linearity. The AD7961 contains a low power, high speed, 16-bit sampling ADC, an internal conversion clock and an internal reference buffer. On the CNV± edge, the AD7961 samples the voltage difference between the IN+ and IN- pins. The voltages on these pins swing in opposite phase between 0 V and 4.096 V/5 V. The reference voltage is applied to the part externally. All conversion results are available on a single LVDS self-clocked or echo-clocked serial interface. | [[adi>AD7961]] | | | [[adi>EVAL-AD7961|EVAL-AD7961FMCZ]] | {{:resources:alliances:eval_ad7960_fmc.jpg?150 |}} **Reference Design:** [[/resources/fpga/xilinx/fmc/ad7961|View Reference Design]]\\ \\ The EVAL-AD7961FMCZ board is based on the AD7961, which is an 16-bit, 5 MSPS charge redistribution successive approximation (SAR), analog-to-digital converter (ADC). The SAR architecture allows unmatched performance both in noise and in linearity. The AD7961 contains a low power, high speed, 16-bit sampling ADC, an internal conversion clock and an internal reference buffer. On the CNV± edge, the AD7961 samples the voltage difference between the IN+ and IN- pins. The voltages on these pins swing in opposite phase between 0 V and 4.096 V/5 V. The reference voltage is applied to the part externally. All conversion results are available on a single LVDS self-clocked or echo-clocked serial interface. | [[adi>AD7961]] | |
| [[adi>EVAL-AD9434|AD9434-FMC-500EBZ]] |{{:resources:alliances:cf_ad9434_board.jpg?150 }} **Reference Design:** [[/resources/fpga/xilinx/fmc/ad9434|Analog Devices]]\\ \\ The AD9434-FMC-500EBZ board is based on the AD9434, which is a 12-Bit monolithic sampling analog-to-digital converter (ADC) optimized for high performance, low power, and ease of use. The part operates at up to a 500 MSPS conversion rate and is optimized for outstanding dynamic performance in wideband carrier and broadband systems. | [[adi>AD9434]] [[adi>AD9517-4]] | | | [[adi>EVAL-AD9434|AD9434-FMC-500EBZ]] |{{:resources:alliances:cf_ad9434_board.jpg?150 }} **Reference Design:** [[/resources/fpga/xilinx/fmc/ad9434|View Reference Design]]\\ \\ The AD9434-FMC-500EBZ board is based on the AD9434, which is a 12-Bit monolithic sampling analog-to-digital converter (ADC) optimized for high performance, low power, and ease of use. The part operates at up to a 500 MSPS conversion rate and is optimized for outstanding dynamic performance in wideband carrier and broadband systems. | [[adi>AD9434]] [[adi>AD9517-4]] | |
| [[adi>EVAL-AD9467|AD9467-FMC-250EBZ]] | [[http://www.digilentinc.com/Products/Detail.cfm?Prod=AD9467-FMC|{{http://www.digilentinc.com/Data/Products/AD9467-FMC/TILE_AD9467_150.jpg }}]] **Reference Design:** [[/resources/fpga/xilinx/fmc/ad9467|Analog Devices]]\\ \\ The AD9467-FMC-250EBZ board is based on the AD9467, which is a 16-Bit, 250 MSPS analog-to-digital converter that. The AD9467 provides a new level of signal processing performance for test and measurement instrumentation, defense electronics, and communications applications where high resolution over a wide bandwidth is needed. | [[adi>AD9467]] [[adi>AD9517-4]] | | | [[adi>EVAL-AD9467|AD9467-FMC-250EBZ]] | [[http://www.digilentinc.com/Products/Detail.cfm?Prod=AD9467-FMC|{{http://www.digilentinc.com/Data/Products/AD9467-FMC/TILE_AD9467_150.jpg }}]] **Reference Design:** [[/resources/fpga/xilinx/fmc/ad9467|View Reference Design]]\\ \\ The AD9467-FMC-250EBZ board is based on the AD9467, which is a 16-Bit, 250 MSPS analog-to-digital converter that. The AD9467 provides a new level of signal processing performance for test and measurement instrumentation, defense electronics, and communications applications where high resolution over a wide bandwidth is needed. | [[adi>AD9467]] [[adi>AD9517-4]] | |
| [[adi>EVAL-AD9265|AD9265-FMC-125EBZ]] |{{:resources:alliances:cf_ad9265_board.jpg?150 }} **Reference Design:** [[/resources/fpga/xilinx/fmc/ad9265|Analog Devices]]\\ \\ The AD9265-FMC-125EBZ board is based on the AD9265, which is a 16-Bit, 125 MSPS analog-to-digital converter (ADC) featuring a wide bandwidth differential sample-and-hold analog input amplifier supporting a variety of user-selectable input ranges. | [[adi>AD9265]] [[adi>AD9517-4]] | | | [[adi>EVAL-AD9265|AD9265-FMC-125EBZ]] |{{:resources:alliances:cf_ad9265_board.jpg?150 }} **Reference Design:** [[/resources/fpga/xilinx/fmc/ad9265|View Reference Design]]\\ \\ The AD9265-FMC-125EBZ board is based on the AD9265, which is a 16-Bit, 125 MSPS analog-to-digital converter (ADC) featuring a wide bandwidth differential sample-and-hold analog input amplifier supporting a variety of user-selectable input ranges. | [[adi>AD9265]] [[adi>AD9517-4]] | |
| [[adi>EVAL-AD9739A|AD9739A-FMC-EBZ]] | [[http://www.digilentinc.com/Products/Detail.cfm?Prod=AD9739A-FMC|{{http://www.digilentinc.com/Data/Products/AD9739A-FMC/TILE_AD9739A_150.jpg }}]] **Reference Design:** [[/resources/fpga/xilinx/fmc/ad9739a|Analog Devices]]\\ \\ The new AD9739A-FMC-EBZ board is based on the AD9739A is a 14-bit, 2.5 GSPS high performance RF DAC capable of synthesizing wideband signals from dc up to 3 GHz. | [[adi>AD9739A]] [[adi>ADF4350]] | | | [[adi>EVAL-AD9739A|AD9739A-FMC-EBZ]] | [[https://reference.digilentinc.com/ad9739a_fmc/ad9739a_fmc|{{http://www.digilentinc.com/Data/Products/AD9739A-FMC/TILE_AD9739A_150.jpg }}]] **Reference Design:** [[/resources/fpga/xilinx/fmc/ad9739a|View Reference Design]]\\ \\ The new AD9739A-FMC-EBZ board is based on the AD9739A is a 14-bit, 2.5 GSPS high performance RF DAC capable of synthesizing wideband signals from dc up to 3 GHz. | [[adi>AD9739A]] [[adi>ADF4350]] | |
| [[adi>ad-fmcomms1-ebz|AD-FMCOMMS1-EBZ]] |{{:resources:alliances:cf_xcomm_board.jpg?150 }} **Reference Design:** [[/resources/eval/user-guides/ad-fmcomms1-ebz|Analog Devices]]\\ \\ The AD-FMCOMMS1-EBZ is an analog front end hardware platform that addresses a broad range of research, academic, industrial and defense applications. The AD-FMCOMMS1-EBZ enables RF applications from 400MHz to 4 GHz. The module is customizable to a wide range of frequencies by software without any hardware changes, providing options for GPS or IEEE 1588 Synchronization, and MIMO configurations. | [[adi>AD9122]] [[adi>ADL5375]] [[adi>ADF4351]] [[adi>ADL5602]] [[adi>ADL5380]] [[adi>AD8366]] [[adi>AD9643]] [[adi>ADF4351]] [[adi>AD9548]] [[adi>AD9523-1]] | | | [[adi>ad-fmcomms1-ebz|AD-FMCOMMS1-EBZ]] |{{:resources:alliances:cf_xcomm_board.jpg?150 }} **Reference Design:** [[/resources/eval/user-guides/ad-fmcomms1-ebz|View Reference Design]]\\ \\ The AD-FMCOMMS1-EBZ is an analog front end hardware platform that addresses a broad range of research, academic, industrial and defense applications. The AD-FMCOMMS1-EBZ enables RF applications from 400MHz to 4 GHz. The module is customizable to a wide range of frequencies by software without any hardware changes, providing options for GPS or IEEE 1588 Synchronization, and MIMO configurations. | [[adi>AD9122]] [[adi>ADL5375]] [[adi>ADF4351]] [[adi>ADL5602]] [[adi>ADL5380]] [[adi>AD8366]] [[adi>AD9643]] [[adi>ADF4351]] [[adi>AD9548]] [[adi>AD9523-1]] | |
| [[adi>eval-ad-fmcomms2|AD-FMCOMMS2-EBZ]] |{{:resources:alliances:ad_fmcomms2_ebz.jpg?150 }} **Reference Design:** [[/resources/eval/user-guides/ad-fmcomms2-ebz|Analog Devices]]\\ \\ The AD-FMCOMMS2-EBZ is a high-speed analog module designed to showcase the AD9361, a high performance, highly integrated RF agile transceiver intended for use in RF applications, such as 3G and 4G base station applications and software defined radios. The AD-FMCOMMS2-EBZ provides RF engineers the ability to connect the AD9361 to a RF testbench (Vector Signal Analyzer, Signal generator, etc) and measure performance. The external components (which can easily be swapped) on the AD-FMCOMMS2-EBZ have a narrower RF tuning range 2400 – 2500 MHz. It is expected that most engineers will change these external components (pin for pin replacements from various vendors are available) for their specific application/ frequency of interest. Anyone interested in a wider tuning range board should look at the AD-FMCOMMS3-EBZ. | [[adi>AD9361]] | | | [[adi>eval-ad-fmcomms2|AD-FMCOMMS2-EBZ]] |{{:resources:alliances:ad_fmcomms2_ebz.jpg?150 }} **Reference Design:** [[/resources/eval/user-guides/ad-fmcomms2-ebz|View Reference Design]]\\ \\ The AD-FMCOMMS2-EBZ is a high-speed analog module designed to showcase the AD9361, a high performance, highly integrated RF agile transceiver intended for use in RF applications, such as 3G and 4G base station applications and software defined radios. The AD-FMCOMMS2-EBZ provides RF engineers the ability to connect the AD9361 to a RF testbench (Vector Signal Analyzer, Signal generator, etc) and measure performance. The external components (which can easily be swapped) on the AD-FMCOMMS2-EBZ have a narrower RF tuning range 2400 – 2500 MHz. It is expected that most engineers will change these external components (pin for pin replacements from various vendors are available) for their specific application/ frequency of interest. Anyone interested in a wider tuning range board should look at the AD-FMCOMMS3-EBZ. | [[adi>AD9361]] | |
| [[adi>eval-ad-fmcomms3-ebz|AD-FMCOMMS3-EBZ]] |{{:resources:alliances:ad_fmcomms3_ebz.jpg?150 }} **Reference Design:** [[/resources/eval/user-guides/ad-fmcomms3-ebz|Analog Devices]]\\ \\ The AD-FMCOMMS3-EBZ is a high-speed analog module designed to showcase the AD9361, a high performance, highly integrated RF agile transceiver intended for use in RF applications, such as 3G and 4G base station applications and software defined radios. The purpose of the AD-FMCOMMS3-EBZ is to provide an RF platform to software developers, system architects, etc, who want a single platform that operates over a much wider tuning range (70 MHz – 6 GHz) than the AD-FMCOMMS2-EBZ. | [[adi>AD9361]] | | | [[adi>eval-ad-fmcomms3-ebz|AD-FMCOMMS3-EBZ]] |{{:resources:alliances:ad_fmcomms3_ebz.jpg?150 }} **Reference Design:** [[/resources/eval/user-guides/ad-fmcomms3-ebz|View Reference Design]]\\ \\ The AD-FMCOMMS3-EBZ is a high-speed analog module designed to showcase the AD9361, a high performance, highly integrated RF agile transceiver intended for use in RF applications, such as 3G and 4G base station applications and software defined radios. The purpose of the AD-FMCOMMS3-EBZ is to provide an RF platform to software developers, system architects, etc, who want a single platform that operates over a much wider tuning range (70 MHz – 6 GHz) than the AD-FMCOMMS2-EBZ. | [[adi>AD9361]] | |
| [[adi>eval-ad-fmcomms4-ebz|AD-FMCOMMS4-EBZ]] |{{:resources:alliances:ad_fmcomms4_ebz.jpg?150 }} **Reference Design:** [[/resources/eval/user-guides/ad-fmcomms4-ebz|Analog Devices]]\\ \\ The AD-FMCOMMS4-EBZ is a high-speed analog module designed to showcase the AD9364, a high performance, highly integrated RF agile transceiver intended for use in RF applications, such as 3G and 4G base station applications and software defined radios. The purpose of the AD-FMCOMMS4-EBZ is to provide an RF platform to software developers, system architects, etc, who want a single platform that operates over a much wider tuning range (70 MHz – 6 GHz) than the AD-FMCOMMS2-EBZ. | [[adi>AD9364]] | | | [[adi>eval-ad-fmcomms4-ebz|AD-FMCOMMS4-EBZ]] |{{:resources:alliances:ad_fmcomms4_ebz.jpg?150 }} **Reference Design:** [[/resources/eval/user-guides/ad-fmcomms4-ebz|View Reference Design]]\\ \\ The AD-FMCOMMS4-EBZ is a high-speed analog module designed to showcase the AD9364, a high performance, highly integrated RF agile transceiver intended for use in RF applications, such as 3G and 4G base station applications and software defined radios. The purpose of the AD-FMCOMMS4-EBZ is to provide an RF platform to software developers, system architects, etc, who want a single platform that operates over a much wider tuning range (70 MHz – 6 GHz) than the AD-FMCOMMS2-EBZ. | [[adi>AD9364]] | |
| [[adi>eval-ad-fmcomms5-ebz|AD-FMCOMMS5-EBZ]] |{{:resources:alliances:ad_fmcomms5_ebz.jpg?150 }} **Reference Design:** [[/resources/eval/user-guides/ad-fmcomms5-ebz|Analog Devices]]\\ \\ The AD-FMCOMMS5-EBZ is a high-speed analog module designed to showcase the AD9361, a high performance, highly integrated RF agile transceiver intended for use in RF applications, such as 3G and 4G base station applications and software defined radios. The board includes two AD9361s in a 4 x 4 RF configuration, which demonstrates how to synchronize multiple devices together. | [[adi>AD9361]] | | | [[adi>eval-ad-fmcomms5-ebz|AD-FMCOMMS5-EBZ]] |{{:resources:alliances:ad_fmcomms5_ebz.jpg?150 }} **Reference Design:** [[/resources/eval/user-guides/ad-fmcomms5-ebz|View Reference Design]]\\ \\ The AD-FMCOMMS5-EBZ is a high-speed analog module designed to showcase the AD9361, a high performance, highly integrated RF agile transceiver intended for use in RF applications, such as 3G and 4G base station applications and software defined radios. The board includes two AD9361s in a 4 x 4 RF configuration, which demonstrates how to synchronize multiple devices together. | [[adi>AD9361]] | |
| [[adi>eval-ad-fmcomms6-ebz|AD-FMCOMMS6-EBZ]] | {{:resources:fpga:xilinx:fmc:fmcomms6:top_view_main_page.png?150 }} **Reference Design:** [[/resources/eval/user-guides/ad-fmcomms6-ebz|Analog Devices]]\\ \\ The AD-FMCOMMS6-EBZ evaluation board is a 400 MHz to 4.4 GHz receiver based on the AD9652 dual 16-bit ADC, the ADL5566 High Dynamic Range RF/IF Dual Differential Amplifier and the ADL5380 quadrature demodulator. The AD-FMCOMMS6-EBZ is a discrete hardware receiver platform that addresses L and S band radar applications and enables RF applications from 400 MHz to 4 GHz. The module is configurable to a wide range of frequencies small filter hardware changes, providing options for RF up to 4 GHz and IF up to 155 MHz. | [[adi>AD9652]] [[adi>ADF4351]] [[adi>ADL5380]] [[adi>ADL5566]] [[adi>AD9517]] [[adi>ADCLK925]] [[adi>ADP2370]] [[adi>ADM7150]] [[adi>ADP1740]] | | | [[adi>eval-ad-fmcomms6-ebz|AD-FMCOMMS6-EBZ]] | {{:resources:fpga:xilinx:fmc:fmcomms6:top_view_main_page.png?150 }} **Reference Design:** [[/resources/eval/user-guides/ad-fmcomms6-ebz|View Reference Design]]\\ \\ The AD-FMCOMMS6-EBZ evaluation board is a 400 MHz to 4.4 GHz receiver based on the AD9652 dual 16-bit ADC, the ADL5566 High Dynamic Range RF/IF Dual Differential Amplifier and the ADL5380 quadrature demodulator. The AD-FMCOMMS6-EBZ is a discrete hardware receiver platform that addresses L and S band radar applications and enables RF applications from 400 MHz to 4 GHz. The module is configurable to a wide range of frequencies small filter hardware changes, providing options for RF up to 4 GHz and IF up to 155 MHz. | [[adi>AD9652]] [[adi>ADF4351]] [[adi>ADL5380]] [[adi>ADL5566]] [[adi>AD9517]] [[adi>ADCLK925]] [[adi>ADP2370]] [[adi>ADM7150]] [[adi>ADP1740]] | |
| [[adi>ad9250#product-samples|AD-FMCJESDADC1-EBZ]] |{{:resources:alliances:cf_fmc27x_board.jpg?150 }} **Reference Design:** [[/resources/fpga/xilinx/fmc/ad-fmcjesdadc1-ebz|Analog Devices]]\\ \\ The AD-FMCJESDADC1-EBZ board features two [[adi>AD9250]], which is a 14-Bit, 250MSPS analog-to-digital converter (ADC). This board shares the [[http://www.4dsp.com/fmc176|4DSP FMC-176]] PCB, which in addition to the ADC, has two AD9129, which is a 14-Bit, 2.8GSPS digital-to-analog converter (DAC). | [[adi>AD9250]] [[adi>AD9129]] [[adi>AD9517-1]] | | | [[adi>EVAL-AD-FMCADC2-EBZ|AD-FMCADC2-EBZ]] | {{:resources:alliances:ad_fmcadc2_ebz.jpg?150 }} **Reference Design:** [[/resources/eval/user-guides/ad-fmcadc2-ebz|View Reference Design]]\\ \\ The AD-FMCADC2-EBZ is a data acquisition and signal processing platform that contains a complete signal chain for digitizing wideband RF signals for a variety of high-performance applications. The board has operating software and drivers for seamless connectivity within the Xilinx FPGA development platform ecosystem. This board is comprised of the AD9625-2.5 12-bit, 2.5 GSPS JESD204B ADC, input balun, clock oscillator, and critical power management components. | [[adi>AD9625]] | |
| [[adi>en/evaluation/eval-ad-fmcmotcon1/eb.html|AD-FMCMOTCON1]] |{{:resources:eval:user-guides:mc_system.jpg?250 }} **Reference Design:** [[/resources/eval/user-guides/ad-fmcmotcon1-ebz|Analog Devices]]\\ \\ The AD-FMCMOTCON1-EBZ is a complete high performance servo system on an FPGA Mezzanine Card (FMC) board. Information on the FMC board, and how to use it, the design package that surrounds it, and the software which can make it work, can be found by clicking the documentation link. The purpose of the AD-FMCMOTCON1-EBZ is to provide a complete motor drive system demonstrating efficient and high dynamic control of three phase PMSM and induction motors. The kit consists of two boards: a controller board and a drive board. The system incorporates high quality power sources; reliable power, control, and feedback signals isolation; accurate measurement of motor current & voltage signals; high speed interfaces for control signals to allow fast controller response; industrial Ethernet high speed interfaces; flexible control with a FPGA/SoC interface. | [[adi>AD7401]] [[adi>AD8207]] [[adi>AD8251]] [[adi>ADA4084-2]] [[adi>AD8646]] [[adi>AD2S1210]] [[adi>ADUM5000]] [[adi>ADP1614]] [[adi>ADP1621]] [[adi>ADP2301]] [[adi>ADP7102]] [[adi>ADM660]] [[adi>ADUM7640]] [[adi>ADUM5230]] [[adi>ADG3308]] [[adi>ADG704]] [[adi>ADG759]] | | | [[adi>EVAL-AD-FMCDAQ2-EBZ|AD-FMCDAQ2-EBZ]] | {{:resources:alliances:ad_fmcdaq2_ebz.jpg?150 }} **Reference Design:** [[/resources/eval/user-guides/ad-fmcdaq2-ebz|View Reference Design]]\\ \\ The AD-FMCDAQ2-EBZ module is comprised of the AD9680 dual, 14-bit, 1.0 GSPS, JESD204B ADC, the AD9144 quad, 16-bit, 2.8 GSPS, JESD204B DAC, the AD9523-1 14-output, 1 GHz clock generator, and power management components. It is clocked by an internally generated carrier platform via the FMC connector, comprising a completely self-contained data acquisition and signal synthesis prototyping platform. The module’s combination of wideband data conversion, clocking, and power closely approximates real-world hardware and software for system prototyping and design, with no compromise in signal chain performance. | [[adi>AD9680]] [[adi>AD9144]] [[adi>AD9523-1]] [[adi>ADN4661]] [[adi>ADP1740]] [[adi>ADP150]] | |
| | [[adi>EVAL-AD-FMCJESDADC1-EBZ|AD-FMCJESDADC1-EBZ]] | {{:resources:alliances:ad_fmcjesdadc1_ebz.jpg?150 }} **Reference Design:** [[/resources/fpga/xilinx/fmc/ad-fmcjesdadc1-ebz|View Reference Design]]\\ \\ The AD-FMCJESDADC1-EBZ board features two [[adi>AD9250]], which is a 14-Bit, 250MSPS analog-to-digital converter (ADC). This board shares the [[http://www.4dsp.com/fmc176|4DSP FMC-176]] PCB, which in addition to the ADC, has two AD9129, which is a 14-Bit, 2.8GSPS digital-to-analog converter (DAC). | [[adi>AD9250]] [[adi>AD9129]] [[adi>AD9517-1]] | |
| | [[adi>eval-fmcmotcon2|AD-FMCMOTCON2]] | {{:resources:alliances:eval-fmcmotcon2-system.jpg?200 }} **Reference Design:** [[/resources/eval/user-guides/ad-fmcmotcon2-ebz|View Reference Design]]\\ \\ The AD-FMCMOTCON2-EBZ is a complete high performance servo system on an FPGA Mezzanine Card (FMC) board. Information on the FMC board, and how to use it, the design package that surrounds it, and the software which can make it work, can be found by clicking the documentation link. The purpose of the AD-FMCMOTCON2-EBZ is to provide a complete motor drive system demonstrating efficient and high dynamic control of three phase PMSM and induction motors. The kit consists of two boards: a controller board and a drive board. The system incorporates high quality power sources; reliable power, control, and feedback signals isolation; accurate measurement of motor current & voltage signals; high speed interfaces for control signals to allow fast controller response; industrial Ethernet high speed interfaces; flexible control with a FPGA/SoC interface. An optional AD-DYNO2-EBZ dynamometer can be purchased through Avnet and is intended to be an extension of the drive system. | [[adi>ADUM7640]] [[adi>ADUM7641]] [[adi>ADM2486]] [[adi>ADUM1400]] [[adi>ADUM1402]] [[adi>ADG3308]] [[adi>AD8646]] [[adi>AD8137]] [[adi>ADUM5000]] [[adi>AD2S1210]] [[adi>ADN4662]] [[adi>ADG759]] [[adi>ADUM1250]] [[adi>CMP04]] [[adi>ADP2301]] [[adi>ADP1621]] [[adi>ADUM7223]] [[adi>ADUM5230]] [[adi>AD8207]] [[adi>AD7403]] [[adi>AD7402]] [[adi>AD7405]] | |