Skip to content

analogdevicesinc/plutosdr-m2k-drivers-win

Repository files navigation

plutosdr-m2k-drivers-win

Windows USB drivers for PlutoSDR & M2k

Latest Release : GitHub release

Supported Hardware

  • ADALM-PLUTO
  • ADALM-2000
  • Generic IIO/Serial Console device using VID_0456&PID_B671

Release History

  • v0.5
    • Fix package installer on Windows 32-bit
  • v0.6 (No need to update from v0.5)
    • Add reference to M2k onto the wizard pages (no functional changes)
    • Force DPInst to install the driver even if the driver that is currently installed is a better match than the new driver
  • v0.7
    • Removed language nodes from dpinst.xml, this should fix this Error: "The current language is not supported by the Device Driver Installation Wizard)"
  • v0.8
    • New device support
  • v0.9
    • Support for Windows 8.1 (no need to update in case you're not using Windows 8.1)