This is an old revision of the document!
The ADIS16470 IMU board is ADI's rugged, tactical IMU designed for use in a wide variety of applications, including industrial robots, smart agriculture, and autonomous vehicles. The ADIS16470 is a 10 degree-of-freedom IMU, with 3-axis gyro, 3-axis accelerometer, 3-axis magnetometer, and a barometer.
ADIS16470 software and examples for Java, C+ +, and LabVIEW can be found here. If your team wants to use this board with other programming languages, please refer to the ADIS16470 product datasheet for more information on how to communicate with this IMU via SPI.
If you're looking for information on other ADI donation resources, click here to go back to the main page.
The ADIS16470 IMU Board is designed to plug directly into the SPI port on the RoboRIO. The IMU board has an extension with two mounting holes which should be used to secure it to the RoboRIO with #4-40 screws. The figure to the right illustrates the locations of the X, Y, and Z axes in relation to the device package.
To help the robot minimize start-up drift and improve overall sensor performance, an offset calibration function has been built into the IMU driver. This function captures several seconds worth of data and calculates an average offset which is then applied to the sensor outputs. By default, calibration is automatically started once the RoboRIO begins executing user code and usually takes about 10 seconds to complete. The “Ready?” LED indicator will also illuminate once calibration is complete. New in 2020, all three language libraries also have this functionality made available via the “Recalibrate” function.
As mentioned above, the 2020 versions of the libraries include a new function called “recalibrate” that takes advantage of features available on the ADIS16470. It's important to note the difference between “reset” and “recalibrate” as they are very different functions and have differing use cases!
“Recalibrating” the IMU will reconfigure the offset calibration in the device. Upon startup, the libraries for the ADIS16470 will automatically perform an offset calibration as described above. It does this by taking readings for a few seconds (the default is 4 seconds) and averaging those values together to form an offset, one for each axis. This allows the IMU to calibrate out some drift to improve the sensor performance. We discussed above that any movement of the robot during this calibration period will negatively impact sensor performance. Before 2020, there was no function that would allow teams to recalibrate the IMU without restarting robot code. If the robot was bumped or moved during startup, IMU performance would be impaired. The ADIS16470 has an internal feature which continuously averages the internal sensor readings and stores them on the device. The device can be instructed to use these averages as the new internal offset values when a certain command is issued. This is what the new recalibrate function does.
“Resetting” the IMU simply “re-zeros” the device. You may recall that gyros output data as degrees per second, not degrees,and we must integrate the readings from the device in order to determine a heading in degrees. When we reset the IMU, we are resetting this integration and starting back at zero. This means that the direction that the robot is facing when you reset the IMU will become the new zero degrees direction.
For more information on how to add IMU functionality to your robot code, select your team's programming language from the list below.
Using the ADIS16470 IMU in LabVIEW
Using the ADIS16470 IMU in C++
Using the ADIS16470IMU in Java