This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
eval:hmc8362_user_guide [10 Aug 2020 19:31] – [Evaluation Kit Contents] Kieran Barrett | eval:hmc8362_user_guide [10 Aug 2020 19:39] (current) – Indenting headings. Kieran Barrett | ||
---|---|---|---|
Line 13: | Line 13: | ||
EV1HMC8364LP6G evaluation board | EV1HMC8364LP6G evaluation board | ||
- | ====Equipment Needed==== | + | =====Equipment Needed===== |
* Power supply (6 V) | * Power supply (6 V) | ||
* Power supply (low noise, variable 0 V to 13.5 V) | * Power supply (low noise, variable 0 V to 13.5 V) | ||
Line 19: | Line 19: | ||
* Signal source analyzer | * Signal source analyzer | ||
- | ====Online Resources==== | + | =====Online Resources===== |
* [[adi> | * [[adi> | ||
* [[adi> | * [[adi> | ||
* Linduino DC2026C Demo Manual | * Linduino DC2026C Demo Manual | ||
- | ====General Description==== | + | =====General Description===== |
The EV1HMC8362LP6G and EV1HMC8364LP6G allow the evaluation of the performance of the [[adi> | The EV1HMC8362LP6G and EV1HMC8364LP6G allow the evaluation of the performance of the [[adi> | ||
Consult the [[adi> | Consult the [[adi> | ||
- | ====EV1HMC8362LP6G/ | + | =====EV1HMC8362LP6G/ |
{{ : | {{ : | ||
Figure 1. Evaluation Board | Figure 1. Evaluation Board | ||
- | ====Getting Started==== | + | =====Getting Started===== |
- | ===Evaluation Board Setup Procedure=== | + | ====Evaluation Board Setup Procedure==== |
To configure the EV1HMC8362LP6G or EV1HMC8364LP6G for the first time, perform the following steps. | To configure the EV1HMC8362LP6G or EV1HMC8364LP6G for the first time, perform the following steps. | ||
- Verify that the analog power supply that is used to power the evaluation board configured to allow an output of 6.0 V and 200 mA of compliance current. | - Verify that the analog power supply that is used to power the evaluation board configured to allow an output of 6.0 V and 200 mA of compliance current. | ||
Line 46: | Line 46: | ||
{{ : | {{ : | ||
Figure 2. Connector P1 Jumper Configuration: | Figure 2. Connector P1 Jumper Configuration: | ||
- | ====Evaluation Board Hardware==== | + | =====Evaluation Board Hardware===== |
The EV1HMC8362LP6G and EV1HMC8364LP6G are identical except for Resistor R6, which sets the current limit function of the [[adi> | The EV1HMC8362LP6G and EV1HMC8364LP6G are identical except for Resistor R6, which sets the current limit function of the [[adi> | ||
The evaluation board schematics, assembly, silkscreen, and bill of materials are available in the Evaluation Board Schematics and Artwork section and Ordering Information section. The gerber fabrication files are available on the [[adi> | The evaluation board schematics, assembly, silkscreen, and bill of materials are available in the Evaluation Board Schematics and Artwork section and Ordering Information section. The gerber fabrication files are available on the [[adi> | ||
- | ===POWER SUPPLIES=== | + | ====POWER SUPPLIES==== |
The EV1HMC8362LP6G and EV1HMC8364LP6G boards are powered by a 6 V dc (150 mA) power supply connected to the SMA connector J1 labeled 6.0 V. This supply path includes a single ultralow noise, (LDO) regulator, the [[adi> | The EV1HMC8362LP6G and EV1HMC8364LP6G boards are powered by a 6 V dc (150 mA) power supply connected to the SMA connector J1 labeled 6.0 V. This supply path includes a single ultralow noise, (LDO) regulator, the [[adi> | ||
Users that intend to use an external power supply such as the Linduino® or Arduino® Uno microcontroller to directly program the logic from the P3 header must remove the five 10 kΩ resistors (R18, R26, R35, R36, and R37) or damage may occur. | Users that intend to use an external power supply such as the Linduino® or Arduino® Uno microcontroller to directly program the logic from the P3 header must remove the five 10 kΩ resistors (R18, R26, R35, R36, and R37) or damage may occur. | ||
A second low noise power supply cable providing up to 13.5 V is required to tune the VCOs. Use of a noisy power supply on the tuning port results in narrow-band FM modulation and sidebands. | A second low noise power supply cable providing up to 13.5 V is required to tune the VCOs. Use of a noisy power supply on the tuning port results in narrow-band FM modulation and sidebands. | ||
- | ===VOLTAGE CONTROLLED OSCILLATOR (VCO)=== | + | ====VOLTAGE CONTROLLED OSCILLATOR (VCO)==== |
The [[adi> | The [[adi> | ||
By generating fundamental frequencies, | By generating fundamental frequencies, | ||
Line 61: | Line 61: | ||
The EV1HMC8362LP6G and EV1HMC8364LP6G boards include additional filtering to prevent supply voltage overshoot and undershoot, which can damage the device if overshoot exceeds 5.5 V. This filtering provides 5 V of biasing that settles within about 1 µs. | The EV1HMC8362LP6G and EV1HMC8364LP6G boards include additional filtering to prevent supply voltage overshoot and undershoot, which can damage the device if overshoot exceeds 5.5 V. This filtering provides 5 V of biasing that settles within about 1 µs. | ||
- | ===BUFFER AMPLIFIER=== | + | ====BUFFER AMPLIFIER==== |
The buffer amplifier used in the [[adi> | The buffer amplifier used in the [[adi> | ||
Refer to the [[adi> | Refer to the [[adi> | ||
Line 68: | Line 68: | ||
For additional details on the buffer amplifier circuitry, consult the [[adi> | For additional details on the buffer amplifier circuitry, consult the [[adi> | ||
- | ===RF Output=== | + | ====RF Output==== |
The EV1HMC8362LP6G and EV1HMC8364LP6G boards have a single RF output port (RF1). RF1 is supplied by a buffer amplifier that is common to all four VCO cores. | The EV1HMC8362LP6G and EV1HMC8364LP6G boards have a single RF output port (RF1). RF1 is supplied by a buffer amplifier that is common to all four VCO cores. | ||
RF1 (J3) is a single-ended RF output that operates up to 26.6 GHz. The actual frequency range and power level at any given time depends on which model is being evaluated and the VCO core that is enabled. Consult the [[adi> | RF1 (J3) is a single-ended RF output that operates up to 26.6 GHz. The actual frequency range and power level at any given time depends on which model is being evaluated and the VCO core that is enabled. Consult the [[adi> | ||
- | ===Loop Filter=== | + | ====Loop Filter==== |
Although the EV1HMC8362LP6G and EV1HMC8364LP6G boards do not incorporate the entire loop filter, they do provide the means to filter noise that may appear on the tuning port when evaluating only the VCOs. | Although the EV1HMC8362LP6G and EV1HMC8364LP6G boards do not incorporate the entire loop filter, they do provide the means to filter noise that may appear on the tuning port when evaluating only the VCOs. | ||
By default, a 100 pF capacitor (C12) is placed near Pin 27 (VTUNE) of the [[adi> | By default, a 100 pF capacitor (C12) is placed near Pin 27 (VTUNE) of the [[adi> | ||
Line 80: | Line 80: | ||
SMA Connector J2 provides means to connect the PLL CP output to the tuning port (VTUNE) when the EV1HMC8362LP6G and EV1HMC8364LP6G are used with an optional PLL evaluation board. J2 can also be used to manually tune the VCO within its band when evaluating the open-loop VCO performance. | SMA Connector J2 provides means to connect the PLL CP output to the tuning port (VTUNE) when the EV1HMC8362LP6G and EV1HMC8364LP6G are used with an optional PLL evaluation board. J2 can also be used to manually tune the VCO within its band when evaluating the open-loop VCO performance. | ||
- | ===Default Configuration=== | + | ====Default Configuration==== |
All components necessary for local oscillator generation are inserted on the EV1HMC8362LP6G and EV1HMC8364LP6G boards. | All components necessary for local oscillator generation are inserted on the EV1HMC8362LP6G and EV1HMC8364LP6G boards. | ||
- | ====Evaluation Board Software==== | + | =====Evaluation Board Software===== |
- | ===Software=== | + | ====Software==== |
Currently there is no software available for the EV1HMC8362LP6G and EV1HMC8364LP6G because they can be evaluated without the use of software. However, the EV1HMC8362LP6G and EV1HMC8364LP6G are configured in a manner that allows use of a Linduino, Arduino Uno, or similar microcontroller board, which may be beneficial for users needing to develop and test switching algorithms for their application. | Currently there is no software available for the EV1HMC8362LP6G and EV1HMC8364LP6G because they can be evaluated without the use of software. However, the EV1HMC8362LP6G and EV1HMC8364LP6G are configured in a manner that allows use of a Linduino, Arduino Uno, or similar microcontroller board, which may be beneficial for users needing to develop and test switching algorithms for their application. | ||
To connect the Arduino Uno microcontroller to the EV1HMC8362LP6G or EV1HMC8364LP6G, | To connect the Arduino Uno microcontroller to the EV1HMC8362LP6G or EV1HMC8364LP6G, | ||
- | ====Evaluation and Test==== | + | =====Evaluation and Test===== |
To configure the EV1HMC8362LP6G and EV1HMC8364LP6G for the first time, follow Step 1 through Step 6 outlined in the Evaluation Board Setup Procedure section. | To configure the EV1HMC8362LP6G and EV1HMC8364LP6G for the first time, follow Step 1 through Step 6 outlined in the Evaluation Board Setup Procedure section. | ||
The frequency vs. tune voltage listed in the following steps are specific to the EV1HMC8362LP6G, | The frequency vs. tune voltage listed in the following steps are specific to the EV1HMC8362LP6G, | ||
Line 104: | Line 104: | ||
Figure 5. EV1HMC8362LP6G Phase Noise at RF1, VCO Band 1, VTUNE = 8.45 V, 13.5 GHz | Figure 5. EV1HMC8362LP6G Phase Noise at RF1, VCO Band 1, VTUNE = 8.45 V, 13.5 GHz | ||
- | ====Schematics, | + | =====Schematics, |
====EV1HMC8362LP6G==== | ====EV1HMC8362LP6G==== | ||
* {{ : | * {{ : |