This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
eval:hmc8362_user_guide [10 Aug 2020 15:26] – [EV1HMC8362LP6G/EV1HMC8364LP6G EVALUATION BOARD PHOTOGRAPH] Kieran Barrett | eval:hmc8362_user_guide [10 Aug 2020 19:39] (current) – Indenting headings. Kieran Barrett | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== EV1HMC8362LP6G/ | ====== EV1HMC8362LP6G/ | ||
- | ====Evaluating the HMC8362/ | + | =====Evaluating the HMC8362/ |
- | ====FEATURES==== | + | =====Features===== |
- | * Self contained board, Including HMC8362 or HMC8364 low noise quadband VCO, | + | * Self contained board, Including |
- | * ADG1604 4:1 multiplexer, | + | * [[adi>ADG1604]] 4:1 multiplexer, |
* Filtering options, | * Filtering options, | ||
- | * LT3042 voltage regulator | + | * [[adi>LT3042]] voltage regulator |
* Header connectivity to allow use of Arduino Uno or Linduino microcontroller | * Header connectivity to allow use of Arduino Uno or Linduino microcontroller | ||
* Externally powered by a single 6.0 V supply | * Externally powered by a single 6.0 V supply | ||
- | ====EVALUATION KIT CONTENTS==== | + | =====Evaluation Kit Contents===== |
- | EV1HMC8362LP6G or EV1HMC8364LP6G evaluation board | + | EV1HMC8362LP6G or |
+ | EV1HMC8364LP6G evaluation board | ||
- | ====EQUIPMENT NEEDED==== | + | =====Equipment Needed===== |
* Power supply (6 V) | * Power supply (6 V) | ||
* Power supply (low noise, variable 0 V to 13.5 V) | * Power supply (low noise, variable 0 V to 13.5 V) | ||
Line 18: | Line 19: | ||
* Signal source analyzer | * Signal source analyzer | ||
- | ====ONLINE RESOURCES==== | + | =====Online Resources===== |
- | * HMC8362 data sheet | + | * [[adi>HMC8362]] data sheet |
- | * HMC8364 data sheet | + | * [[adi>HMC8364]] data sheet |
* Linduino DC2026C Demo Manual | * Linduino DC2026C Demo Manual | ||
- | ====GENERAL DESCRIPTION==== | + | =====General Description===== |
- | The EV1HMC8362LP6G and EV1HMC8364LP6G allow the evaluation of the performance of the HMC8362 and HMC8364 low noise quadband voltage controlled oscillators (VCOs). A photograph of the evaluation board is shown in Figure 1. The evaluation board contains the HMC8362 or HMC8364 VCO, an LT3042 ultralow noise voltage regulator, a jumper, an ADG1604 4:1 multiplexer, | + | The EV1HMC8362LP6G and EV1HMC8364LP6G allow the evaluation of the performance of the [[adi>HMC8362]] and [[adi>HMC8364]] low noise quadband voltage controlled oscillators (VCOs). A photograph of the evaluation board is shown in Figure 1. The evaluation board contains the [[adi>HMC8362]] or [[adi>HMC8364]] VCO, an [[adi>LT3042]] ultralow noise voltage regulator, a jumper, an [[adi>ADG1604]] 4:1 multiplexer, |
- | Consult the HMC8362 and HMC8364 data sheets in conjunction with this user guide when working with the evaluation boards. | + | Consult the [[adi>HMC8362]] and [[adi>HMC8364]] data sheets in conjunction with this user guide when working with the evaluation boards. |
- | ====EV1HMC8362LP6G/ | + | =====EV1HMC8362LP6G/ |
- | {{ : | + | {{ :resources: |
Figure 1. Evaluation Board | Figure 1. Evaluation Board | ||
- | + | =====Getting Started===== | |
- | ====GETTING STARTED==== | + | ====Evaluation Board Setup Procedure==== |
- | ===EVALUATION BOARD SETUP PROCEDURE=== | + | |
To configure the EV1HMC8362LP6G or EV1HMC8364LP6G for the first time, perform the following steps. | To configure the EV1HMC8362LP6G or EV1HMC8364LP6G for the first time, perform the following steps. | ||
- Verify that the analog power supply that is used to power the evaluation board configured to allow an output of 6.0 V and 200 mA of compliance current. | - Verify that the analog power supply that is used to power the evaluation board configured to allow an output of 6.0 V and 200 mA of compliance current. | ||
- Disable the power supply output. | - Disable the power supply output. | ||
- Using a double shielded BNC cable and a BNC to SMA adapter, connect the analog power supply to J1. | - Using a double shielded BNC cable and a BNC to SMA adapter, connect the analog power supply to J1. | ||
- | - Use the supplied shorting jumpers to configure the logic, as shown in Figure 2. In the configuration shown in Figure 2, the ADG1604 multiplexer, | + | - Use the supplied shorting jumpers to configure the logic, as shown in Figure 2. In the configuration shown in Figure 2, the [[adi>ADG1604]] multiplexer, |
- Connect the low noise, variable power supply to the SMA connector on the tuning port (J2) using a double shielded BNC cable and a BNC to SMA adapter. Torque this connection to 8 in/lb using an SMA torque wrench. | - Connect the low noise, variable power supply to the SMA connector on the tuning port (J2) using a double shielded BNC cable and a BNC to SMA adapter. Torque this connection to 8 in/lb using an SMA torque wrench. | ||
- Connect a 50 Ω RF cable capable of mating to the 2.92 mm K connector at J3 and torque this connection to 8 in/lb. Connect the other end of the cable to a signal source analyzer. | - Connect a 50 Ω RF cable capable of mating to the 2.92 mm K connector at J3 and torque this connection to 8 in/lb. Connect the other end of the cable to a signal source analyzer. | ||
- Enable the 6 V power supply. Approximately 103 mA is drawn if the part is configured correctly. | - Enable the 6 V power supply. Approximately 103 mA is drawn if the part is configured correctly. | ||
- Enable the variable power supply and adjust the tuning voltage to within the range of the VCO band being used. | - Enable the variable power supply and adjust the tuning voltage to within the range of the VCO band being used. | ||
- | - Verify that the correct output frequency is observed on the signal source analyzer. An example using the HMC8362 is outlined in the Evaluation and Test section. | + | - Verify that the correct output frequency is observed on the signal source analyzer. An example using the [[adi>HMC8362]] is outlined in the Evaluation and Test section. |
- | {{ : | + | {{ :resources: |
- | Figure 2 Connector P1 Jumper Configuration: | + | Figure 2. Connector P1 Jumper Configuration: |
- | + | =====Evaluation Board Hardware===== | |
- | ====EVALUATION BOARD HARDWARE==== | + | The EV1HMC8362LP6G and EV1HMC8364LP6G are identical except for Resistor R6, which sets the current limit function of the [[adi>LT3042]], and C31 which is the AC coupling capacitor on the RF output port. |
- | The EV1HMC8362LP6G and EV1HMC8364LP6G are identical except for Resistor R6, which sets the current limit function of the LT3042, and C31 which is the AC coupling capacitor on the RF output port. | + | The evaluation board schematics, assembly, silkscreen, and bill of materials are available in the Evaluation Board Schematics and Artwork section and Ordering Information section. The gerber fabrication files are available on the [[adi>HMC8362]]and [[adi>HMC8364]] product pages on analog.com. |
- | The evaluation board schematics, assembly, silkscreen, and bill of materials are available in the Evaluation Board Schematics and Artwork section and Ordering Information section. The gerber fabrication files are available on the HMC8362 and HMC8364 product pages on analog.com. | + | |
- | ===POWER SUPPLIES=== | + | ====POWER SUPPLIES==== |
- | The EV1HMC8362LP6G and EV1HMC8364LP6G boards are powered by a 6 V dc (150 mA) power supply connected to the SMA connector J1 labeled 6.0 V. This supply path includes a single ultralow noise, (LDO) regulator, the LT3042. As an extra safeguard, the LT3042 is configured to use the current-limit feature. A resistor (R6) sets the current limit on ILIM (Pin 5) of the LT3042 to 114 mA (R6 = 1100 Ω) on EV1HMC8362LP6G and 156 mA (R6 = 806 Ω) for the EV1HMC8364LP6G. | + | The EV1HMC8362LP6G and EV1HMC8364LP6G boards are powered by a 6 V dc (150 mA) power supply connected to the SMA connector J1 labeled 6.0 V. This supply path includes a single ultralow noise, (LDO) regulator, the [[adi>LT3042]]. As an extra safeguard, the [[adi>LT3042]] is configured to use the current-limit feature. A resistor (R6) sets the current limit on ILIM (Pin 5) of the [[adi>LT3042]] to 114 mA (R6 = 1100 Ω) on EV1HMC8362LP6G and 156 mA (R6 = 806 Ω) for the EV1HMC8364LP6G. |
Users that intend to use an external power supply such as the Linduino® or Arduino® Uno microcontroller to directly program the logic from the P3 header must remove the five 10 kΩ resistors (R18, R26, R35, R36, and R37) or damage may occur. | Users that intend to use an external power supply such as the Linduino® or Arduino® Uno microcontroller to directly program the logic from the P3 header must remove the five 10 kΩ resistors (R18, R26, R35, R36, and R37) or damage may occur. | ||
A second low noise power supply cable providing up to 13.5 V is required to tune the VCOs. Use of a noisy power supply on the tuning port results in narrow-band FM modulation and sidebands. | A second low noise power supply cable providing up to 13.5 V is required to tune the VCOs. Use of a noisy power supply on the tuning port results in narrow-band FM modulation and sidebands. | ||
- | ===VOLTAGE CONTROLLED OSCILLATOR (VCO)=== | + | ====VOLTAGE CONTROLLED OSCILLATOR (VCO)==== |
- | The HMC8362 and HMC8364 models include a total of four VCO cores that generate a range of fundamental frequencies. The frequency range of each core overlaps the adjacent core to allow continuous frequency coverage including any supply and temperature variation. | + | The [[adi>HMC8362]] and [[adi>HMC8364]] models include a total of four VCO cores that generate a range of fundamental frequencies. The frequency range of each core overlaps the adjacent core to allow continuous frequency coverage including any supply and temperature variation. |
By generating fundamental frequencies, | By generating fundamental frequencies, | ||
- | The oscillator cores must be selected, one at a time, depending on the frequency range required at any point in time by the application. The VCO cores are selected by simply enabling the supply voltage at its respective bias pin (VC1 through VC4). The EV1HMC8362LP6G and EV1HMC8364LP6G boards accomplish this VCO core selection through the use of the ADG1604 4:1 multiplexer. The VCO cores can be enabled and disabled in any sequence desired. | + | The oscillator cores must be selected, one at a time, depending on the frequency range required at any point in time by the application. The VCO cores are selected by simply enabling the supply voltage at its respective bias pin (VC1 through VC4). The EV1HMC8362LP6G and EV1HMC8364LP6G boards accomplish this VCO core selection through the use of the [[adi>ADG1604]] 4:1 multiplexer. The VCO cores can be enabled and disabled in any sequence desired. |
The EV1HMC8362LP6G and EV1HMC8364LP6G boards include additional filtering to prevent supply voltage overshoot and undershoot, which can damage the device if overshoot exceeds 5.5 V. This filtering provides 5 V of biasing that settles within about 1 µs. | The EV1HMC8362LP6G and EV1HMC8364LP6G boards include additional filtering to prevent supply voltage overshoot and undershoot, which can damage the device if overshoot exceeds 5.5 V. This filtering provides 5 V of biasing that settles within about 1 µs. | ||
- | ===BUFFER AMPLIFIER=== | + | ====BUFFER AMPLIFIER==== |
- | The buffer amplifier used in the HMC8362 and HMC8364 is a broadband cascode design that draws approximately 12 mA and is shared by all four VCO cores. Pin 8 (VCB) of the HMC8362 and HMC8364 provides the bias voltage for the upper half of the cascode amplifier. The VCO outputs provide the biasing for the lower half of the cascode amplifier stage. When one of the four VCOs is enabled, the cascode amplifier becomes fully enabled and provides an output signal at Pin 5 (RF1 on the HMC8364 or RFOUT on the HMC8362). The buffer amplifier was designed to handle the power supplied by only one VCO at a time. To prevent long-term damage that can occur if more than one VCO is powered up simultaneously, | + | The buffer amplifier used in the [[adi>HMC8362]] and [[adi>HMC8364]]is a broadband cascode design that draws approximately 12 mA and is shared by all four VCO cores. Pin 8 (VCB) of the [[adi>HMC8362]] and [[adi>HMC8364]] provides the bias voltage for the upper half of the cascode amplifier. The VCO outputs provide the biasing for the lower half of the cascode amplifier stage. When one of the four VCOs is enabled, the cascode amplifier becomes fully enabled and provides an output signal at Pin 5. The buffer amplifier was designed to handle the power supplied by only one VCO at a time. To prevent long-term damage that can occur if more than one VCO is powered up simultaneously, |
- | Refer to the ADG1604 data sheet for more information regarding the ADG1604 logic and use with other logic levels. | + | Refer to the [[adi>ADG1604]] data sheet for more information regarding the [[adi>ADG1604]] logic and use with other logic levels. |
Users can opt to leave the VCO enabled and power down Pin 8 (VCB) to mute the output signal, which leaves the lower stage of the cascode enabled. However, because the upper circuitry is disabled, RF is not routed to the output. | Users can opt to leave the VCO enabled and power down Pin 8 (VCB) to mute the output signal, which leaves the lower stage of the cascode enabled. However, because the upper circuitry is disabled, RF is not routed to the output. | ||
- | Figure 5 shows the HMC8362 with VC1 enabled but the output buffer muted (VCB_EN on P3 = 0). | + | Figure 5 shows the [[adi>HMC8362]] with VC1 enabled but the output buffer muted (VCB_EN on P3 = 0). |
- | For additional details on the buffer amplifier circuitry, consult the HMC8362 or HMC8364 data sheet. | + | For additional details on the buffer amplifier circuitry, consult the [[adi>HMC8362]] or [[adi>HMC8364]] data sheet. |
- | ===RF OUTPUT=== | + | ====RF Output==== |
The EV1HMC8362LP6G and EV1HMC8364LP6G boards have a single RF output port (RF1). RF1 is supplied by a buffer amplifier that is common to all four VCO cores. | The EV1HMC8362LP6G and EV1HMC8364LP6G boards have a single RF output port (RF1). RF1 is supplied by a buffer amplifier that is common to all four VCO cores. | ||
- | RF1 (J3) is a single-ended RF output that operates up to 26.6 GHz. The actual frequency range and power level at any given time depends on which model is being evaluated and the VCO core that is enabled. Consult the HMC8362 and HMC8364 data sheets for additional information relative to the specific model being evaluated for more information. | + | RF1 (J3) is a single-ended RF output that operates up to 26.6 GHz. The actual frequency range and power level at any given time depends on which model is being evaluated and the VCO core that is enabled. Consult the [[adi>HMC8362]] and [[adi>HMC8364]] data sheets for additional information relative to the specific model being evaluated for more information. |
- | ===LOOP FILTER=== | + | ====Loop Filter==== |
Although the EV1HMC8362LP6G and EV1HMC8364LP6G boards do not incorporate the entire loop filter, they do provide the means to filter noise that may appear on the tuning port when evaluating only the VCOs. | Although the EV1HMC8362LP6G and EV1HMC8364LP6G boards do not incorporate the entire loop filter, they do provide the means to filter noise that may appear on the tuning port when evaluating only the VCOs. | ||
- | By default, a 100 pF capacitor (C12) is placed near Pin 27 (VTUNE) of the HMC8362 and HMC8364 to filter high frequency noise that may couple onto the tune port path when evaluating the various VCOs. | + | By default, a 100 pF capacitor (C12) is placed near Pin 27 (VTUNE) of the [[adi>HMC8362]] and [[adi>HMC8364]] to filter high frequency noise that may couple onto the tune port path when evaluating the various VCOs. |
- | The EV1HMC8362LP6G and EV1HMC8364LP6G boards also include placements for the last pole of a loop filter on the tuning port path for use when configuring the HMC8362 and HMC8364 with an Analog Devices, Inc., standalone phase-locked loop (PLL) product like the ADF41513. Although the tuning port path and input capacitance of the VCO makes up the last pole of the loop filter, this user guide refers to the last pole as that which can be accessed by the user. | + | The EV1HMC8362LP6G and EV1HMC8364LP6G boards also include placements for the last pole of a loop filter on the tuning port path for use when configuring the [[adi>HMC8362]] and [[adi>HMC8364]] with an Analog Devices, Inc., standalone phase-locked loop (PLL) product like the ADF41513. Although the tuning port path and input capacitance of the VCO makes up the last pole of the loop filter, this user guide refers to the last pole as that which can be accessed by the user. |
Due to the increased length of the loop filter path that typically occurs when using evaluation boards to build a synthesizer, | Due to the increased length of the loop filter path that typically occurs when using evaluation boards to build a synthesizer, | ||
- | The tuning voltage requirements of the HMC8362 and HMC8364 (1.0 V to 13.5 V) require an active loop filter to be used unless the charge pump of the PLL can output at least 14 V. The PLL evaluation board typically includes placements for the operational amplifier, its biasing circuitry, and any component placements. Therefore, these components are not included on the EV1HMC8362LP6G and EV1HMC8364LP6G. | + | The tuning voltage requirements of the [[adi>HMC8362]] and [[adi>HMC8364]] (1.0 V to 13.5 V) require an active loop filter to be used unless the charge pump of the PLL can output at least 14 V. The PLL evaluation board typically includes placements for the operational amplifier, its biasing circuitry, and any component placements. Therefore, these components are not included on the EV1HMC8362LP6G and EV1HMC8364LP6G. |
SMA Connector J2 provides means to connect the PLL CP output to the tuning port (VTUNE) when the EV1HMC8362LP6G and EV1HMC8364LP6G are used with an optional PLL evaluation board. J2 can also be used to manually tune the VCO within its band when evaluating the open-loop VCO performance. | SMA Connector J2 provides means to connect the PLL CP output to the tuning port (VTUNE) when the EV1HMC8362LP6G and EV1HMC8364LP6G are used with an optional PLL evaluation board. J2 can also be used to manually tune the VCO within its band when evaluating the open-loop VCO performance. | ||
- | ===DEFAULT CONFIGURATION=== | + | ====Default Configuration==== |
All components necessary for local oscillator generation are inserted on the EV1HMC8362LP6G and EV1HMC8364LP6G boards. | All components necessary for local oscillator generation are inserted on the EV1HMC8362LP6G and EV1HMC8364LP6G boards. | ||
- | ====EVALUATION BOARD SOFTWARE==== | + | =====Evaluation Board Software===== |
- | ===SOFTWARE=== | + | ====Software==== |
Currently there is no software available for the EV1HMC8362LP6G and EV1HMC8364LP6G because they can be evaluated without the use of software. However, the EV1HMC8362LP6G and EV1HMC8364LP6G are configured in a manner that allows use of a Linduino, Arduino Uno, or similar microcontroller board, which may be beneficial for users needing to develop and test switching algorithms for their application. | Currently there is no software available for the EV1HMC8362LP6G and EV1HMC8364LP6G because they can be evaluated without the use of software. However, the EV1HMC8362LP6G and EV1HMC8364LP6G are configured in a manner that allows use of a Linduino, Arduino Uno, or similar microcontroller board, which may be beneficial for users needing to develop and test switching algorithms for their application. | ||
To connect the Arduino Uno microcontroller to the EV1HMC8362LP6G or EV1HMC8364LP6G, | To connect the Arduino Uno microcontroller to the EV1HMC8362LP6G or EV1HMC8364LP6G, | ||
- | ====EVALUATION AND TEST==== | + | =====Evaluation and Test===== |
To configure the EV1HMC8362LP6G and EV1HMC8364LP6G for the first time, follow Step 1 through Step 6 outlined in the Evaluation Board Setup Procedure section. | To configure the EV1HMC8362LP6G and EV1HMC8364LP6G for the first time, follow Step 1 through Step 6 outlined in the Evaluation Board Setup Procedure section. | ||
The frequency vs. tune voltage listed in the following steps are specific to the EV1HMC8362LP6G, | The frequency vs. tune voltage listed in the following steps are specific to the EV1HMC8362LP6G, | ||
- | 1. Enable the variable power supply and adjust the tuning voltage to 8.45 V. | + | - Enable the variable power supply and adjust the tuning voltage to 8.45 V. |
- | 2. If the EV1HMC8362LP6G is configured correctly, a signal at approximately 13.5 GHz with approximately 0 dBm to 2 dBm of output power appears on a spectrum analyzer or signal source analyzer. Refer to Figure 4. | + | |
- | 3. Remove the bias for the buffer amplifier (VCB), which results in the output power decreasing by approximately 28 dBm. Refer to Figure 5. | + | |
- | 4. Finally, use the signal source analyzer to measure the phase noise. Refer to Figure 6. | + | |
+ | {{ : | ||
+ | Figure 3. EV1HMC8362LP6G, | ||
+ | {{ : | ||
+ | Figure 4. EV1HMC8362LP6G, | ||
+ | {{ : | ||
+ | Figure 5. EV1HMC8362LP6G Phase Noise at RF1, VCO Band 1, VTUNE = 8.45 V, 13.5 GHz | ||
+ | =====Schematics, | ||
+ | ====EV1HMC8362LP6G==== | ||
+ | * {{ : | ||
+ | * {{ : | ||
+ | ====EV1HMC8364LP6G==== | ||
+ | * {{ : | ||
+ | * {{ : |