This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
eval:ad9625 [30 Jan 2015 15:54] – [FEATURES] Ian Beavers | eval:ad9625 [08 Feb 2019 09:20] (current) – updated schematic file Patrick Errgy Pasaquian | ||
---|---|---|---|
Line 14: | Line 14: | ||
* SPI interface for setup and control | * SPI interface for setup and control | ||
* Balun input drive option | * Balun input drive option | ||
- | * On-board LDO regulator | + | * On-board |
* VisualAnalog® and SPI controller software interfaces | * VisualAnalog® and SPI controller software interfaces | ||
- | {{resources: | + | {{ :resources:eval:user-guides: |
<WRAP centeralign> | <WRAP centeralign> | ||
//Figure 1. AD9625 Evaluation Board Connection—[[adi> | //Figure 1. AD9625 Evaluation Board Connection—[[adi> | ||
</ | </ | ||
- | ==== REQUIRED | + | ==== REQUIRED |
- | * AC to 12V DC power supplies (2) | + | * AC to 12V DC power supply |
* Analog signal source, anti-aliasing filter and SMA cable. | * Analog signal source, anti-aliasing filter and SMA cable. | ||
* Analog Clock source and SMA cable. | * Analog Clock source and SMA cable. | ||
Line 32: | Line 32: | ||
====DESIGN AND INTEGRATION FILES==== | ====DESIGN AND INTEGRATION FILES==== | ||
- | * Schematic, | + | * Schematics: |
- | * Board File, | + | * RevA: {{: |
- | * BOM, | + | * RevB: {{ : |
+ | * Board File: | ||
+ | * RevA: {{: | ||
+ | * RevB: {{ : | ||
+ | * BOM: | ||
+ | * RevA: {{: | ||
+ | * RevB: {{ : | ||
* Analog Input S-Parameter Model, {{: | * Analog Input S-Parameter Model, {{: | ||
====HELPFUL DOCUMENTS==== | ====HELPFUL DOCUMENTS==== | ||
* AD9625 data sheet http:// | * AD9625 data sheet http:// | ||
- | * AD9625 Evaluation Board "Quick Start User Guide", {{: | + | * AD9625 Evaluation Board "Quick Start User Guide": |
+ | * RevA: {{: | ||
+ | * RevB: {{ : | ||
* * High Speed ADC Capture Evaluation Kit Rev E (HSC-ADC-EVALEZ) http:// | * * High Speed ADC Capture Evaluation Kit Rev E (HSC-ADC-EVALEZ) http:// | ||
* [[adi> | * [[adi> | ||
Line 44: | Line 52: | ||
* [[adi> | * [[adi> | ||
* [[adi> | * [[adi> | ||
+ | * Power by Linear Journal: " | ||
====EASY START Steps==== | ====EASY START Steps==== | ||
Line 52: | Line 61: | ||
1. Download and Install VisualAnalog. For the latest updates to the software, check the Analog Devices website at [[adi> | 1. Download and Install VisualAnalog. For the latest updates to the software, check the Analog Devices website at [[adi> | ||
- | 2. Connect the ADC capture | + | 2. Connect the ADC evaluation |
3. Connect the provided USB cable to the ADC capture board and to an available USB port on the computer. | 3. Connect the provided USB cable to the ADC capture board and to an available USB port on the computer. |