Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
Next revision
Previous revision
eval:ad9625 [30 Jan 2015 15:54]
Ian Beavers [FEATURES]
eval:ad9625 [08 Feb 2019 09:20]
Patrick Errgy Pasaquian updated schematic file
Line 14: Line 14:
   * SPI interface for setup and control   * SPI interface for setup and control
   * Balun input drive option   * Balun input drive option
-  * On-board LDO regulator ​needing a single external 12V, 3 A dc supply+  * On-board ​Power Supply options: Switcher only, Switcher + LC Filter, Switcher + LDO regulator
   * VisualAnalog® and SPI controller software interfaces   * VisualAnalog® and SPI controller software interfaces
  
-{{resources:​quick-start:a02cdd9c483783f2c1fd59d63c34fd2b_media_900x415.jpg|}}+{{ :resources:eval:user-guides:​ad9625:ad9625_board_with_capture_board.png?​nolink&​900 ​|}}
 <WRAP centeralign>​ <WRAP centeralign>​
 //Figure 1. AD9625 Evaluation Board Connection—[[adi>​AD9625|AD9625-2.5EBZ]] (on Left) and [[adi>​hsadcevalboard|HSC-ADC-EVALEZ]] (on Right)// //Figure 1. AD9625 Evaluation Board Connection—[[adi>​AD9625|AD9625-2.5EBZ]] (on Left) and [[adi>​hsadcevalboard|HSC-ADC-EVALEZ]] (on Right)//
 </​WRAP>​ </​WRAP>​
  
-==== REQUIRED ​HADWARE ​==== +==== REQUIRED ​HARDWARE ​==== 
-  * AC to 12V DC power supplies (2)+  * AC to 12V DC power supply
   * Analog signal source, anti-aliasing filter and SMA cable.   * Analog signal source, anti-aliasing filter and SMA cable.
   * Analog Clock source and SMA cable.   * Analog Clock source and SMA cable.
Line 32: Line 32:
  
 ====DESIGN AND INTEGRATION FILES==== ====DESIGN AND INTEGRATION FILES====
-  * Schematic,  ​{{:​resources:​eval:​9625ce04c1_sch.pdf|}} +  * Schematics: ​   
-  * Board File ​{{:​resources:​eval:​9625ce04c1-1-24.zip|}} +    * RevA: {{:​resources:​eval:​9625ce04c1_sch.pdf|}}  
-  * BOM ​{{:​resources:​9625CE04C1_BOM-NEW04222014.xls|}}+    * RevB: {{ :​resources:​eval:​user-guides:​ad9625:​ad9625_demo_board_revb.pdf |}} 
 +  * Board File  
 +    * RevA: {{:​resources:​eval:​9625ce04c1-1-24.zip|}} 
 +    * RevB: {{ :​resources:​eval:​user-guides:​ad9625:​ad9625_board_layout_revb_.zip |}} 
 +  * BOM  
 +    * RevA: {{:​resources:​9625CE04C1_BOM-NEW04222014.xls|}} 
 +    * RevB: {{ :​eval:​ad9625_board_bom_revb_.xls |}}
   * Analog Input S-Parameter Model, {{:​resources:​AD9625_input_model.zip|}}   * Analog Input S-Parameter Model, {{:​resources:​AD9625_input_model.zip|}}
 ====HELPFUL DOCUMENTS==== ====HELPFUL DOCUMENTS====
   * AD9625 data sheet http://​www.analog.com/​AD9625   * AD9625 data sheet http://​www.analog.com/​AD9625
-  * AD9625 Evaluation Board "Quick Start User Guide"{{:​resources:​quick-start:​ quickstartguide_ad9625_2p5.docx|}}+  * AD9625 Evaluation Board "Quick Start User Guide"
 +    * RevA: {{:​resources:​quick-start:​ quickstartguide_ad9625_2p5.docx|}} 
 +    * RevB: {{ :​resources:​eval:​user-guides:​ad9625:​quickstartguide_ad9625_2p5_revb_.docx |}}
   *   * High Speed ADC Capture Evaluation Kit Rev E (HSC-ADC-EVALEZ) http://​wiki.analog.com/​resources/​eval/​hsc-adc-evale   *   * High Speed ADC Capture Evaluation Kit Rev E (HSC-ADC-EVALEZ) http://​wiki.analog.com/​resources/​eval/​hsc-adc-evale
   * [[adi>​an-905|AN-905 Application Note]], //​VisualAnalog Converter Evaluation Tool Version 1.0 User Manual// ​   * [[adi>​an-905|AN-905 Application Note]], //​VisualAnalog Converter Evaluation Tool Version 1.0 User Manual// ​
Line 44: Line 52:
   * [[adi>​an-877|AN-877 Application Note]], //​Interfacing to High Speed ADCs via SPI//   * [[adi>​an-877|AN-877 Application Note]], //​Interfacing to High Speed ADCs via SPI//
   * [[adi>​an-835|AN-835 Application Note]], //​Understanding ADC Testing and Evaluation//​   * [[adi>​an-835|AN-835 Application Note]], //​Understanding ADC Testing and Evaluation//​
 +  * Power by Linear Journal: "​Silent Switcher uModule Regulators Quietly Power GSPS Sampling ADC in Half the Space" https://​www.analog.com/​media/​en/​technical-documentation/​lt-journal-article/​PbLJournal-V1N3-2018-08-RevA.pdf
  
 ====EASY START Steps==== ====EASY START Steps====
Line 52: Line 61:
 1. Download and Install VisualAnalog. For the latest updates to the software, check the Analog Devices website at [[adi>​hsadcevalboard|High Speed ADC Eval Boards]]. 1. Download and Install VisualAnalog. For the latest updates to the software, check the Analog Devices website at [[adi>​hsadcevalboard|High Speed ADC Eval Boards]].
  
-2. Connect the ADC capture ​board to the ADC evaluation ​board. ​If an adapter is required, insert ​the adapter ​between ​the ADC evaluation ​board and the ADC capture board.+2. Connect the ADC evaluation ​board to the ADC capture ​board. ​Insert ​the 12V wallwart ​adapter ​to the ADC capture ​board. The ADC capture board will provide power to the ADC evaluation board through the FMC connector.
    
 3. Connect the provided USB cable to the ADC capture board and to an available USB port on the computer. 3. Connect the provided USB cable to the ADC capture board and to an available USB port on the computer.
eval/ad9625.txt · Last modified: 08 Feb 2019 09:20 by Patrick Errgy Pasaquian