The purpose of this activity is to investigate the collector current, IC vs. collector voltage, VCE characteristics of the BJT. The kit of parts you have for the EPS system module will contain a number of transistors ( both NPN and PNP devices of various types ).
The variable analog outputs supplied by the Discovery hardware are voltages. The BJT collector current is controlled by the base current. The AWG output voltage must be converted into a suitable current to drive the base terminal of the device under investigation. A simple resistor can be used to convert a voltage into a current, as shown in figure 1. However, only if the voltage across the resistor is known or controlled in some way. In this simple circuit, the base current IB = (VAWG2 - VBE)/100KΩ. We can set VAWG2 to known values but we don't know the exact value of VBE. We can of course remove an estimate of the VBE mathematically. This is still only an estimate.
Figure 1 NPN IC vs. VCE characteristic curve measurements
Analog Discovery Lab Instrument Hardware
Solder-less Breadboard
1 - 100KΩ Resistor
1 - 100Ω Resistor
1 - small signal NPN transistor (2N3904)
Build the simple characteristic curve measurement circuit shown in figure 1. The green boxes indicate where to connect the Discovery Board.
Using the custom waveform editor in the Waveforms AWG tool, construct a stair-step waveform with 5 levels for AWG2. Be sure to reset so that you are starting with flat line at 0%. First set the type to constant. Then with start set to 0%, length set to 20% and offset set to -100% click on generate function. There should now be a line at -100% from 0 to 20%. Next change the start to 20% and the offset to -50% and then click on generate function again. There should now be a line at -50% from 20% to 40%. Next set the offset to +50% and the start to 60% and then click on generate function again. There should now be a line at 0% from 40% to 60% and a line at 50% from 60% to 80%. Finally set the offset to 100% and start to 80% and click on generate function one last time. There should now be a final line at 100% from 80% to 100%. Click on save and your new waveform should be in channel 2. Now at this point set the frequency to 40Hz, the amplitude to 2 V and the offset to 2.6 V. The waveform in the display should start at 0.6V and increase in 1 V increments to 4.6 V (0.6, 1.6, 2.6, 3.6, 4.6) Each step should be 5 mSec long for a total of 25 mSec. In AWG channel 1 configure a triangle wave with an amplitude of 2.5 V and an offset of 2.5V (wave should swing from 0 to 5V). Set the frequency to 200 Hz ( 5 times the 40 Hz of channel 2). Comparing the waveforms in channel 1 and channel 2, the triangle wave in channel 1 should go through one cycle from 0 to 5 V and back to zero during the time of one step in the waveform in channel 2. It will probably be necessary to set the phase of channel 1 to 270 degrees to make them line up in this way.
You may wish to export your newly created stair-step waveform to a .csv file for future use.
The 1 V steps in the voltage driving the 100 KΩ base resistor will produce approximately 1 V/100 KΩ or 10 uA steps in the base current. Using the scope in XY mode plot channel 1 on the horizontal axis (VCE) and channel 2 (IC) on the vertical axis. You should see a set of 5 curves of IC vs. VCE, one for each of the 5 different base current levels. These base current levels should be approximately 0, 10uA, 20uA, 30uA and 40uA. It may be necessary to slightly adjust the 0.6V offset level of the first step of AWG2 up or down slightly to insure it is right at the initial turn on value ( IB=0 and IC=0) of the transistor you are testing.
To measure the PNP device, alter the characteristic curve measurement circuit as shown in figure 2. The connections are not very different but the polarity of the voltage waveforms generated by AWG1 and AWG2 must now be negative with respect to ground.
You can use the same 5 step staircase waveform you generated for the NPN device to drive the base current for the PNP device. You will need to set the amplitude to 2 V again but set the offset to -2.6 V. The waveform in the display should now start at -0.6 V and decrease in 1 V increments to -4.6 V (-0.6, -1.6, -2.6, -3.6, -4.6) Each step should be 5 mSec long for a total of 25 mSec. In AWG channel 1 change the triangle wave with an amplitude of 2.5 V to an offset of -2.5V (wave should swing from 0 to -5V). Check to make sure that the triangle wave in channel 1 goes through one cycle from 0 to -5 V and back to zero during the time of one step in the waveform in channel 2. Change the phase of channel 1 if necessary.
Figure 2 PNP IC vs. VCE characteristic curve measurements
For Further Reading:
Waveform file:
5_steps.csv
Return to EPS Lab Activity Table of Contents.