This is an old revision of the document!
The schematic of a typical common-emitter amplifier is shown in figure 1. Capacitors CB and CC are used to block the amplifier DC bias point from the input and output (AC coupling). Capacitor CE is an AC bypass capacitor used to establish a low frequency AC ground at the emitter of Q1. Miller capacitor CF is a small capacitance that will be used to control the high frequency 3-dB response of the amplifier.
Figure 1: Common-emitter BJT amplifier.
For this section, assume that CB = CC = CE = 1 Farad and CF = CΠ = Cµ = 0. You can find the DC collector current (IC) and the resistor values following the analysis provided in your text book. Since the topology and the requirements might be slightly different than in the text, you will need to make minor modifications to the design procedure and equations.
Figure 2 shows the low-frequency small-signal equivalent circuit of the amplifier. Note that CF is ignored since it is assumed that its impedance at these frequencies is very high. RB is the parallel combination of RB1 and RB2.
Figure 2: Low-frequency equivalent circuit.
Using short-circuit time constant analysis, the lower 3-dB frequency (ωL) can be found as:
Where
Figure 3 shows the high-frequency small-signal equivalent circuit of the amplifier. At high frequencies, CB, CC and CE can be replaced with short circuits since their impedance becomes very small compared to RS, RL and RE.
Figure 3: High-frequency equivalent circuit.
The higher 3-dB frequency (ωH) can be derived as:
Where
Thus, if we assume that the common-emitter amplifier is properly characterized by these dominant low and high frequency poles, then the frequency response of the amplifier can be approximated by:
Assuming CB = CC = CE = 1 Farad and CF = CΠ = Cµ = 0, and using a 2N3904 transistor, design a common-emitter amplifier with the following specifications:
VCC = 5 V
RS = 50Ω
RL = 1 kΩ
RIN > 250
Isupply < 8mA
AV > 50
peak-to-peak unclipped output swing > 3 V
1. Show all your calculations, design procedure, and final component values.
2. Verify your results using the LTSpice circuit simulator. Submit all necessary simulation plots showing that the specifications are satisfied. Also provide the circuit schematic with DC bias points annotated.
3. Using the LTSpice simulator, find the higher 3-dB frequency (fH) while CF = 0.
4. Determine Cp, Cµ and rb of the transistor from the simulated operating point data, (refer to your simulator's documentation on how to obtain operating point data). Calculate fH using the equation from section 1.3 and compare it with the simulation result obtained in Step 3. Remember that the equation gives you the radian frequency and you need to convert to Hz.
5. Calculate the value of CF to have fH = 50 kHz. Simulate the circuit to verify your result, and adjust the value of CF if necessary.
6. Calculate CB, CC, CE to have fL = 500 Hz. Simulate the circuit to verify your result, and adjust the values of capacitors if necessary.
7. Be prepared to discuss your design at the beginning of the lab period with your TA.
The objective of this section of the Lab Activity is to validate your pre-Lab design values by building the actual circuit and measuring its frequency response performance.
ADALM2000 Active Learning Module
Solder-less breadboard
6 - Resistors various values from the ADALP2000 Analog Parts Kit
4 - Capacitors various values from the ADALP2000 Analog Parts Kit
1 - small signal NPN transistor (2N3904)
Note on the source resistor RS and the AWG output of the ADALM2000. The AWG output has a 50 Ω series output resistance and you will need to include it along with the external resistance in series with its output. Also because of the relatively high gain of your design you will need an input signal with a small amplitude of around 100mV peak-to-peak. Rather than turning down the AWG in software it would be better from a noise point of view to insert a resistor voltage divider between the AWG output and your circuit input to attenuate the signal. Using something like that shown in figure 4 will provide both an attenuation factor of 1/8 and a 60Ω equivalent source resistance. Other combinations of resistor values are of course also possible based on what you have available.
Figure 4 Signal attenuator with 60Ω source resistance
Construct the circuit on your breadboard.
Figure 5 Common Emitter BJT amplifier breadboard connection
1. Construct the amplifier, based on the schematic in figure 1, you designed in the pre-lab. Based on your design values from the pre-Lab, use the closest standard value from your kit. Remember that you can combine the standard values in series or parallel to get a combined value closer to your design number.
2. Check your DC operating point by measuring IC, VE, VC and VB. If any DC bias value is significantly different than the one obtained from simulation, modify your circuit to get the desired DC bias before moving onto the next step.
3. Measure Isupply.
4. Use the Network analyzer instrument in the Scopy software to obtain the magnitude of the frequency response of the amplifier from 10 Hz to as high as 5 MHz and determine the lower and upper 3-dB frequencies fL and fH.
5. At mid-band frequencies, measure AV, RIN, and ROUT.
6. Measure the maximum un-clipped output signal amplitude.
7. Prepare a data sheet showing your simulated and measured values.
8. Be prepared to discuss your experiment with your TA. Have your lab data sheet checked off by your TA before submitting the lab report.
Figure 6 Scopy Network Analyzer plot with CF = 0
Figure 7 Scopy Oscilloscope plot with CF = 0 at frequency = 500Hz
For further experimentation replace each capacitor with ones that are factors of 2 and 10 larger and smaller than your design values and re-measure the response curve with the Network Analyzer instrument. Do this to only one capacitor at a time to observe its individual effect on the response. Explain the changes in the response that you see.
Resources
Return to Lab Activity Table of Contents