This is an old revision of the document!
Linux Industrial I/O Subsystem
IIO Overview
The overall aim is to fill the gap between the somewhat similar hwmon and input subsystems.
Hwmon is very much directed at low sample rate sensors used in applications such as fan speed control and temperature measurement.
Input is, as it's name suggests focused on human interaction input devices.:
Keyboard
Mouse
Touch Screen
Joystick
A typical device falling into the IIO category would be connected via
SPI or
I2C.
However typical
DMA operated devices such as ones connected to a high speed synchronous serial (McBSP,
SPORT) or high speed synchronous parallel (EPI,
PPI) peripherals are also subject to this subsystem.
Since latter ones unlike
SPI or
I2C are not generally abstracted by Linux bus drivers they are subject to processor platform dependent implementations.
IIO Subsystem Overview
Functionality of IIO
A given device may have one or more event channel. These events are turned on or off (if possible) via sysfs interfaces.
Hardware ring buffer support
Some recent sensors have included fifo / ring buffers on the sensor chip.
These greatly reduce the load on the host CPU by buffering relatively large numbers of data samples based on an internal sampling clock.
Each ring buffer typically has an event chrdev (similar to the more general ones above) to pass on events such as buffer 50% full and an access chrdev via which the raw data it self may be read back.
Trigger and software ring buffer support
Trigger and software ring buffer support
In many data analysis applications it is useful to be able to capture data based on some external signal (trigger).
These triggers might be a
data ready signal
gpio line connected to some external system
on processor periodic interrupt.
User space reading a specific file in sysfs.
A single trigger many initialize data capture or reading from a number of sensors.
These triggers are used in iio to fill software ring buffers acting in a very similar fashion to the hardware buffers described above.
Triggers can be completely unrelated to the sensor itself
Standalone trigger drivers
name | description |
iio-trig-gpio | Provides support for using GPIO pins as IIO triggers. |
iio-trig-rtc | Provides support for using periodic capable real time clocks as IIO triggers. |
iio-trig-sysfs | Provides support for using SYSFS entry as IIO triggers. |
iio-trig-bfin-timer | Provides support for using a Blackfin timer as IIO triggers. |
IIO Ring Buffer
Pointers