The ADIS16227 iSensor® is a complete vibration sensing system that combines wide bandwidth, triaxial acceleration sensing with advanced time domain and frequency domain signal processing. Time domain signal processing includes a programmable decimation filter and selectable windowing function. Frequency domain processing includes a 512 point, real-valued FFT for each axis, along with FFT averaging, which reduces the noise floor variation for finer resolution. The 16-record FFT storage system offers users the ability to track changes over time and to capture FFTs with multiple decimation filter settings.
The goal of this project (Microcontroller No-OS) is to be able to provide reference projects for lower end processors, which can't run Linux, or aren't running a specific operating system, to help those customers using microcontrollers with ADI parts. Here you can find a generic driver which can be used as a base for any microcontroller platform and also specific drivers for Renesas platforms.
HW Platform(s):
The driver contains two parts:
The Communication Driver has a standard interface, so the ADIS16227 driver can be used exactly as it is provided. There are three functions which are called by the ADIS16227 driver:
Driver architecture
The implementation of these three functions depends on the used microcontroller.
The following functions are implemented in this version of ADIS16227 driver:
| Function | Description |
|---|---|
| unsigned short ADIS16227_GetRegister16Value(unsigned char registerAddress) | Reads the value of a register. |
| void ADIS16227_SetRegister8Value(unsigned char registerAddress, unsigned char registerValue) | Writes 1 byte into a register. |
| void ADIS16227_SetRegister16Value(unsigned char registerAddress, unsigned short registerValue) | Writes 2 bytes into a register. |
| unsigned char ADIS16227_Init(void) | Initializes the SPI and checks if the ADIS16227 part is present. |
| void ADIS16227_ConfigCapture(unsigned char window, unsigned char sampleRate, unsigned char pwrDwn, unsigned char range, unsigned char mode) | Configures the ADIS16227_REC_CTRL register. |
| unsigned char ADIS16227_DataReady(void) | Reads the value of the “Data ready/busy” bit (DIAG_STAT register). |
| void ADIS16227_Capture(void) | Initiates a manual data capture and wait until the process is finished. |
| void ADIS16227_GetBuffers(unsigned short* x, unsigned short* y, unsigned short* z, unsigned short samplesNumber) | Reads “samplesNumber” samples from each axis's buffer. |
| unsigned short ADIS16227_GetPowerSupplyInfo(void) | Reads the power supply voltage and returns the data in mV. |
| char ADIS16227_GetTemperatureInfo(void) | Reads the internal temperature and returns the data in degrees Celsius. |
This section contains a description of the steps required to run the ADIS16227 demonstration project on a Renesas RL78G13 platform.
An ADIS16227/PCBZ board has to be interfaced with the Renesas Demonstration Kit (RDK) for RL78G13:
ADIS16227/PCBZ J1 connector Pin 3 (CS) → YRDKRL78G13 PMOD1 connector Pin 1 ADIS16227/PCBZ J1 connector Pin 6 (MOSI) → YRDKRL78G13 PMOD1 connector Pin 2 ADIS16227/PCBZ J1 connector Pin 4 (MISO) → YRDKRL78G13 PMOD1 connector Pin 3 ADIS16227/PCBZ J1 connector Pin 2 (SCLK) → YRDKRL78G13 PMOD1 connector Pin 4 ADIS16227/PCBZ J1 connector Pin 1 (RST) → YRDKRL78G13 PMOD1 connector Pin 8 ADIS16227/PCBZ J1 connector Pin 7 (GND) → YRDKRL78G13 PMOD1 connector Pin 11 ADIS16227/PCBZ J1 connector Pin 10 (VCC) → YRDKRL78G13 PMOD1 connector Pin 12
With the Applilet3 for RL78G13 tool the following peripherals have to be configured:
Choose to generate the Transmit/receive function for the CSI10 and configure the interface with the following settings:
Configure TM00 as an interval timer:
Disable the watchdog timer:
The reference project runs an offset correction operation, configures the REC_CTRL register and initiates a Manual Time recording. After the process is finished on the LCD are displayed the internal temperature, the power supply voltage and the first value of each axis's buffer.
This section presents the steps for developing a software application that will run on the Renesas Demo Kit for RL78G13 for controlling and monitoring the operation of the ADI part.
Two software applications have to be used: Applilet3 for RL78G13 (a tool that automatically generates device drivers for MCU peripheral functions) and IAR Embedded Workbench for Renesas RL78 (the integrated development environment).
This section contains a description of the steps required to run the ADIS16227 demonstration project on a Renesas RX62N platform.
An ADIS16227/PCBZ board has to be interfaced with the Renesas Demonstration Kit (RDK) for RX62N:
ADIS16227/PCBZ J1 connector Pin 3 (CS) → YRDKRX62N J8 connector Pin 15 ADIS16227/PCBZ J1 connector Pin 6 (MOSI) → YRDKRX62N J8 connector Pin 19 ADIS16227/PCBZ J1 connector Pin 4 (MISO) → YRDKRX62N J8 connector Pin 22 ADIS16227/PCBZ J1 connector Pin 2 (SCLK) → YRDKRX62N J8 connector Pin 20 ADIS16227/PCBZ J1 connector Pin 1 (RST) → YRDKRX62N JN1 connector Pin 16 ADIS16227/PCBZ J1 connector Pin 7 (GND) → YRDKRX62N J8 connector Pin 4 ADIS16227/PCBZ J1 connector Pin 10 (VCC) → YRDKRX62N J8 connector Pin 3
The reference project runs an offset correction operation, configures the REC_CTRL register and initiates a Manual Time recording. After the process is finished on the LCD are displayed the internal temperature, the power supply voltage and the first value of each axis's buffer.
This section presents the steps for developing a software application that will run on the Renesas Demo Kit for RX62N for controlling and monitoring the operation of the ADI part.