This shows you the differences between two versions of the page.
Next revisionBoth sides next revision | |||
resources:tools-software:uc-drivers:renesas:adf7023 [09 May 2013 17:48] – created Dragos Bogdan | resources:tools-software:uc-drivers:renesas:adf7023 [23 May 2013 10:31] – [Required Software] Lucian Sin | ||
---|---|---|---|
Line 21: | Line 21: | ||
==== Required Software ==== | ==== Required Software ==== | ||
* [[http:// | * [[http:// | ||
- | * To run the ADF7023 demonstration project | + | * The ADF7023 demonstration project |
+ | <WRAP round info 80%> | ||
+ | The ADF7023 demonstration project for the Renesas RL78G14 platform consists of three parts: the **ADF7023 Driver**, | ||
+ | |||
+ | All three parts have to be downloaded. | ||
+ | </ | ||
==== Hardware Setup ==== | ==== Hardware Setup ==== | ||
A PmodAD6 has to be connected to the PMOD1 connector (see image below). | A PmodAD6 has to be connected to the PMOD1 connector (see image below). |