This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:tools-software:uc-drivers:renesas:adf4360 [28 Mar 2012 09:56] – Added RL78G13 driver. Dragos Bogdan | resources:tools-software:uc-drivers:renesas:adf4360 [25 Jan 2021 05:24] (current) – update renesas links after their web site update Robin Getz | ||
---|---|---|---|
Line 14: | Line 14: | ||
===== Evaluation Boards ===== | ===== Evaluation Boards ===== | ||
- | * [[adi> | + | * [[adi>EVAL-ADF4360-0 | EVAL-ADF4360-0EBZ1]] |
- | * [[adi> | + | * [[adi> |
- | * [[adi> | + | * [[adi> |
- | * [[adi> | + | * [[adi>EVAL-ADF4360-3 | EVAL-ADF4360-3EBZ1]] |
- | * [[adi> | + | * [[adi> |
- | * [[adi> | + | * [[adi> |
- | * [[adi> | + | * [[adi> |
- | * [[adi> | + | * [[adi>EVAL-ADF4360-7 | EVAL-ADF4360-7EBZ1]] |
- | * [[adi> | + | * [[adi>EVAL-ADF4360-8 | EVAL-ADF4360-8EBZ1]] |
- | * [[adi> | + | * [[adi>EVAL-ADF4360-9 | EVAL-ADF4360-9EBZ1]] |
===== Overview ===== | ===== Overview ===== | ||
Line 45: | Line 45: | ||
* [[adi> | * [[adi> | ||
* [[adi> | * [[adi> | ||
- | * [[adi> | + | * [[adi> |
- | * [[http://am.renesas.com/ | + | * [[https://www.renesas.com/us/en/products/microcontrollers-microprocessors/rl78-low-power-8-16-bit-mcus/yrdkrl78g13-yrdkrl78g13-demonstration-kit-rl78g13|Renesas Demo Kit for RL78G13 (Renesas)]] |
+ | * [[https://www.renesas.com/ | ||
===== Driver Description ===== | ===== Driver Description ===== | ||
Line 67: | Line 68: | ||
The following functions are implemented in this version of ADF4360 driver: | The following functions are implemented in this version of ADF4360 driver: | ||
^ Function | ^ Function | ||
- | | void ADF4360_Write3Bytes(unsigned | + | | unsigned char ADF4360_Init(unsigned char adf4360Version) | Initialize the device. | |
- | | unsigned char ADF4360_Init(void) | Initializes | + | | void ADF4360_Write(unsigned |
+ | | void ADF4360_Power(unsigned char powerMode) | Powers down or powers up the device. | | ||
+ | | unsigned long long ADF4360_SetFrequency(unsigned long long frequency) | Sets the ADF4360 frequency. | | ||
===== Downloads ===== | ===== Downloads ===== | ||
Line 79: | Line 82: | ||
==== Required Hardware ==== | ==== Required Hardware ==== | ||
- | * [[http://am.renesas.com/ | + | * [[https://www.renesas.com/ |
* [[adi> | * [[adi> | ||
* [[adi> | * [[adi> | ||
Line 94: | Line 97: | ||
==== Required Software ==== | ==== Required Software ==== | ||
* [[http:// | * [[http:// | ||
- | * [[http:// | ||
==== Hardware Setup ==== | ==== Hardware Setup ==== | ||
Line 119: | Line 121: | ||
{{ : | {{ : | ||
- | ==== Software Setup ==== | + | ==== Reference Project Overview |
- | With the // | + | In this example |
- | === CSI10 (Clocked Serial Interface 10) – For the ADF4360 part and the ST7579 LCD === | ||
- | Choose to generate the Transmit/ | ||
- | * Transfer mode setting: //**Single transfer mode**// | ||
- | * Data length setting : //**8 bits**// | ||
- | * Transfer direction setting: //**MSB**// | ||
- | * Specification of data timing: //**Type 1**// | ||
- | * Transfer rate setting – Clock mode: // | ||
- | * Transfer rate setting – Baudrate: // | ||
- | * Interrupt setting – Transfer interrupt priority (INTCSI10): //**Low**// | ||
- | * Uncheck the callback functions. | ||
- | === TM00 (Timer 00) – For the DelayMs() function === | + | {{ :resources: |
- | Configure TM00 as an interval timer: | + | |
- | * Interval timer setting | + | |
- | * Interval timer setting | + | |
- | * Interrupt setting - Uncheck // End of timer channel 0 count, generate an interrupt (INTM00)// | + | |
- | + | ||
- | === Watchdog Timer === | + | |
- | Disable the watchdog timer: | + | |
- | * Choose for the Watchdog timer operation setting: // | + | |
- | + | ||
- | ==== Reference Project Overview ==== | + | |
- | In this example, two values are loaded into R and N Counters and the MUXOUT is configured to be connected to the R Divider output. | + | |
==== Software Project Tutorial ==== | ==== Software Project Tutorial ==== | ||
- | {{page>rl78g13_software_tutorial}} | + | {{page>rl78g13_software_tutorial_without_applilet3}} |
====== Renesas RX62N Quick Start Guide ====== | ====== Renesas RX62N Quick Start Guide ====== | ||
Line 153: | Line 134: | ||
==== Required Hardware ==== | ==== Required Hardware ==== | ||
- | * [[http://am.renesas.com/ | + | * [[https://www.renesas.com/ |
* [[adi> | * [[adi> | ||
* [[adi> | * [[adi> | ||
Line 166: | Line 147: | ||
==== Required Software ==== | ==== Required Software ==== | ||
- | * [[http:// | + | * [[https:// |
- | * [[http://am.renesas.com/ | + | * [[https://www.renesas.com/ |
==== Hardware Setup ==== | ==== Hardware Setup ==== | ||
Line 198: | Line 179: | ||
==== Software Project Setup ==== | ==== Software Project Setup ==== | ||
{{page> | {{page> | ||
+ | |||
+ | ====== More information ====== | ||
+ | {{page> |