This is an old revision of the document!
The AD7991/AD7995/AD7999 are 12-/10-/8-bit, low power, successive approximation ADCs with an I2C®-compatible interface. Each part operates from a single 2.7 V to 5.5 V power supply and features a 1 μs conversion time.
Each AD7991/AD7995/AD7999 provides a 2-wire serial interface compatible with I2C interfaces. The AD7991 and AD7995 come in two versions and each version has an individual I2C address (see Table 8 of data sheet for address and part number selection). This allows two of the same devices to be connected to the same I2C bus. Both versions support standard, fast, and high speed I2C interface modes. The AD7999 comes in one version.
The AD7991/AD7995/AD7999 normally remain in a shutdown state, powering up only for conversions. The conversion process is controlled by a command mode, during which each I2C read operation initiates a conversion and returns the result over the I2C bus.
When four channels are used as analog inputs, the reference for the part is taken from VDD; this allows the widest dynamic input range to the ADC. Therefore, the analog input range to the ADC is 0 V to VDD. An external reference, applied through the VIN3/VREF input, can also be used with this part.
The goal of this project (Microcontroller No-OS) is to be able to provide reference projects for lower end processors, which can't run Linux, or aren't running a specific operating system, to help those customers using microcontrollers with ADI parts. Here you can find a generic driver which can be used as a base for any microcontroller platform and also specific drivers for different microcontroller platforms.
The driver contains two parts:
The Communication Driver has a standard interface, so the AD799x driver can be used exactly as it is provided.
There are three functions which are called by the AD799x driver:
I2C driver architecture
The following functions are implemented in this version of AD799x driver:
Function | Description |
---|---|
char AD799x_Init(char partNumber, char deviceVersion) | Initializes I2C. |
void AD799x_SetConfigurationReg(unsigned char registerValue) | Writes data into the Configuration Register. |
void AD799x_GetConversionResult(short* convValue, char* channel) | Reads the High byte and the Low byte of the conversion. |
float AD799x_ConvertToVolts(short rawSample, float vRef) | Converts a raw sample to volts. |
This section contains a description of the steps required to run the AD7991 demonstration project on a Renesas RL78G13 platform using the PmodAD2.
A PmodAD2 has to be interfaced with the Renesas Demonstration Kit (RDK) for RL78G13:
PmodAD2 J1 connector Pin SCL → YRDKRL78G13 J9 connector Pin 1 PmodAD2 J1 connector Pin SDA → YRDKRL78G13 J9 connector Pin 3 PmodAD2 J1 connector Pin GND → YRDKRL78G13 J11 connector Pin 5 PmodAD2 J1 connector Pin VCC → YRDKRL78G13 J11 connector Pin 6
In the reference project the device is enabled and continuous conversions are made for all four channels. The results of the conversions are displayed on the LCD.
This section presents the steps for developing a software application that will run on the Renesas Demo Kit for RL78G13 for controlling and monitoring the operation of the ADI part.
This section contains a description of the steps required to run the AD7991 demonstration project on a Renesas RL78G14 platform using the PmodAD2.
The AD7991 demonstration project for the Renesas RL78G14 platform consists of three parts: the AD799x Driver, the PmodAD2 Demo for RL78G14 and the RL78G14 Common Drivers.
All three parts have to be downloaded.
A PmodAD2 has to be interfaced with the Renesas Demonstration Kit (RDK) for RL78G14:
PmodAD2 J1 connector Pin SCL → RDKRL78G14 J9 connector Pin 1 PmodAD2 J1 connector Pin SDA → RDKRL78G14 J9 connector Pin 3 PmodAD2 J1 connector Pin GND → RDKRL78G14 J11 connector Pin 5 PmodAD2 J1 connector Pin VCC → RDKRL78G14 J11 connector Pin 6
The reference project:
This section presents the steps for developing a software application that will run on the Renesas Demo Kit for RL78G14 for controlling and monitoring the operation of the ADI part.
This section contains a description of the steps required to run the AD7991 demonstration project on a Renesas RX62N platform using the PmodAD2.
A PmodAD2 has to be interfaced with the Renesas Demonstration Kit (RDK) for RX62N:
PmodAD2 J1 connector 1 (SCL) → YRDKRX62N J2 connector Pin 1 PmodAD2 J1 connector 3 (SDA) → YRDKRX62N J2 connector Pin 3 PmodAD2 J1 connector 5 (GND) → YRDKRX62N J8 connector Pin 4 PmodAD2 J1 connector 7 (VCC) → YRDKRX62N J8 connector Pin 3
In the reference project the device is enabled and continuous conversions are made for all four channels. The results of the conversions are displayed on the LCD.
This section presents the steps for developing a software application that will run on the Renesas Demo Kit for RX62N for controlling and monitoring the operation of the ADI part.