This shows you the differences between two versions of the page.
Next revision | Previous revision | ||
resources:tools-software:uc-drivers:renesas:ad7746 [11 May 2012 14:20] – Created Dragos Bogdan | resources:tools-software:uc-drivers:renesas:ad7746 [08 Apr 2021 16:48] (current) – link to newer project page Darius B | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== AD7746 - Microcontroller No-OS Driver ====== | ====== AD7746 - Microcontroller No-OS Driver ====== | ||
+ | |||
+ | <note important> | ||
+ | You're looking at a legacy page. A newer driver and reference project demo are available at [[resources/ | ||
+ | </ | ||
===== Supported Devices ===== | ===== Supported Devices ===== | ||
Line 11: | Line 15: | ||
===== Overview ===== | ===== Overview ===== | ||
+ | The [[adi> | ||
+ | |||
+ | The [[adi> | ||
+ | |||
+ | The parts have an on-chip temperature sensor with a resolution of 0.1°C and accuracy of ±2°C. The on-chip voltage reference and the on-chip clock generator eliminate the need for any external components in capacitive sensor applications. The parts have a standard voltage input, which together with the differential reference input allows easy interface to an external temperature sensor, such as an RTD, thermistor, or diode. | ||
+ | |||
+ | The [[adi> | ||
+ | |||
+ | == Applications == | ||
+ | Automotive, Industrial and Medical Systems for: | ||
+ | * Pressure Measurement | ||
+ | * Position Sensors | ||
+ | * Level Sensors | ||
+ | * Flowmeters | ||
+ | * Humidity Sensors | ||
+ | * Impurity Detection | ||
+ | |||
+ | {{ : | ||
+ | |||
The goal of this project (Microcontroller No-OS) is to be able to provide reference projects for lower end processors, which can't run Linux, or aren't running a specific operating system, to help those customers using microcontrollers with ADI parts. Here you can find a generic driver which can be used as a base for any microcontroller platform and also specific drivers for Renesas platforms. | The goal of this project (Microcontroller No-OS) is to be able to provide reference projects for lower end processors, which can't run Linux, or aren't running a specific operating system, to help those customers using microcontrollers with ADI parts. Here you can find a generic driver which can be used as a base for any microcontroller platform and also specific drivers for Renesas platforms. | ||
**HW Platform(s): | **HW Platform(s): | ||
- | * [[http://am.renesas.com/ | + | * [[https://www.renesas.com/ |
===== Driver Description ===== | ===== Driver Description ===== | ||
Line 49: | Line 72: | ||
==== Required Hardware ==== | ==== Required Hardware ==== | ||
- | * [[http://am.renesas.com/ | + | * [[https://www.renesas.com/ |
* [[adi> | * [[adi> | ||
==== Required Software ==== | ==== Required Software ==== | ||
* [[http:// | * [[http:// | ||
- | * [[http://am.renesas.com/ | + | * [[https://www.renesas.com/ |
==== Hardware Setup ==== | ==== Hardware Setup ==== | ||
Line 109: | Line 132: | ||
==== Software Project Setup ==== | ==== Software Project Setup ==== | ||
{{page> | {{page> | ||
+ | |||
+ | ====== More information ====== | ||
+ | {{page> |