This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:tools-software:uc-drivers:renesas:ad7091r [23 May 2013 15:41] – minor change in Renesas RL78G14 Quick Start Guide Lucian Sin | resources:tools-software:uc-drivers:renesas:ad7091r [28 May 2013 08:54] – [Reference Project Overview] Lucian Sin | ||
---|---|---|---|
Line 43: | Line 43: | ||
<WRAP round important 80%> | <WRAP round important 80%> | ||
- | * The function that converts the raw data to volts uses the 2.5 value as reference voltage. When using an external VREF, set the vRef parameter of the ' | + | * The function that converts the raw data to volts uses the 2.5 value as reference voltage. When using an external VREF, set the vRef parameter of the ' |
</ | </ |