This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:tools-software:uc-drivers:renesas:ad5933 [13 Nov 2012 13:55] – Removed applilet3 content / updated drivers. Dan Nechita | resources:tools-software:uc-drivers:renesas:ad5933 [29 May 2013 11:28] – added RENESAS RL78G14 QUICK START GUIDE and RL78G14 source code downloads Lucian Sin | ||
---|---|---|---|
Line 8: | Line 8: | ||
===== Downloads ===== | ===== Downloads ===== | ||
- | <WRAP round download | + | <WRAP round download |
* {{: | * {{: | ||
* {{: | * {{: | ||
* {{: | * {{: | ||
+ | * **AD5933 Driver: | ||
+ | * **PmodIA Demo for RL78G14: ** https:// | ||
+ | * **RL78G14 Common Drivers: | ||
</ | </ | ||
Line 35: | Line 38: | ||
==== Reference Project Overview ==== | ==== Reference Project Overview ==== | ||
- | The reference project reads the temperature from AD5933 part, initializes and start a sweep operation, calculates the gain factor for an impedance of 47k and calculates the impedance between the VOUT and VIN pins. | + | The reference project: |
- | + | * reads the temperature from AD5933 part; | |
- | The temperature and the impedance | + | * initializes and start a sweep operation; |
+ | * calculates the gain factor for an impedance of 47k; | ||
+ | * calculates the impedance between the VOUT and VIN pins; | ||
+ | * displays the temperature and the impedance on the LCD. | ||
{{ : | {{ : | ||
Line 43: | Line 49: | ||
==== Software Project Tutorial ==== | ==== Software Project Tutorial ==== | ||
{{page> | {{page> | ||
+ | |||
+ | ====== Renesas RL78G14 Quick Start Guide ====== | ||
+ | This section contains a description of the steps required to run the AD5933 demonstration project on a Renesas RL78G14 platform using the PmodIA. | ||
+ | |||
+ | ==== Required Hardware ==== | ||
+ | * [[http:// | ||
+ | * [[http:// | ||
+ | |||
+ | ==== Required Software ==== | ||
+ | * [[http:// | ||
+ | * The AD5933 demonstration project for the Renesas RL78G14 platform. | ||
+ | |||
+ | <WRAP round info 80%> | ||
+ | The AD5933 demonstration project for the Renesas RL78G14 platform consists of three parts: the **AD5933 Driver**, | ||
+ | |||
+ | All three parts have to be downloaded. | ||
+ | </ | ||
+ | |||
+ | ==== Hardware Setup ==== | ||
+ | A PmodIA has to be interfaced with the Renesas Demonstration Kit (RDK) for RL78G14: | ||
+ | |||
+ | PmodIOXP J1 connector pin SCL → RDKRL78G14 J8 connector Pin 1 | ||
+ | PmodIOXP J1 connector pin SDA → RDKRL78G14 J8 connector Pin 3 | ||
+ | PmodIOXP J1 connector pin GND → RDKRL78G14 J11 connector Pin 5 | ||
+ | PmodIOXP J1 connector pin VCC → RDKRL78G14 J11 connector Pin 6 | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | <WRAP round important 80%> | ||
+ | \\ | ||
+ | * The default value for the calibration resistor is 47 Kohms. If another resistor is used for calibration, | ||
+ | \\ | ||
+ | </ | ||
+ | |||
+ | ==== Reference Project Overview ==== | ||
+ | The reference project: | ||
+ | * reads the temperature from AD5933 part; | ||
+ | * initializes and start a sweep operation; | ||
+ | * calculates the gain factor for an impedance of 47k; | ||
+ | * calculates the impedance between the VOUT and VIN pins; | ||
+ | * displays the temperature and the impedance on the LCD. | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | ==== Software Project Tutorial ==== | ||
+ | {{page> | ||
+ | |||
====== Renesas RX62N Quick Start Guide ====== | ====== Renesas RX62N Quick Start Guide ====== |