This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:tools-software:uc-drivers:renesas:ad5252 [13 Apr 2012 08:37] – Approved Dragos Bogdan | resources:tools-software:uc-drivers:renesas:ad5252 [01 Jun 2012 12:48] – Added the "More Information" section Dragos Bogdan | ||
---|---|---|---|
Line 47: | Line 47: | ||
* {{: | * {{: | ||
* {{: | * {{: | ||
+ | * {{: | ||
====== Renesas RL78G13 Quick Start Guide ====== | ====== Renesas RL78G13 Quick Start Guide ====== | ||
Line 104: | Line 104: | ||
==== Software Project Setup ==== | ==== Software Project Setup ==== | ||
{{page> | {{page> | ||
+ | |||
+ | ====== Renesas RX62N Quick Start Guide ====== | ||
+ | |||
+ | This section contains a description of the steps required to run the AD5252 demonstration project on a Renesas RX62N platform. | ||
+ | |||
+ | ==== Required Hardware ==== | ||
+ | * [[http:// | ||
+ | * [[adi> | ||
+ | |||
+ | ==== Required Software ==== | ||
+ | * [[http:// | ||
+ | |||
+ | ==== Hardware Setup ==== | ||
+ | An EVAL-AD5252EBZ board has to be interfaced with the Renesas Demonstration Kit (RDK) for RX62N: | ||
+ | |||
+ | EVAL-AD5252SDZ A connector Pin SCL_BF | ||
+ | EVAL-AD5252SDZ A connector Pin SDA_BF | ||
+ | EVAL-AD5252SDZ A connector Pin WP_BF | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | ==== Reference Project Overview ==== | ||
+ | The reference project: | ||
+ | The reference project initializes the device, reads the RDAC1 tolerance and then continuously increases the output resistance until reaches the upper limit followed by a continuously decrease until reaches lower limit. The project also provides an example of writing and reading from EEMEM. | ||
+ | |||
+ | {{ : | ||
+ | ==== Software Project Setup ==== | ||
+ | {{page> | ||
+ | |||
+ | ====== More information ====== | ||
+ | {{page> |