This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:tools-software:uc-drivers:renesas:ad5162 [06 Apr 2012 13:15] – Approved Dragos Bogdan | resources:tools-software:uc-drivers:renesas:ad5162 [01 Jun 2012 12:48] – Added the "More Information" section Dragos Bogdan | ||
---|---|---|---|
Line 43: | Line 43: | ||
* {{: | * {{: | ||
* {{: | * {{: | ||
+ | * {{: | ||
====== Renesas RL78G13 Quick Start Guide ====== | ====== Renesas RL78G13 Quick Start Guide ====== | ||
This section contains a description of the steps required to run the AD5162 demonstration project on a Renesas RL78G13 platform. | This section contains a description of the steps required to run the AD5162 demonstration project on a Renesas RL78G13 platform. | ||
Line 64: | Line 64: | ||
EVAL-AD5162SDZ A connector Pin MUX-A1 | EVAL-AD5162SDZ A connector Pin MUX-A1 | ||
EVAL-AD5162SDZ A connector Pin MUX-A2 | EVAL-AD5162SDZ A connector Pin MUX-A2 | ||
+ | |||
{{ : | {{ : | ||
Line 97: | Line 98: | ||
==== Software Project Setup ==== | ==== Software Project Setup ==== | ||
{{page> | {{page> | ||
+ | |||
+ | ====== Renesas RX62N Quick Start Guide ====== | ||
+ | |||
+ | This section contains a description of the steps required to run the AD5162 demonstration project on a Renesas RX62N platform. | ||
+ | |||
+ | ==== Required Hardware ==== | ||
+ | * [[http:// | ||
+ | * [[adi> | ||
+ | |||
+ | ==== Required Software ==== | ||
+ | * [[http:// | ||
+ | |||
+ | ==== Hardware Setup ==== | ||
+ | An EVAL-AD5162EBZ board has to be interfaced with the Renesas Demonstration Kit (RDK) for RX62N: | ||
+ | |||
+ | EVAL-AD5162SDZ A connector Pin SYNC_BF | ||
+ | EVAL-AD5162SDZ A connector Pin DIN_BF | ||
+ | EVAL-AD5162SDZ A connector Pin SCLK_BF | ||
+ | EVAL-AD5162SDZ A connector Pin MUX-A0 | ||
+ | EVAL-AD5162SDZ A connector Pin MUX-A1 | ||
+ | EVAL-AD5162SDZ A connector Pin MUX-A2 | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | ==== Reference Project Overview ==== | ||
+ | The reference project: | ||
+ | The reference project initializes the device and continuously writes to one of the two channels available. | ||
+ | |||
+ | {{ : | ||
+ | ==== Software Project Setup ==== | ||
+ | {{page> | ||
+ | |||
+ | ====== More information ====== | ||
+ | {{page> |