This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:tools-software:uc-drivers:microchip:ad5160 [09 Oct 2012 09:15] – Replaced Arduino with chipKIT. Dragos Bogdan | resources:tools-software:uc-drivers:microchip:ad5160 [04 Jul 2013 16:41] (current) – source code change and source code put on github Lucian Sin | ||
---|---|---|---|
Line 7: | Line 7: | ||
===== Downloads ===== | ===== Downloads ===== | ||
- | * {{: | + | <WRAP round download 80%> |
- | * {{: | + | |
* {{: | * {{: | ||
* {{: | * {{: | ||
+ | * **AD5160 Driver: | ||
+ | * **PmodDPOT Demo for PIC32MX320F128H: | ||
+ | * **PIC32MX320F128H Common Drivers: | ||
+ | </ | ||
====== Digilent Cerebot MX3cK Quick Start Guide ====== | ====== Digilent Cerebot MX3cK Quick Start Guide ====== | ||
This section contains a description of the steps required to run the AD5160 demonstration project on a Digilent Cerebot MX3cK platform. | This section contains a description of the steps required to run the AD5160 demonstration project on a Digilent Cerebot MX3cK platform. | ||
Line 17: | Line 19: | ||
==== Required Hardware ==== | ==== Required Hardware ==== | ||
* [[http:// | * [[http:// | ||
- | * PmodDPOT | + | * [[http:// |
==== Required Software ==== | ==== Required Software ==== | ||
* [[http:// | * [[http:// | ||
* [[http:// | * [[http:// | ||
+ | * The AD5160 demonstration project for PIC32MX320F128H. | ||
+ | |||
+ | <WRAP round info 80%> | ||
+ | The AD5160 demonstration project for PIC32MX320F128H consists of three parts: the **AD5160 Driver**, | ||
+ | |||
+ | All three parts have to be downloaded. | ||
+ | </ | ||
==== Hardware Setup ==== | ==== Hardware Setup ==== | ||
Line 29: | Line 38: | ||
==== Reference Project Overview ==== | ==== Reference Project Overview ==== | ||
- | Following | + | The following |
^ Command ^ Description ^ | ^ Command ^ Description ^ | ||
| help? | Displays all available commands. | | | help? | Displays all available commands. | | ||
- | | resistance= | Sets the output resistance. Accepted values | + | | resistance= | Sets the output resistance |
- | | resistance? | Displays the last written value. | | + | | resistance? | Displays the last written |
- | | register= | Writes to the DAC register | + | | register= | Writes to the DAC register. Accepted values:\\ 0 .. 255 - the value written to the DAC. | |
- | | register? | Displays the last written value. | | + | | register? | Displays the last written value in register. | |
Commands can be executed using a serial terminal connected to the UART1 peripheral of PIC32MX320F128H. | Commands can be executed using a serial terminal connected to the UART1 peripheral of PIC32MX320F128H. | ||
- | The following image shows a list of commands in a serial terminal connected to processor’s UART peripheral. | + | The following image shows a generic |
{{ : | {{ : | ||