The MAX9611 / MAX9612 are high-side current-sense amplifiers with an integrated 12-bit ADC and a gain block that can be configured either as an op amp or comparator, making these devices ideal for a number of industrial and automotive applications.
The high-side, current-sense amplifiers operate over a wide 0 V to 60 V input common-mode voltage range. The programmable full-scale voltage (440 mV, 110 mV, and 55 mV) of these amplifiers offers wide dynamic range, accurate current measurement, and application flexibility in choosing sense resistor values. A choice of either an internal op amp or a comparator is provided to the user.
The internal amplifier can be used to limit the inrush current or to create a current source in a closed-loop system. The comparator can be used to monitor fault events for fast response.
An I2C-controlled 12-bit, 500 sps analog-to-digital converter (ADC) can be used to read the voltage across the sense resistor (VSENSE), the input common-mode voltage (VRSCM), op amp/comparator output (VOUT), op amp/ comparator reference voltage (VSET), and internal die temperature.
The I2C bus is compatible with 1.8 V and 3.3 V logic, allowing modern microcontrollers to interface to it. The MAX9611 features a noninverting input-to-output configuration, while the MAX9612 features an inverting input-to-output configuration.
The goal of the ADI Microcontroller No-OS is to provide reference projects for lower end processors, which can't run Linux or aren't running a specific operating system, and to help those customers using microcontrollers with ADI parts. ADI No-OS offers generic drivers, which can be used as a base for any microcontroller platform and also example projects, which are using these drivers on various microcontroller platforms.
For more information about ADI No-OS and supported microcontroller platforms, visit the No-OS User Guide.
The source code for MAX9611 driver can be found here:
This driver also uses the ADI utility library, so make sure you also add the necessary files to your project. The source code for the utility library can be found here:
To use the MAX9611 No-OS driver, you need to provide the specific implementation for the communication APIs and the specific types they use.
If the SPI communication is chosen, there are three functions which are called by the MAX9611 driver and have to be implemented:
no_os_i2c_init() | initializes the communication peripheral. |
no_os_i2c_write() | writes data to the device. |
no_os_i2c_read() | reads data from the device. |
no_os_i2c_remove() | deinitializes the communication peripheral. |
And there are two data types that have to be defined:
no_os_i2c_desc | structure holding the I2C descriptor |
no_os_i2c_init_param | structure holding the parameters for I2C initialization |
An example of a header file containing the prototypes of the functions which have to be implemented, along with some generic data types they are using, can be found below:
Source code documentation for the driver is automatically generated using the Doxygen tool and can be accessed in these links:
To use the device, you need to provide the support for the communication protocol (I2C) as mentioned above.
The first API function to be called is max9611_addr_gen to generate the corresponding device's slave address. Once a proper address is generated, use the function max9611_init to initialize the device and make sure that it returns 0. This indicates a successful driver initialization.
The MAX9611 / MAX9612 have the provision for multiple I2C slave addresses via the A0 and A1 pins. To generate the proper address, supply the voltage level going into pins A0 and A1 to the max9611_addr_gen function.
The MAX9611 contains an internally selectable op amp and comparator whose inputs are the current sense amplifier with a 2.5 gain and the SET pin. By using the max9611_set_mode and max9611_get_mode functions, the user would be able to set and obtain the configuration of the OUT pin, respectively. The header file contains the enumerations pertaining to the valid operating modes.
The MAX9611 contains an internal dual-slope integrating 12-bit ADC with a 2 mS conversion time. This ADC is also compatible with 1.8 V or 3.3 V I2C logic level buses. This ADC contains an internal MUX to allow selection between the following measurements: input sense voltage, input common-mode voltage, SET pin voltage, OUT pin voltage, and die temperature.
Similarly, the mux configuration can be set or read through the max9611_set_mux and max9611_get_mux driver functions. The max9611_set_mux function also allows a burst read of all viable channels, which might be useful for certain applications. The valid enumerations corresponding to each usable mode can be seen below:
MAX9611_CONF_SENSE_1X | measure Current Sense Amplifier Output with gain = 1 |
MAX9611_CONF_SENSE_4X | measure Current Sense Amplifier Output with gain = 4 |
MAX9611_CONF_SENSE_8X | measure Current Sense Amplifier Output with gain = 8 |
MAX9611_CONF_IN_COM_MODE | measure input common mode voltage |
MAX9611_CONF_OUT_ADC | measure OUT pin voltage |
MAX9611_CONF_SET_ADC | measure SET pin voltage |
MAX9611_CONF_TEMP | measure internal die temperature |
MAX9611_FAST_MODE | measure all channels in fast mode (uses last gain setting) |
Once the mux configuration has been set, the selected channel measurement can be read using the max9611_get_raw function.
Die Temperature Measurement
By configuring the internal mux using max9611_set_mux function, the die temperature of the MAX9611 can also be measured. The temperature measurement ranges from -40°C to +125°C with a 0.48°C step size. The temperature measurement is encoded using 9 bits in two's complement format.
The MAX9611's internal digital block sports a watchdog function for handling false fault transients, applicable for both op amp and comparator operating modes. Different time delay options for the comparator are configured in CONTROL REGISTER 2 through the corresponding driver functions:
max9611_set_delay | configures the watchdog delay time |
max9611_get_delay | acquires the configured watchdog delay time |
max9611_set_retry | configure the watchdog retry delay time |
max9611_get_retry | acquires the configured watchdog retry delay time |
The valid delay times for the watchdog delay and retry delay times are as follows:
Watchdog Delay Times
MAX9611_1MS | 1 mS watchdog delay time (default) |
MAX9611_100US | 100 µS watchdog delay time |
Watchdog Retry Delay Times
MAX9611_50MS | 50 mS watchdog retry delay time (default) |
MAX9611_10MS | 10 mS watchdog retry delay time |
During Normal Operation (MAX9611_NORMAL_MODE), the internal amplifier output depends on its inputs: the CSA output and the SET pin voltage level. This internal amplifier can act as a comparator for open-loop configurations.
For op amp (MAX9611_OPAMP_MODE) or comparator (MAX9611_COMPARATOR_MODE), the comparator output ensures the CSA output stays above the SET voltage level for a watchdog delay time, and then latches on to this state. The retry delay time dictates the time taken before the comparator state is reset and the cycle repeats.
For more information on this, refer to the MAX9611 data sheet under the Watchdog/Latch/Retry Functionality section and other related sections.
To save power, one may use the max9611_shutdown function resulting in a 5 µA supply current drawn. Alternatively, this function can also be used to bring the component back to its 'power on' state.
int ret; uint8_t mux_conf[] = { MAX9611_CONF_SENSE_1X, MAX9611_CONF_SENSE_4X, MAX9611_CONF_SENSE_8X, MAX9611_CONF_IN_COM_MODE, MAX9611_CONF_OUT_ADC, MAX9611_CONF_SET_ADC, MAX9611_CONF_TEMP, MAX9611_FAST_MODE, }; uint8_t mode_conf[] = { MAX9611_NORMAL_MODE, MAX9611_OPAMP_MODE, MAX9611_COMPARATOR_MODE, }; uint8_t delays[] = { MAX9611_1MS, MAX9611_100US, }; uint8_t retries[] = { MAX9611_50MS, MAX9611_10MS, }; struct max_i2c_init_param max9611_extra = { .vssel = MXC_GPIO_VSSEL_VDDIOH, }; struct max9611_init_param max9611_ip = { .i2c_init.device_id = 0, .i2c_init.max_speed_hz = MAX_I2C_STD_MODE, .i2c_init.extra = &max9611_extra, .i2c_init.platform_ops = &max_i2c_ops, }; ret = max9611_addr_gen(&max9611_ip, MAX9611_ZERO_VCC, MAX9611_ZERO_VCC); if (ret) return ret; struct max9611_dev *max9611_device; ret = max9611_init(&max9611_device, max9611_ip); if (ret) return ret; while (1){ uint16_t raw_val; int mux_cnt = 0, mode_cnt = 0, dcnt = 0, rcnt = 0; for (int i = 0; i < 8; i++) { enum max9611_mux_conf mux, mux_new; ret = max9611_get_mux(max9611_device, &mux); if (ret) return ret; ret = max9611_set_mux(max9611_device, mux_conf[i]); if (ret) return ret; ret = max9611_get_mux(max9611_device, &mux_new); if (ret) return ret; ret = max9611_get_raw(max9611_device, &raw_val); if (ret) return ret; if (mux_conf[i] != mux_new) mux_cnt++; } for (int i = 0; i < 3; i++) { enum max9611_mode_conf mode, mode_new; ret = max9611_get_mode(max9611_device, &mode); if (ret) return ret; ret = max9611_set_mode(max9611_device, mode_conf[i]); if (ret) return ret; ret = max9611_get_mode(max9611_device, &mode_new); if (ret) return ret; if (mode_conf[i] != mode_new) mode_cnt++; } for (int i = 0; i < 2; i++) { enum max9611_delay_time dtime, dtime_new; ret = max9611_get_delay(max9611_device, &dtime); if (ret) return ret; ret = max9611_set_delay(max9611_device, delays[i]); if (ret) return ret; ret = max9611_get_delay(max9611_device, &dtime_new); if (ret) return ret; if (delays[i] != dtime_new) dcnt++; } for (int i = 0; i < 2; i++) { enum max9611_retry_time rtime, rtime_new; ret = max9611_get_retry(max9611_device, &rtime); if (ret) return ret; ret = max9611_set_retry(max9611_device, retries[i]); if (ret) return ret; ret = max9611_get_retry(max9611_device, &rtime_new); if (ret) return ret; if (retries[i] != rtime_new) rcnt++; } ret = max9611_shutdown(max9611_device, true); if (ret) return ret; ret = max9611_shutdown(max9611_device, false); if (ret) return ret; }