world leader in high performance signal processing
This version (15 Nov 2012 15:35) was approved by BillJ.The Previously approved version (14 Nov 2012 23:07) is available.Diff

ABS Max and Hold

Click here to return to the BasicDSP page

The ABSMax and Hold algorithm monitors one (or more) input(s) and routes the input absolute maximum value to the output. While the 'Hold' pin is held high (1), the output will remain at the highest absolute input value.