This shows you the differences between two versions of the page.
|
resources:tools-software:sigmastudio:gettingstarted:installation [12 Jun 2012 16:25] BillJ [Step 1: Before You Install] |
resources:tools-software:sigmastudio:gettingstarted:installation [14 Jun 2012 20:36] (current) BrettG [Step 4: Hardware Configuration] Updated link to online EVB help |
||
|---|---|---|---|
| Line 1: | Line 1: | ||
| ====== Installation Procedure ====== | ====== Installation Procedure ====== | ||
| + | \\ | ||
| + | [[resources/tools-software/sigmastudio/gettingstarted|Click here to return to the Getting Started page]] | ||
| + | \\ | ||
| \\ | \\ | ||
| Line 6: | Line 9: | ||
| ====System Requirements==== | ====System Requirements==== | ||
| - | * Windows XP Professional or Home Edition with SP2; Windows 2000 with SP4; Windows ME; Windows Server 2003 | + | * Windows XP Professional or Home Edition with SP3, Windows Vista, or Windows 7 |
| * 128 MB of RAM (256 MB recommended) | * 128 MB of RAM (256 MB recommended) | ||
| * 50 MB of available hard disk space | * 50 MB of available hard disk space | ||
| * 1024 x 768 screen resolution | * 1024 x 768 screen resolution | ||
| * USB 1.1/2.0 data port (Required for use with Evaluation hardware only) | * USB 1.1/2.0 data port (Required for use with Evaluation hardware only) | ||
| - | \\ | + | * Note that USB 2.0 or higher is required for use with the USBi (EVAL-ADUSB2EBZ) |
| - | + | ||
| - | Note: SigmaStudio can be installed under Windows Vista, however Windows Vista is not officially supported at this time and Analog Devices cannot offer any technical support regarding Vista installation or issues. | + | |
| \\ | \\ | ||
| ====Step 1: Before You Install==== | ====Step 1: Before You Install==== | ||
| * Quit any applications you are running. | * Quit any applications you are running. | ||
| - | * Confirm that the Microsoft .NET Framework v2.0 is installed. | + | * Confirm that the Microsoft .NET Framework v3.5 is installed. |
| - | * To install the Microsoft .Net Framework from the SigmaStudio CD, browse to the CD folder, and double-click the installer "dotnetfx.exe". | + | * (The "Microsoft .NET Framework Version 3.5 Redistributable Package" installation and updates are also available for download directly from microsoft www.microsoft.com/downloads ) |
| - | * (The "Microsoft .NET Framework Version 2.0 Redistributable Package" installation and updates are also available for download directly from microsoft www.microsoft.com/downloads ) | + | |
| ====Step 2: Application Setup==== | ====Step 2: Application Setup==== | ||
| - | * Run the setup application (Sigma Studio.msi). | + | * Run the setup application (SigmaStudioInstall.exe) |
| - | * Review the contents of the license agreement. | + | * Review the contents of the license agreement |
| - | * If installing SigmaStudio for the first time, restart your computer when the installation is complete. | + | |
| ====Step 3: Driver Installation==== | ====Step 3: Driver Installation==== | ||
| * Connect the USB cable to your evaluation hardware and to a spare USB port on your PC. | * Connect the USB cable to your evaluation hardware and to a spare USB port on your PC. | ||
| - | * The Windows "Found New Hardware Wizard" will launch. | + | * If this is your first time connecting the USB device, the Windows "Found New Hardware Wizard" will launch. |
| - | * Choose “Install from a list or a specific location” and click "Next". | + | * If prompted, choose “Install from a list or a specific location” and click "Next". |
| - | * Select “Search for the best driver in these locations” and Check the box for “Include this location in the search.” | + | * Select “Search for the best driver in these locations” and check the box for “Include this location in the search.” |
| - | * Press the "Browse" button and locate the appropriate driver file in the SigmaStudio application folder (default folder is C:\Program Files\Analog Devices Inc\Sigma Studio\USB drivers): | + | * Press the "Browse" button and locate the appropriate driver file in the SigmaStudio application folder (default folder is C:\Program Files\Analog Devices Inc\Sigma Studio X.Y\USB drivers, where X.Y represents the release version of the software) |
| - | * For **USB serial converter** and Eval-Boards (FDTIxx.inf) select **ftd2xx.inf** file. | + | * For **USB serial converter** and Eval-Boards (FDTIxx.inf) select **ftd2xx.inf** file. |
| - | * For **USBi** interface select **CyUSB.inf file**. | + | * Any evaluation board sold after 2007 uses the USBi interface, but the FTDI drivers are included for backwards-compatibility. |
| + | * For the **USBi** interface select **CyUSB.inf file**. | ||
| * Click "Continue Anyway" if you're prompted with "This software has not passed Windows Logo testing." | * Click "Continue Anyway" if you're prompted with "This software has not passed Windows Logo testing." | ||
| ====Step 4: Hardware Configuration==== | ====Step 4: Hardware Configuration==== | ||
| - | * Setup the Evaluation hardware jumpers and i/o configurations, refer to Evaluation Board documentation on the on the SigmaStudio CD (EVAL_ADxxx.pdf). Documentation is also available on the web at www.analog.com/sigmadsp. | + | * Setup the Evaluation hardware jumpers and I/O configurations, refer to Evaluation Board documentation available on the web at [[adi>/en/content/sigmadsp_evaluation_boards/fca.html|SigmaDSP Evaluation Boards]]. |
| * For additional help, see the Evaluation Board Setup Examples. | * For additional help, see the Evaluation Board Setup Examples. | ||