This is an old revision of the document!
ARM mbed is a solution to quickly prototype and build embedded applications using ARM microcontrollers. The goal of these projects (microcontroller/mbed) is to be able to provide reference projects for the mbed platform, to help customers use ADI parts with their mbed projects.
These examples can be run using the online compiler at https://developer.mbed.org or by setting up your computer using the following guide: https://wiki.analog.com/resources/tools-software/mbed-user-guide
The latest drivers and shield libraries can be found at: https://github.com/analogdevicesinc/mbed-adi A mirror of the git repository can be found on the mbed website at: https://developer.mbed.org/teams/AnalogDevices/code/mbed-drivers/
Part Number | Reference Project | Description | Driver |
---|---|---|---|
Analog to Digital Converters |
AD7790 | EVAL-CN0357-ARDZ | The AD7790 is a low power, complete analog front end for low frequency measurement applications. It contains a low noise 16-bit ∑-Δ ADC with one differential input that can be buffered or unbuffered along with a digital PGA, which allows gains of 1, 2, 4, and 8. The device operates from an internal clock. Therefore, the user does not have to supply a clock source to the device. The output data rate from the part is software programmable and can be varied from 9.5 Hz to 120 Hz, with the rms noise equal to 1.1 μV at the lower update rate. The internal clock frequency can be divided by a factor of 2, 4, or 8, which leads to a reduction in the current consumption. The update rate, cutoff frequency, and settling time will scale with the clock frequency. The part operates with a power supply from 2.5 V to 5.25 V. When operating from a 3 V supply, the power dissipation for the part is 225 μW maximum. It is housed in a 10-lead MSOP. | mbed driver page: |
AD7791 | EVAL-CN0216-ARDZ | The AD7791 is a low power, complete analog front end for low frequency measurement applications. It contains a low noise 24-bit ∑-Δ ADC with one differential input that can be buffered or unbuffered. The device operates from an internal clock. Therefore, the user does not have to supply a clock source to the device. The output data rate from the part is software programmable and can be varied from 9.5 Hz to 120 Hz, with the rms noise equal to 1.1 μV at the lower update rate. The internal clock frequency can be divided by a factor of 2, 4, or 8, which leads to a reduction in the current consumption. The update rate, cutoff frequency, and settling time will scale with the clock frequency. The part operates with a power supply from 2.5 V to 5.25 V. When operating from a 3 V supply, the power dissipation for the part is 225 μW maximum. It is housed in a 10-lead MSOP. | mbed driver page: |
AD7798 | EVAL-CN0396-ARDZ EVAL-CN0397-ARDZ | The AD7798/AD7799 are low power, low noise, complete analog front ends for high precision measurement applications. The AD7798/AD7799 contains a low noise, 16-/24- it ∑-∆ ADC with three differential analog inputs. The on-chip, low noise instrumentation amplifier means that signals of small amplitude can be interfaced directly to the ADC. With a gain setting of 64, the rms noise is 27 nV for the AD7799 and 40 nV for the AD7798 when the update rate equals 4.17 Hz. On-chip features include a low-side power switch, reference detect, programmable digital output pins, burnout currents, and an internal clock oscillator. The output data rate from the part is software-programmable and can be varied from 4.17 Hz to 470 Hz. The part operates with a power supply from 2.7 V to 5.25 V. The AD7798 consumes a current of 300 µA typical, whereas the AD7799 consumes 380 µA typical. Both devices are housed in a 16-lead TSSOP package. | mbed driver page: |
AD7124 | EVAL-CN0391-ARDZ EVAL-CN0398-ARDZ | The AD7124-8 is a low power, low noise, completely integrated analog front end for high precision measurement applications. The device contains a low noise, 24-bit Σ-Δ analog-to-digital converter (ADC), and can be configured to have 8 differential inputs or 15 single-ended or pseudo differential inputs. The onchip low gain stage ensures that signals of small amplitude can be interfaced directly to the ADC. One of the major advantages of the AD7124-8 is that it gives the user the flexibility to employ one of three integrated power modes. The current consumption, range of output data rates, and rms noise can be tailored with the power mode selected. The device also offers a multitude of filter options, ensuring that the user has the highest degree of flexibility. The AD7124-8 can achieve simultaneous 50 Hz and 60 Hz rejection when operating at an output data rate of 25 SPS (single cycle settling), with rejection in excess of 80 dB achieved at lower output data rates. As many as 16 channels can be enabled at any time, a channel being defined as an analog input or a diagnostic such as a power supply check or a reference check. This unique feature allows diagnostics to be interleaved with conversions. The AD7124-8 also supports per channel configuration. The device allows eight configurations or setups. Each configuration consists of gain, filter type, output data rate, buffering, and reference source. The user can assign any of these setups on a channel by channel basis. The AD7124-8 also has extensive diagnostic functionality integrated as part of its comprehensive feature set. These diagnostics include a cyclic redundancy check (CRC), signal chain checks, and serial interface checks, which lead to a more robust solution. These diagnostics reduce the need for external components to implement diagnostics, resulting in reduced board space needs, reduced design cycle times, and cost savings. The AD7124-8 is housed in a 32-lead LFCSP package | mbed driver page: |
Digital Potentiometers | |||
---|---|---|---|
AD5270 AD5271 | EVAL-CN0357-ARDZ | The AD5270/AD52711 are single-channel, 1024-/256-position digital rheostats that combine industry leading variable resistor performance with nonvolatile memory (NVM) in a compact package. The AD5270/AD5271 ensure less than 1% end-to-end resistor tolerance error and offer 50-times programmable (50-TP) memory. | mbed driver page: |
MEMS Accelerometers | |||
---|---|---|---|
ADXL362 ADXL362 | EVAL-ADXL362-ARDZ | The ADXL362 is an ultralow power, 3-axis MEMS accelerometer that consumes less than 2 μA at a 100 Hz output data rate and 270 nA when in motion triggered wake-up mode. Unlike accelerometers that use power duty cycling to achieve low power consumption, the ADXL362 does not alias input signals by undersampling; it samples the full bandwidth of the sensor at all data rates. The ADXL362 always provides 12-bit output resolution; 8-bit formatted data is also provided for more efficient single-byte transfers when a lower resolution is sufficient. Measurement ranges of ±2 g, ±4 g, and ±8 g are available, with a resolution of 1 mg/LSB on the ±2 g range. | mbed driver page: |
Board | Parts used | Description | Reference project |
---|
EVAL-CN0357-ARDZ | AD7790 AD5270 | CN0357 single-supply, low noise, portable gas detector circuit using an electrochemical sensor. The Alphasense CO-AX carbon monoxide sensor is used in this example. Electrochemical sensors offer several advantages for instruments that detect or measure the concentration of many toxic gases. Most sensors are gas specific and have usable resolutions under one part per million (ppm) of gas concentration | ADI Reference Project:
mbed library |
EVAL-CN0216-ARDZ | AD7791 | CN-0216 is a precision weigh scale signal conditioning system. It uses the AD7791, a low power buffered 24-bit sigma-delta ADC along with dual external ADA4528-1 zero-drift amplifiers. This solution allows for high dc gain with a single supply. This circuit allows great flexibility in designing a custom low-level signal conditioning front end that gives the user the ability to easily optimize the overall transfer function of the combined sensor-amplifier-converter circuit. | ADI Reference Project:
mbed library |
EVAL-ADXL362-ARDZ | ADXL362 | The EVAL-ADXL362-ARDZ shield illustrates the functionality of the ADXL362 - an ultralow power, 3-axis MEMS accelerometer. The ADXL362 is capable of measuring dynamic acceleration (resulting from motion or shock) as well as static acceleration (gravity). It provides 12-bit output resolution and has three operating ranges, ±2 g, ±4 g, and ±8 g. Additional useful features include an on-chip, 12-bit temperature sensor accurate to ±0.5°, motion triggered wake-up functionality, and and several activity detection modes which makes is ideal for portable low-power instruments. The EVAL-ADXL362-ARDZ Shield is designed in Arduino Uno R3 format which makes it suitable to used with both Arduino Due (e.g. EVAL-ADICUP360 based board) and Arduino Uno R3 base boards. | ADI Reference Project:
mbed library |
CN0398 | AD7124 | CN0398 is a single supply, low power, high precision complete solution for soil moisture and pH measurements, including temperature compensation. The circuit is optimized for use with capacitive soil moisture sensors that are insensitive to water salinity and do not corrode over time. The circuit also measures soil pH and that function is suitable in a variety of applications. | ADI Reference Project:
mbed library |