Differences
This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision |
resources:tools-software:linux-software:iio_oscilloscope [10 Jul 2015 17:01] – [Main Window] Lucian Sin | resources:tools-software:linux-software:iio_oscilloscope [20 Jul 2015 09:47] – Small changes related to expression, fix a link Mihai Ionut Suciu |
---|
For building on the target, we recommend using the [[/resources/tools-software/linux-software/zynq_images#staying_up_to_date|update scripts]]. This is a tried/proven method that does everything in a quick script. | For building on the target, we recommend using the [[/resources/tools-software/linux-software/zynq_images#staying_up_to_date|update scripts]]. This is a tried/proven method that does everything in a quick script. |
| |
To build on a host, not not use the script, you **must**: | To build on a host, do not use the script, you **must**: |
- make sure the following libraries are installed. This list is maintained in the ''adi_update_tools.sh'' shell script, and can be copied/pasted to most Debian based distributions. For others - make sure they are installed, or the below steps will not work. If you are not sure how to do this - consult your distribution documentation. <source master/adi_update_tools.sh:/apt/-/if/ bash linux_image_ADI-scripts> | - make sure the following libraries are installed. This list is maintained in the ''adi_update_tools.sh'' shell script, and can be copied/pasted to most Debian based distributions. For others - make sure they are installed, or the below steps will not work. If you are not sure how to do this - consult your distribution documentation. file: [[https://github.com/analogdevicesinc/linux_image_ADI-scripts/blob/master/adi_update_tools.sh|adi_update_tools.sh]] |
- build **and install** the libiio library, by following these [[libiio#how_to_build_it|instructions]]. Make sure you do the final "''make install''". | - build **and install** the libiio library, by following these [[libiio#how_to_build_it|instructions]]. Make sure you do the final ''make install''. |
- download the source <xterm> | - download the source <xterm> |
> **git clone https://github.com/analogdevicesinc/iio-oscilloscope.git** | > **git clone https://github.com/analogdevicesinc/iio-oscilloscope.git** |