This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:tools-software:linux-software:iio_oscilloscope [19 Dec 2013 14:16] – [About] - fix spelling Robin Getz | resources:tools-software:linux-software:iio_oscilloscope [21 Feb 2014 10:30] – syntax errors Lucian Sin | ||
---|---|---|---|
Line 49: | Line 49: | ||
* **Device:** Allows to select one of the ADCs that are available. | * **Device:** Allows to select one of the ADCs that are available. | ||
- | * **Active channels:** Allows to select the to be displayed | + | * **Active channels:** Allows to select the channels |
* **Plot type** | * **Plot type** | ||
* **Time domain:**: Plot the signal in the time domain. Displays the raw samples. | * **Time domain:**: Plot the signal in the time domain. Displays the raw samples. | ||
* **Frequency domain:** Plot the signal in the frequency domain. Performs a FFT on the signal and displays it. | * **Frequency domain:** Plot the signal in the frequency domain. Performs a FFT on the signal and displays it. | ||
- | * **Constalation:** Plot the signal as a constalation | + | * **Constellation:** Plot the signal as a constellation |
* **Time Interval:** Request the samples that can be captured in the given interval. | * **Time Interval:** Request the samples that can be captured in the given interval. | ||
- | * **Sample count:** Selects the number of samples for time domain and constalation | + | * **Sample count:** Selects the number of samples for time domain and constellation |
* **FFT size:** Selects the size of the FFT for frequency domain plotting | * **FFT size:** Selects the size of the FFT for frequency domain plotting | ||
* **FFT Average:** Selects the average weight to be applied to the FFT samples. | * **FFT Average:** Selects the average weight to be applied to the FFT samples. |