This is an old revision of the document!
For compile time configuration, it’s common Linux practice to keep board- and application-specific configuration out of the main driver file, instead putting it into the board support file.
For devices on custom boards, as typical of embedded and SoC-(system-on-chip) based hardware, Linux uses platform_data to point to board-specific structures describing devices and how they are connected to the SoC. This can include available ports, chip variants, preferred modes, default initialization, additional pin roles, and so on. This shrinks the board-support packages (BSPs) and minimizes board and application specific #ifdefs in drivers.
SPI can be used for the SSM2602. Make sure that it is in SPI mode (MODE pin set to 1).
Unlike PCI or USB devices, SPI devices are not enumerated at the hardware level. Instead, the software must know which devices are connected on each SPI bus segment, and what slave selects these devices are using. For this reason, the kernel code must instantiate SPI devices explicitly. The most common method is to declare the SPI devices by bus number.
This method is appropriate when the SPI bus is a system bus, as in many embedded systems, wherein each SPI bus has a number which is known in advance. It is thus possible to pre-declare the SPI devices that inhabit this bus. This is done with an array of struct spi_board_info, which is registered by calling spi_register_board_info().
For more information see: Documentation/spi/spi-summary.rst
static struct spi_board_info board_spi_board_info[] __initdata = { [--snip--] { .modalias = "ssm2602", .max_speed_hz = 25000000, /* max spi clock (SCK) speed in HZ */ .bus_num = 0, .chip_select = GPIO_PF10 + MAX_CTRL_CS, /* CS, change it for your board */ .mode = SPI_MODE_3, }, [--snip--] };
static int __init board_init(void) { [--snip--] spi_register_board_info(board_spi_board_info, ARRAY_SIZE(board_spi_board_info)); [--snip--] return 0; } arch_initcall(board_init);
I2C can be used for the SSM2602, SSM2603, SSM2604. For the SSM2602 make sure that it is in I2C mode (MODE pin set to 0).
For compile time configuration, it’s common Linux practice to keep board- and application-specific configuration out of the main driver file, instead putting it into the board support file.
For devices on custom boards, as typical of embedded and SoC-(system-on-chip) based hardware, Linux uses platform_data to point to board-specific structures describing devices and how they are connected to the SoC. This can include available ports, chip variants, preferred modes, default initialization, additional pin roles, and so on. This shrinks the board-support packages (BSPs) and minimizes board and application specific #ifdefs in drivers.
static struct i2c_board_info __initdata bfin_i2c_board_info[] = { [--snip--] { I2C_BOARD_INFO("ssm2604", 0x1b), }, [--snip--] }
static int __init stamp_init(void) { [--snip--] i2c_register_board_info(0, bfin_i2c_board_info, ARRAY_SIZE(bfin_i2c_board_info)); [--snip--] return 0; } arch_initcall(board_init);
To add support for the built-in codec SSM2602 of BF52xC to the kernel build system, a few things must be enabled properly for things to work.The structure of the driver has been changed after 2008R1.5, so things are a bit different from then on.The configuration is as following:
Linux Kernel Configuration Device Drivers ---> Sound ---> <M> Sound card support Advanced Linux Sound Architecture ---> <M> Advanced Linux Sound Architecture < > Sequencer support <M> OSS Mixer API <M> OSS PCM (digital audio) API Codec configuration for releases 2008R1/1.5: System on Chip audio support ---> <M> ALSA for SoC audio support <M> SoC Audio for ADI BF5xx chip [*] Enable MMAP Support <M> SoC SSM2602 Audio support for BF52x ezkit < > SoC AC97 Audio support for BF5xx (0) Set a SPORT for Sound chip Codec configuration for releases after 2008R1.5: System on Chip audio support ---> <M> ALSA for SoC audio support <M> SoC I2S Audio for the ADI BF5xx chip <M> SoC SSM2602 Audio support for BF52x ezkit < > SoC AC97 Audio support for BF5xx (0x1b) I2c address to SSM2602 on a BF527 (0) Set a SPORT for Sound chip
Linux Kernel Configuration Device Drivers ---> <*> I2C support ---> --- I2C support I2C Hardware Bus Support ---> <*> Blackfin TWI I2C support
Doing this will create modules (outside the kernel). The modules will be inserted automatically when it is needed. You can also build sound driver into kernel.
If audio is configured as modules, skip this section. If audio is built into kernel and you have booted the kernel, there are a few things to check to ensure audio is working:
Advanced Linux Sound Architecture Driver Version 1.0.12rc1 (Thu Jun 22 13:55:50 2006 UTC). ASoC version 0.13.1 dma rx:3 tx:4, err irq:15, regs:ffc00800 ssm2602 Audio Codec 0.1<6>dma_alloc_init: dma_page @ 0x03011000 - 512 pages at 0x03e00000 asoc: SSM2602 <-> bf5xx-i2s-0 mapping ok ALSA device list: #0: bf5xx_ssm2602 (SSM2602)
root:~> modprobe snd-ssm2602 root:~> modprobe snd-pcm-oss root:~> lsmod Module Size Used by snd_pcm_oss 31968 0 snd_mixer_oss 11360 1 snd_pcm_oss snd_ssm2602 1412 0 snd_soc_ssm2602 8528 1 snd_ssm2602 snd_soc_bf5xx 2784 1 snd_ssm2602 snd_soc_bf5xx_i2s 10916 2 snd_ssm2602,snd_soc_bf5xx snd_soc_core 17120 3 snd_ssm2602,snd_soc_ssm2602,snd_soc_bf5xx snd_pcm 48356 3 snd_pcm_oss,snd_soc_bf5xx,snd_soc_core snd_page_alloc 4232 1 snd_pcm snd_timer 13796 1 snd_pcm snd 31092 6 snd_pcm_oss,snd_mixer_oss,snd_soc_ssm2602,snd_soc_core,snd_pcm,snd_timer soundcore 3940 1 snd root:~> tone TONE: generating sine wave at 1000 Hz...
root:~> tone TONE: generating sine wave at 1000 Hz...You should hear something out of the headphone Jack on the top of J8.
root:/> amixer sset 'Input Mux' 'Mic' Simple mixer control 'Input Mux',0 Capabilities: enum Items: 'Line' 'Mic' Item0: 'Mic'Also you can run “alsamixer” to get graphic configuration interface, OSS-based “mixer” can work too.
wget
command assumes that networking is properly configured (you have an IP number, the default gateway is set, and DNS servers can be accessed), and working. See the network setup page for more info. root:/> cd /var root:/var> wget http://www.radiocrazy.com/shows/A/AbbottCostello/ABCOWhosOnFirstclip.mp3
root:/var> mp3play ABCOWhosOnFirstclip.mp3
root:~> mp3play http://www.radiocrazy.com/shows/A/AbbottCostello/ABCOWhosOnFirstclip.mp3 http://www.radiocrazy.com/shows/A/AbbottCostello/ABCOWhosOnFirstclip.mp3: MPEG2-III (0 ms)
root:/> amixer sset 'Input Mux' 'Line' Simple mixer control 'Input Mux',0 Capabilities: enum Items: 'Line' 'Mic' Item0: 'Line' root:~> arecord -d 10 test.wav Recording WAVE "test.wav" : Unsigned 8 bit, Rate 8000 Hz, Mono root:~> aplay test.wavThis should record 10 seconds of whatever is on the Line, and then play it back over the output.
root:~> arecord | aplay
Most of the time, and issues we have seen have been tracked down to proper switch settings, which are detailed on bf527-ezkit getting started.
Name | Description | Model |
---|---|---|
LOUT | Line Output for Left Channel | SSM2602, SSM2603, SSM2604 |
ROUT | Line Output for Right Channel | SSM2602, SSM2603, SSM2604 |
LLINEIN | Line Input for Left Channel | SSM2602, SSM2603, SSM2604 |
RLINEIN | Line Input for Right Channel | SSM2602, SSM2603, SSM2604 |
LHPOUT | Headphone Output for Left Channel | SSM2602, SSM2603 |
RHPOUT | Headphone Output for Right Channel | SSM2602, SSM2603 |
MICIN | Microphone Input Signal | SSM2602, SSM2603 |
Name | Description | Model |
---|---|---|
Capture Volume | Line Input PGA Volume | SSM2602, SSM2603, SSM2604 |
Capture Switch | Mute/Unmute Line Input signal | SSM2602, SSM2603, SSM2604 |
ADC High Pass Filter Switch | Enable/Disable ADC high-pass filter | SSM2602, SSM2603, SSM2604 |
Store DC Offset Switch | Store dc offset when high-pass filter is disabled | SSM2602, SSM2603, SSM2604 |
Playback De-emphasis | Select playback de-emphasis. Possible values: “None”, “32Khz”, “44.1Khz”, “48Khz” | SSM2602, SSM2603, SSM2604 |
Master Playback Volume | Headphone volume | SSM2602, SSM2603 |
Master Playback ZC Switch | Enable/Disable zero cross detection for the playback volume | SSM2602, SSM2603 |
Sidetone Playback Volume | Microphone sidetone gain control | SSM2602, SSM2603 |
Mic Boost (+20dB) | Primary microphone amplifier gain booster control. | SSM2602, SSM2603 |
Mic Boost2 (+20dB) | Additional microphone amplifier gain booster control. | SSM2602, SSM2603 |
Mic Switch | Mute/Unmute the Microphone signal | SSM2602, SSM2603 |
Output Mixer Line Bypass Switch | Mix Line Input signal into the output signal | SSM2602, SSM2603, SSM2604 |
Output Mixer HiFi Playback Switch | Mix DAC signal into the output signal | SSM2602, SSM2603, SSM2604 |
Output Mixer Mic Sidetone Switch | Mix Microphone signal into the output signal | SSM2602, SSM2603 |
Input Select | Select the ADC input signal. Possible values: “Line”, “Mic” | SSM2602, SSM2603 |