This shows you the differences between two versions of the page.
Previous revisionNext revision | |||
— | resources:tools-software:linux-drivers:sound:adau1381 [16 Nov 2012 13:38] – [Evaluation Boards] add missing eval board Lars-Peter Clausen | ||
---|---|---|---|
Line 1: | Line 1: | ||
+ | ====== ADAU1781 Sound CODEC Linux Driver ====== | ||
+ | ===== Supported Devices ===== | ||
+ | |||
+ | * [[adi> | ||
+ | * [[adi> | ||
+ | |||
+ | ===== Evaluation Boards ===== | ||
+ | |||
+ | * [[adi> | ||
+ | * [[adi> | ||
+ | |||
+ | ====== Source Code ====== | ||
+ | |||
+ | ==== Status ==== | ||
+ | |||
+ | ^ Source | ||
+ | | [[bfgit> | ||
+ | |||
+ | ==== Files ==== | ||
+ | |||
+ | ^ Function ^ File ^ | ||
+ | | driver | ||
+ | | driver | ||
+ | | include | [[git.linux.org> | ||
+ | | include | [[git.linux.org> | ||
+ | |||
+ | ====== Example device initialization ====== | ||
+ | |||
+ | {{page> | ||
+ | |||
+ | ==== I2C ==== | ||
+ | |||
+ | {{page> | ||
+ | |||
+ | The I2C device id depends on the ADDR0 and ADDR1 pin settings and needs to be set according to your board setup. | ||
+ | |||
+ | ^ ADDR1 ^ ADDR0 ^ I2C device id ^ | ||
+ | | 0 | 0 | 0x38 | | ||
+ | | 0 | 1 | 0x39 | | ||
+ | | 1 | 0 | 0x3a | | ||
+ | | 1 | 1 | 0x3b | | ||
+ | |||
+ | In this example we assume ADDR0=0 and ADDR1=0. | ||
+ | |||
+ | <code c> | ||
+ | static struct i2c_board_info __initdata bfin_i2c_board_info[] = { | ||
+ | |||
+ | [--snip--] | ||
+ | { | ||
+ | I2C_BOARD_INFO(" | ||
+ | }, | ||
+ | [--snip--] | ||
+ | } | ||
+ | |||
+ | </ | ||
+ | |||
+ | <code c> | ||
+ | static int __init stamp_init(void) | ||
+ | { | ||
+ | [--snip--] | ||
+ | i2c_register_board_info(0, | ||
+ | ARRAY_SIZE(bfin_i2c_board_info)); | ||
+ | [--snip--] | ||
+ | |||
+ | return 0; | ||
+ | } | ||
+ | arch_initcall(board_init); | ||
+ | </ | ||
+ | |||
+ | ===== ASoC DAPM Widgets ===== | ||
+ | |||
+ | ^ Name ^ Description ^ | ||
+ | | AOUTL | Left Lineout Amplifier | | ||
+ | | AOUTR | Right Lineout Amplifier| | ||
+ | | SP | Speaker Amplifier | | ||
+ | | BEEP | Beep Signal Input | | ||
+ | | LMIC | Left Microphone Input or Digital Microphone Input 1 | | ||
+ | | RMIC | Right Microphone Input or Digital Microphone Input 2 | | ||
+ | | MICBIAS | Bias Voltage for Electret Microphone | | ||
+ | |||
+ | ===== ALSA Controls ===== | ||
+ | |||
+ | ^ Name ^ Description ^ | ||
+ | | ADC High Pass Filter Switch | Enable/ | ||
+ | | Playback De-emphasis | Enable/ | ||
+ | | Capture Boost | Mixer amplifier bias boost \\ Valid values: " | ||
+ | | Mic Bias Mode | Microphone bias.\\ Valid values: " | ||
+ | | DAC Mono Stereo | DAC mono mode.\\ | ||
+ | | DSP Bypass Capture Switch | Bypass DSP on the capture path and send ADC data directly to the serial ports | | ||
+ | | DSP Bypass Playback Switch | Bypass DSP on the playback path and send serial port data directly to the DACs | | ||
+ | | Digital Capture Volume | Digital volume attenuation for input from either the ADC or the digital microphone input. | | ||
+ | | Digital Playback Volume | Digital volume attenuation for output from the DAC | | ||
+ | | Beep Capture Volume | Beep input signal gain | | ||
+ | | Beep Capture Switch | Mute/Unmute Beep input signal | | ||
+ | | PGA Capture Volume | Analog Microphone input PGA Gain | | ||
+ | | PGA Capture Switch | Mute/Unmute Analog Microphone input | | ||
+ | | Lineout Playback Switch | Mute/Unmute Lineout | | ||
+ | | Beep ZC Switch | Enable Beep Zero Cross Detection | | ||
+ | | Mono Playback Switch | Mute/Unmute Mono(Speaker) output | | ||
+ | | Mono Playback Volume | Mono(Speaker) output gain | | ||
+ | | ADC Bias | ADC bias.\\ Valid values: " | ||
+ | | DAC Bias | DAC bias.\\ Valid values: " | ||
+ | | Capture Bias | Record path bias.\\ Valid values: " | ||
+ | | Playback Bias | Playback path bias.\\ Valid values: " | ||
+ | | Speaker Bias | Headphone bias.\\ Valid values: " | ||
+ | | Mono Mixer Left Switch | Mix Left DAC signal into the Mono Mixer | | ||
+ | | Mono Mixer Right Switch | Mix Right DAC signal into the Mono Mixer | | ||
+ | | Mono Mixer Beep Playback Volume | Beep signal gain into the Mono Mixer | | ||
+ | | Right Lineout Mixer Switch | Mix Right DAC signal into the Right Lineout Mixer | | ||
+ | | Right Lineout Mixer Beep Playback Volume | Beep signal gain into the Right Lineout Mixer | | ||
+ | | Left Lineout Mixer Switch | Mix Left DAC signal into the Left Lineout Mixer | | ||
+ | | Left Lineout Mixer Beep Playback Volume | Beep signal gain into the Left Lineout Mixer | | ||
+ | ===== PLL configuration ====== | ||
+ | |||
+ | The ADAU1781 features one PLL: | ||
+ | |||
+ | <code c> | ||
+ | enum adau17x1_pll { | ||
+ | ADAU17X1_PLL | ||
+ | }; | ||
+ | </ | ||
+ | |||
+ | The PLL input signal is the MCLK signal. | ||
+ | <code c> | ||
+ | enum adau1xx1_pll_src { | ||
+ | ADAU1XX1_PLL_SRC_MCLK, | ||
+ | }; | ||
+ | </ | ||
+ | |||
+ | (The input frequency must configured to be between 8000000 and 27000000 Hz (8MHz - 27MHz). The output frequency must be configured to be between 45158000 and 49152000. Configuring the PLL with other input or output frequency will fail.) | ||
+ | |||
+ | The PLL runs at 1024 times the base sample rate. So for a 48000 Hz based sample rate you'd normally choose 49152000 Hz for the PLL output frequncey and for a 44100 Hz based sample rate 45158400 Hz. | ||
+ | |||
+ | ===== DAI configuration ===== | ||
+ | |||
+ | The codec driver registers one DAI: **adau-hifi** | ||
+ | |||
+ | ==== Supported DAI formats ==== | ||
+ | |||
+ | ^ Name ^ Supported by driver ^ Description ^ | ||
+ | | SND_SOC_DAIFMT_I2S | ||
+ | | SND_SOC_DAIFMT_RIGHT_J | yes | Right Justified mode | | ||
+ | | SND_SOC_DAIFMT_LEFT_J | ||
+ | | SND_SOC_DAIFMT_DSP_A | ||
+ | | SND_SOC_DAIFMT_DSP_B | ||
+ | | SND_SOC_DAIFMT_AC97 | ||
+ | | SND_SOC_DAIFMT_PDM | ||
+ | | | | | ||
+ | | SND_SOC_DAIFMT_NB_NF | yes | Normal bit- and frameclock | | ||
+ | | SND_SOC_DAIFMT_NB_IF | yes | Normal bitclock, inverted frameclock | | ||
+ | | SND_SOC_DAIFMT_IB_NF | yes | Inverted frameclock, normal bitclock | | ||
+ | | SND_SOC_DAIFMT_IB_IF | yes | Inverted bit- and frameclock | | ||
+ | | | | | ||
+ | | SND_SOC_DAIFMT_CBM_CFM | yes | Codec bit- and frameclock master | | ||
+ | | SND_SOC_DAIFMT_CBS_CFM | no | Codec bitclock slave, frameclock master | | ||
+ | | SND_SOC_DAIFMT_CBM_CFS | no | Codec bitclock master, frameclock slave | | ||
+ | | SND_SOC_DAIFMT_CBS_CFS | yes | Codec bit- and frameclock slave | | ||
+ | |||
+ | ==== DAI sysclk ==== | ||
+ | |||
+ | The DAIs can either use the PLL or the MCLK signal as source. | ||
+ | |||
+ | When using the PLL the DAIs rate should be set to the rate of the PLL. When using MCLK the rate should be set to frequency of the external MCLK signal. | ||
+ | |||
+ | <code c> | ||
+ | enum adau17x1_clk_src { | ||
+ | ADAU17X1_CLK_SRC_MCLK, | ||
+ | ADAU17X1_CLK_SRC_PLL, | ||
+ | }; | ||
+ | </ | ||
+ | |||
+ | When using the MCLK as the DAI source it is possible to use an internal prescaler to divide the signals frequency. Valid divider values are 1, 2, 3 and 4. | ||
+ | |||
+ | Example clock divider configuration: | ||
+ | <code c> | ||
+ | ret = snd_soc_dai_set_clkdiv(codec_dai, | ||
+ | </ | ||
+ | |||
+ | ==== Example DAI configuration ==== | ||
+ | |||
+ | <code c> | ||
+ | static int bfin_eval_adau1x81_hw_params(struct snd_pcm_substream *substream, | ||
+ | struct snd_pcm_hw_params *params) | ||
+ | { | ||
+ | struct snd_soc_pcm_runtime *rtd = substream-> | ||
+ | struct snd_soc_dai *cpu_dai = rtd-> | ||
+ | struct snd_soc_dai *codec_dai = rtd-> | ||
+ | int pll_rate; | ||
+ | int ret; | ||
+ | |||
+ | ret = snd_soc_dai_set_fmt(cpu_dai, | ||
+ | SND_SOC_DAIFMT_NB_NF | SND_SOC_DAIFMT_CBM_CFM); | ||
+ | if (ret) | ||
+ | return ret; | ||
+ | |||
+ | ret = snd_soc_dai_set_fmt(codec_dai, | ||
+ | SND_SOC_DAIFMT_NB_NF | SND_SOC_DAIFMT_CBM_CFM); | ||
+ | if (ret) | ||
+ | return ret; | ||
+ | |||
+ | switch (params_rate(params)) { | ||
+ | case 48000: | ||
+ | case 8000: | ||
+ | case 12000: | ||
+ | case 16000: | ||
+ | case 24000: | ||
+ | case 32000: | ||
+ | pll_rate = 48000 * 1024; | ||
+ | break; | ||
+ | case 44100: | ||
+ | case 7350: | ||
+ | case 11025: | ||
+ | case 14700: | ||
+ | case 22050: | ||
+ | case 29400: | ||
+ | pll_rate = 44100 * 1024; | ||
+ | break; | ||
+ | default: | ||
+ | return -EINVAL; | ||
+ | } | ||
+ | |||
+ | ret = snd_soc_dai_set_pll(codec_dai, | ||
+ | ADAU17X1_PLL_SRC_MCLK, | ||
+ | if (ret) | ||
+ | return ret; | ||
+ | |||
+ | ret = snd_soc_dai_set_sysclk(codec_dai, | ||
+ | SND_SOC_CLOCK_IN); | ||
+ | |||
+ | return ret; | ||
+ | } | ||
+ | |||
+ | |||
+ | static struct snd_soc_ops bfin_eval_adau1x81_ops = { | ||
+ | .hw_params = bfin_eval_adau1x81_hw_params, | ||
+ | }; | ||
+ | |||
+ | static struct snd_soc_dai_link bfin_eval_adau1x81_dai = { | ||
+ | .name = " | ||
+ | .stream_name = " | ||
+ | .cpu_dai_name = " | ||
+ | .codec_dai_name = " | ||
+ | .platform_name = " | ||
+ | .codec_name = " | ||
+ | .ops = & | ||
+ | }; | ||
+ | </ | ||
+ | |||
+ | ===== TDM configuration ===== | ||
+ | |||
+ | The ADAU1381 and ADAU1781 chips have basic TDM support. | ||
+ | |||
+ | * The number of slots can be either 2, 4 or 8. | ||
+ | * The slot width can be 32, 64, 48, 128 or 256 | ||
+ | * The slot mask must be either 0x03 (slot 0 and 1), 0x0c (slot 2 and 3), 0x30 (slot 4 and 5), 0xc0 (slot 6 and 7) | ||
+ | |||
+ | Example TDM configuration: | ||
+ | <code c> | ||
+ | ret = snd_soc_dai_set_tdm_slot(codec_dai, | ||
+ | </ | ||
+ | |||
+ | ====== ADAU1X81 evaluation board driver ====== | ||
+ | |||
+ | There is no dedicated Blackfin STAMP evaluation board for the ADAU1381/ | ||
+ | |||
+ | It can be easily wired to the Blackfin STAMP SPORT header. | ||
+ | |||
+ | ===== Source ===== | ||
+ | |||
+ | ==== Status ==== | ||
+ | |||
+ | ^ Source | ||
+ | | [[bfgit> | ||
+ | |||
+ | ==== Files ==== | ||
+ | |||
+ | ^ Function ^ File ^ | ||
+ | | driver | ||
+ | |||
+ | ===== Kernel configuration ===== | ||
+ | |||
+ | < | ||
+ | Device Drivers | ||
+ | [*] I2C support | ||
+ | [*] I2C Hardware Bus support | ||
+ | *** I2C system bus drivers (mostly embedded / system-on-chip) *** | ||
+ | < | ||
+ | (100) | ||
+ | </ | ||
+ | |||
+ | Enable ALSA SoC evaluation board driver: | ||
+ | < | ||
+ | Device Drivers | ||
+ | <M> Sound card support | ||
+ | < | ||
+ | < | ||
+ | < | ||
+ | </ | ||
+ | |||
+ | ===== Hardware configuration ===== | ||
+ | |||
+ | Connect the STAMP SPORT 0 port (P6) to the EVAL-ADAU1X81 Control port(J1) and Serial Data Interface(J4) headers. | ||
+ | |||
+ | Note that the SPORT has separate signals for the capture and playback clocks, while the ADAU1381/ | ||
+ | |||
+ | ^ STAMP pin ^ EVAL-ADAU1X81 pin ^ Function ^ | ||
+ | | P6-26 (SPORT 0 - PJ2_SCL) | J1-1 | I2C SCL | | ||
+ | | P6-24 (SPORT 0 - PJ3_SDA) | J1-3 | I2C SDA | | ||
+ | | P6-6 (SPORT 0 - PJ9_TSCLK0), | ||
+ | | P6-11 (SPORT 0 - PJ10_TFS0), P6-7 (SPORT 0 - PJ7_RFS0) | J4-5| LRCLK | | ||
+ | | P6-8 (SPORT 0 - PJ8_DR0PRI) | J4-9 | Captrue data | | ||
+ | | P6-14 (SPORT 0 - PJ11_DT0PRI | J4-11 | Playback data | | ||
+ | | P6-33 | J4-2 | GND | | ||
+ | |||
+ | ===== Driver testing ===== | ||
+ | |||
+ | Load the driver and make sure the sound card is properly instantiated. | ||
+ | |||
+ | <box 100% green|shell prompt running on the target> | ||
+ | < | ||
+ | root:/> modprobe snd-bf5xx-i2s | ||
+ | root:/> modprobe snd-soc-bf5xx-i2s | ||
+ | root:/> modprobe snd-soc-adau1781 | ||
+ | root:/> modprobe snd-soc-bfin-eval-adau1x81 | ||
+ | bfin-i2s bfin-i2s.0: dma rx:3 tx:4, err irq:45, regs: | ||
+ | dma_alloc_init: | ||
+ | asoc: adau-hifi <-> bfin-i2s.0 mapping ok | ||
+ | ALSA device list: | ||
+ | #0: bfin-eval-adau1x81 | ||
+ | </ | ||
+ | </ | ||
+ | |||
+ | <box 100% green|shell prompt running on the target> | ||
+ | < | ||
+ | root:/> modprobe snd-pcm-oss | ||
+ | root:/> tone | ||
+ | TONE: generating sine wave at 1000 Hz... | ||
+ | |||
+ | root:/> arecord -f cd | aplay | ||
+ | Recording WAVE ' | ||
+ | Playing WAVE ' | ||
+ | </ | ||
+ | </ | ||
+ | |||
+ | ===== More information ===== | ||
+ | |||
+ | * [[resources/ | ||
+ | * [[resources/ | ||
+ | |||
+ | {{page> |