The ADL5960 is a wideband, vector network analyzer front-end that consists of a bidirectional bridge, downconverters, programmable IF amplifiers, and a configurable local oscillator (LO) interface.
This is a Linux industrial I/O (IIO) subsystem driver, targeting integrated Vector Network Analyzer Front-Ends. The industrial I/O subsystem provides a unified framework for drivers for many different types of converters and sensors using a number of different physical interfaces (i2c, spi, etc). See IIO for more information.
Function | File |
---|---|
driver | drivers/iio/frequency/adl5960.c |
Documentation | Documentation/ABI/testing/sysfs-bus-iio-frequency-adl5960 |
Documentation | Documentation/ABI/testing/sysfs-bus-iio |
dt-bindings | Documentation/devicetree/bindings/iio/frequency/adi,adl5960.yaml |
Unlike PCI or USB devices, SPI devices are not enumerated at the hardware level. Instead, the software must know which devices are connected on each SPI bus segment, and what slave selects these devices are using. For this reason, the kernel code must instantiate SPI devices explicitly. The most common method is to declare the SPI devices by bus number.
This method is appropriate when the SPI bus is a system bus, as in many embedded systems, wherein each SPI bus has a number which is known in advance. It is thus possible to pre-declare the SPI devices that inhabit this bus. This is done with an array of struct spi_board_info, which is registered by calling spi_register_board_info().
For more information see: Documentation/spi/spi-summary.rst
compatible: enum: - adi,adl5960
reg: maxItems: 1
spi-max-frequency: maximum: 50000000
clocks: description: Definition of the external clock (see clock/clock-bindings.txt) minItems: 2
clock-names: items: - const: lo_in - const: offs_in maxItems: 2
lo_in-clock-scales: description: The Common Clock Framework max rate is limited by MAX of unsigned long. For ADL5960 device this is a deficiency. If specified, this property allows arbitrary scales. The first element in the array should be the multiplier and the second element should be the divider. $ref: /schemas/types.yaml#/definitions/uint32-array minimum: 1
avcc-supply: description: analog voltage regulator (see regulator/regulator.txt)
'#clock-cells': const: 0
required: - compatible - reg - clocks - clock-names
spi { adl5960-1@0 { compatible = "adi,adl5960"; reg = <0>; spi-max-frequency = <12500000>; /* Clocks */ clocks = <&adf5610>, <&ad9528 4>; clock-names = "lo_in", "offs_in"; lo_in-clock-scales = <1 10>; label = "adl5960-1"; }; };
Configure kernel with “make menuconfig” (alternatively use “make xconfig” or “make qconfig”)
The ADL5960 Driver depends on CONFIG_SPI
Linux Kernel Configuration Device Drivers ---> <*> Industrial I/O support ---> --- Industrial I/O support RF Font-Ends ---> <*> Analog Devices ADL5960 Vector Network Analyzer Front-End"
Each and every IIO device, typically a hardware chip, has a device folder under /sys/bus/iio/devices/iio:deviceX. Where X is the IIO index of the device. Under every of these directory folders reside a set of files, depending on the characteristics and features of the hardware device in question. These files are consistently generalized and documented in the IIO ABI documentation. In order to determine which IIO deviceX corresponds to which hardware device, the user can read the name file /sys/bus/iio/devices/iio:deviceX/name. In case the sequence in which the iio device drivers are loaded/registered is constant, the numbering is constant and may be known in advance.
This specifies any shell prompt running on the target
root@analog:~# cd /sys/bus/iio/devices/ root@analog:/sys/bus/iio/devices# ls iio:device0 iio:device10 iio:device12 iio:device14 iio:device16 iio:device18 iio:device3 iio:device5 iio:device7 iio:device9 iio:device1 iio:device11 iio:device13 iio:device15 iio:device17 iio:device2 iio:device4 iio:device6 iio:device8 iio_sysfs_trigger root@analog:/sys/bus/iio/devices# grep “” */name iio:device0/name:ams iio:device1/name:adrf5720 iio:device10/name:adl5960 iio:device11/name:adl5960 iio:device12/name:adl5960 iio:device13/name:adl5960 iio:device14/name:adl5960 iio:device15/name:admv8818 iio:device16/name:iio-gen-mux iio:device17/name:iio-gen-mux iio:device18/name:admv8818 iio:device2/name:adrf5720 iio:device3/name:ad9528 iio:device4/name:adf5610 iio:device5/name:axi-ad9083-rx-hpc iio:device6/name:one-bit-adc-dac iio:device7/name:adl5960 iio:device8/name:adl5960 iio:device9/name:adl5960 root@analog:/sys/bus/iio/devices# cd iio:device7 root@analog:/sys/bus/iio/devices/iio:device7# ls -al total 0 drwxr-xr-x 3 root root 0 Mar 30 11:21 . drwxr-xr-x 5 root root 0 Mar 30 11:21 .. -rw-rw-rw- 1 root root 4096 Mar 30 11:21 dev -rw-rw-rw- 1 root root 4096 Mar 30 11:21 in_altvoltage0_lo_frequency -rw-rw-rw- 1 root root 4096 Mar 30 11:21 in_altvoltage0_lo_mode -rw-rw-rw- 1 root root 4096 Mar 30 11:21 in_altvoltage0_lo_mode_available -rw-rw-rw- 1 root root 4096 Mar 30 11:21 in_altvoltage1_if_frequency -rw-rw-rw- 1 root root 4096 Mar 30 11:21 in_altvoltage1_offset_frequency -rw-rw-rw- 1 root root 4096 Mar 30 11:21 in_altvoltage1_offset_mode -rw-rw-rw- 1 root root 4096 Mar 30 11:21 in_altvoltage1_offset_mode_available -rw-rw-rw- 1 root root 4096 Mar 30 11:21 in_temp0_input -rw-rw-rw- 1 root root 4096 Mar 30 11:21 label -rw-rw-rw- 1 root root 4096 Mar 30 11:21 name lrwxrwxrwx 1 root root 0 Mar 30 11:21 of_node -> ../../../../../../../../firmware/devicetree/base/fpga-axi@0/spi@88100000/adl5960-1@0 -rw-rw-rw- 1 root root 4096 Mar 30 11:21 out_voltage0_forward_hardwaregain -rw-rw-rw- 1 root root 4096 Mar 30 11:21 out_voltage1_reverse_hardwaregain -rw-rw-rw- 1 root root 4096 Mar 30 11:21 out_voltage_filter_low_pass_3db_frequency -rw-rw-rw- 1 root root 4096 Mar 30 11:21 out_voltage_hardwaregain_available drwxrwxrwx 2 root root 0 Mar 30 11:21 power lrwxrwxrwx 1 root root 0 Mar 30 11:21 subsystem -> ../../../../../../../../bus/iio -rw-rw-rw- 1 root root 4096 Mar 30 11:21 uevent root@analog:/sys/bus/iio/devices/iio:device7#
What: /sys/bus/iio/devices/iio:deviceX/in_altvoltage0_lo_frequency
Description:
Stores the Local Oscillator (LO) frequency in Hz.
Reading returns the actual frequency in Hz.
The values take the in_altvoltage0_lo_mode into account.
What: /sys/bus/iio/devices/iio:deviceX/in_altvoltage0_lo_mode
Description:
The frequency divider and multipliers in the LO interface
enable measurement sweeps beyond the operating frequency
range of the source driving the (LOP, LOM) pins.
This enables operation over the full 20 GHz bandwidth
of the ADL5960 using a 6 GHz synthesizer as the LO source.
This attribute Configures the LO path multiplier/divider or bypass. Reading returns the actual mode.
What: /sys/bus/iio/devices/iio:deviceX/in_altvoltage0_lo_mode_available
Description:
Reading this returns the valid values that can be written to the
in_altvoltage0_lo_mode attribute:
Value | Description |
---|---|
bypass | Bypasses the IF frequency mixer |
x1 | The external applied LO frequency is directly passed into the mixer |
x2 | The external applied LO frequency is doubled and passed into the mixer |
x4 | The external applied LO frequency is quadrupled and passed into the mixer |
/2 | The external applied LO frequency is divided and passed into the mixer |
What: /sys/bus/iio/devices/iio:deviceX/in_altvoltage1_offset_frequency
Description:
Stores the Offset frequency applied to the OFP, OFM inputs in Hz.
Reading returns the actual frequency in Hz.
The values do not take the in_altvoltage1_offset_mode into
account. Please see in_altvoltage1_if_frequency.
What: /sys/bus/iio/devices/iio:deviceX/in_altvoltage1_offset_mode
Description:
This attribute Configures the Offset path divider and modes.
Reading returns the actual mode.
What: /sys/bus/iio/devices/iio:deviceX/in_altvoltage1_offset_mode_available
Description:
Reading this returns the valid values that can be written to the
in_altvoltage1_offset_mode attribute:
Value | Description |
---|---|
bypass | Bypasses the IF frequency mixer |
off | Dividers are off, offset signal is disconnected |
x1 | The external applied OFFS frequency is directly passed into the mixer |
/2 | The external applied OFFS frequency is divided by 2 and passed into the mixer |
/4 | The external applied OFFS frequency is divided by 4 and passed into the mixer |
What: /sys/bus/iio/devices/iio:deviceX/in_altvoltage1_if_frequency
Description:
Stores the IF frequency applied to IF frequency offset mixer in Hz.
Reading returns the actual frequency in Hz.
The values take the in_altvoltage1_offset_mode into
account.
What: /sys/bus/iio/devices/iio:deviceX/out_voltage0_forward_hardwaregain
Description:
Stores the gain of the IF amplifier in the Forward path,
to the (IFFP, IFFM) output, in 6dB steps.
Reading returns the actual gain in dB.
What: /sys/bus/iio/devices/iio:deviceX/out_voltage1_reverse_hardwaregain
Description:
Stores the gain of the IF amplifier in the Reverse path,
to the (IFRP, IFRM) output, in 6dB steps.
Reading returns the actual gain in dB.
What: /sys/bus/iio/devices/iio:deviceX/out_voltage_filter_low_pass_3db_frequency
Description:
Stores the corner frequency of the narrow (CIF2) & wideband (CIF1)
bandwidth IF filter in Hz.
Reading returns the actual frequency in Hz.
What: /sys/bus/iio/devices/iio:deviceX/in_temp0_input
Description:
Scaled device (die) temperature measurement in milli degrees Celsius.