This is a Linux industrial I/O (IIO) subsystem driver, targeting multi-channel serial interface DACs. The industrial I/O subsystem provides a unified framework for drivers for many different types of converters and sensors using a number of different physical interfaces (i2c, spi, etc). See IIO for more information.
| Function | File |
|---|---|
| driver | drivers/iio/dac/ad5764.c |
Depending on the part it will either have an internal reference(AD5764R, AD5744R) or use an external reference(AD5764, AD5744) In case an external reference voltage is used the regulator framework must be used to provide the regulator supplys. The supplys must be be called “vrefAB” and “vrefCD”.
Below example specifies a 2.5 Volt reference for the SPI device 3 on SPI-Bus 0. (spi0.3)
#if IS_ENABLED(CONFIG_REGULATOR_FIXED_VOLTAGE) static struct regulator_consumer_supply ad5764_consumer_supplies[] = { REGULATOR_SUPPLY("vrefAB", "spi0.3"), REGULATOR_SUPPLY("vrefCD", "spi0.3"), }; static struct regulator_init_data stamp_avdd_reg_init_data = { .constraints = { .name = "2V5", .valid_ops_mask = REGULATOR_CHANGE_STATUS, }, .consumer_supplies = ad5764_consumer_supplies, .num_consumer_supplies = ARRAY_SIZE(ad5764_consumer_supplies), }; static struct fixed_voltage_config stamp_vdd_pdata = { .supply_name = "board-2V5", .microvolts = 2500000, .gpio = -EINVAL, .enabled_at_boot = 0, .init_data = &stamp_avdd_reg_init_data, }; static struct platform_device brd_voltage_regulator = { .name = "reg-fixed-voltage", .id = -1, .num_resources = 0, .dev = { .platform_data = &stamp_vdd_pdata, }, }; #endif
static struct platform_device *board_devices[] __initdata = { #if IS_ENABLED(CONFIG_REGULATOR_FIXED_VOLTAGE) &brd_voltage_regulator #endif };
static int __init board_init(void) { [--snip--] platform_add_devices(board_devices, ARRAY_SIZE(board_devices)); [--snip--] return 0; } arch_initcall(board_init);
Unlike PCI or USB devices, SPI devices are not enumerated at the hardware level. Instead, the software must know which devices are connected on each SPI bus segment, and what slave selects these devices are using. For this reason, the kernel code must instantiate SPI devices explicitly. The most common method is to declare the SPI devices by bus number.
This method is appropriate when the SPI bus is a system bus, as in many embedded systems, wherein each SPI bus has a number which is known in advance. It is thus possible to pre-declare the SPI devices that inhabit this bus. This is done with an array of struct spi_board_info, which is registered by calling spi_register_board_info().
For more information see: Documentation/spi/spi-summary
Depending on the converter IC used, you may need to set the modalias accordingly, matching your part name. It may also required to adjust max_speed_hz. Please consult the datasheet, for maximum spi clock supported by the device in question.
static struct spi_board_info board_spi_board_info[] __initdata = { #if IS_ENABLED(CONFIG_AD5764) { /* the modalias must be the same as spi device driver name */ .modalias = "ad5764", /* Name of spi_driver for this device */ .max_speed_hz = 1000000, /* max spi clock (SCK) speed in HZ */ .bus_num = 0, /* Framework bus number */ .chip_select = 3, /* Framework chip select */ .mode = SPI_MODE_1, }, #endif };
static int __init board_init(void) { [--snip--] spi_register_board_info(board_spi_board_info, ARRAY_SIZE(board_spi_board_info)); [--snip--] return 0; } arch_initcall(board_init);
Configure kernel with “make menuconfig” (alternatively use “make xconfig” or “make qconfig”)
The AD5764 Driver depends on CONFIG_SPI_MASTER
Linux Kernel Configuration
Device Drivers --->
...
<*> Industrial I/O support --->
--- Industrial I/O support
...
Digital to analog converters --->
...
<*> Analog Devices AD5764/64R/44/44R DAC drive
...
...
...
Each and every IIO device, typically a hardware chip, has a device folder under /sys/bus/iio/devices/iio:deviceX. Where X is the IIO index of the device. Under every of these directory folders reside a set of files, depending on the characteristics and features of the hardware device in question. These files are consistently generalized and documented in the IIO ABI documentation. In order to determine which IIO deviceX corresponds to which hardware device, the user can read the name file /sys/bus/iio/devices/iio:deviceX/name. In case the sequence in which the iio device drivers are loaded/registered is constant, the numbering is constant and may be known in advance.
This specifies any shell prompt running on the target
root:/> cd /sys/bus/iio/devices/ root:/sys/bus/iio/devices> ls iio:device0 root:/sys/bus/iio/devices> cd iio:device0 root:/sys/devices/platform/bfin-spi.0/spi0.3/iio:device0> ls -l -r--r--r-- 1 root root 4096 Jan 4 04:06 dev -r--r--r-- 1 root root 4096 Jan 4 04:06 name -rw-r--r-- 1 root root 4096 Jan 4 04:06 out_voltage0_calibbias -rw-r--r-- 1 root root 4096 Jan 4 04:06 out_voltage0_calibscale -rw-r--r-- 1 root root 4096 Jan 4 04:06 out_voltage0_raw -rw-r--r-- 1 root root 4096 Jan 4 04:06 out_voltage0_scale -rw-r--r-- 1 root root 4096 Jan 4 04:06 out_voltage1_calibbias -rw-r--r-- 1 root root 4096 Jan 4 04:06 out_voltage1_calibscale -rw-r--r-- 1 root root 4096 Jan 4 04:06 out_voltage1_raw -rw-r--r-- 1 root root 4096 Jan 4 04:06 out_voltage1_scale -rw-r--r-- 1 root root 4096 Jan 4 04:06 out_voltage2_calibbias -rw-r--r-- 1 root root 4096 Jan 4 04:06 out_voltage2_calibscale -rw-r--r-- 1 root root 4096 Jan 4 04:06 out_voltage2_raw -rw-r--r-- 1 root root 4096 Jan 4 04:06 out_voltage2_scale -rw-r--r-- 1 root root 4096 Jan 4 04:06 out_voltage3_calibbias -rw-r--r-- 1 root root 4096 Jan 4 04:06 out_voltage3_calibscale -rw-r--r-- 1 root root 4096 Jan 4 04:06 out_voltage3_raw -rw-r--r-- 1 root root 4096 Jan 4 04:06 out_voltage3_scale -rw-r--r-- 1 root root 4096 Jan 4 04:06 out_voltage_offset drwxr-xr-x 2 root root 0 Jan 4 04:06 power lrwxrwxrwx 1 root root 0 Jan 4 04:06 subsystem -> ../../../../../bus/iio -rw-r--r-- 1 root root 4096 Jan 4 04:06 uevent
This specifies any shell prompt running on the target
root:/sys/devices/platform/bfin-spi.0/spi0.3/iio:device0> cat name ad5764
Description:
/sys/bus/iio/devices/iio:deviceX/out_voltageY_scale
scale to be applied to out_voltageY_raw in order to obtain the measured voltage in millivolts.
This specifies any shell prompt running on the target
root:/sys/devices/platform/bfin-spi.0/spi0.3/iio:device0> cat out_voltage0_scale 0.305170
Description:
/sys/bus/iio/devices/iio:deviceX/out_offset_raw
Raw offset to be applied to out_voltage_raw in order to obtain the measured voltage in millivolts. The offset is applied before scale is applied.
This specifies any shell prompt running on the target
root:/sys/devices/platform/bfin-spi.0/spi0.3/iio:device0> cat out_voltage_offset -32768
Description:
/sys/bus/iio/devices/iio:deviceX/out_voltageY_raw
Raw (unscaled, no bias etc.) output voltage for channel Y.
This specifies any shell prompt running on the target
root:/sys/devices/platform/bfin-spi.0/spi0.3/iio:device0> echo 10000 > out_voltage0_raw
U = (out_voltage0_raw + out_voltage0_offset) * out_voltage0_scale = (10000 - 32768) * 0.305170 mV = -6948.11 mV
Description:
/sys/bus/iio/devices/iio:deviceX/out_voltageY_calibscale
Each channel has an adjustable gain which can be used to calibrate the channel's scale and compensate for full-scale errors. The default value is 0. The minimum value is -32, the maximum value is 31.
Description:
/sys/bus/iio/devices/iio:deviceX/out_voltageY_calibbias
Each channel has an adjustable offset which can be used to calibrate the channel's offset and compensate for zero-scale errors. The default value is 0. The minimum value is -128, the maximum value is 127.