This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:tools-software:linux-drivers:iio-amplifiers:ad8366 [15 Nov 2012 19:54] – [Evaluation Boards] Remove datasheet link Lars-Peter Clausen | resources:tools-software:linux-drivers:iio-amplifiers:ad8366 [16 Dec 2014 09:07] – [Supported Devices] Michael Hennerich | ||
---|---|---|---|
Line 4: | Line 4: | ||
* [[adi> | * [[adi> | ||
+ | * [[adi> | ||
===== Evaluation Boards ===== | ===== Evaluation Boards ===== | ||
Line 66: | Line 66: | ||
"make qconfig" | "make qconfig" | ||
- | <note> | + | <WRAP round help> |
The AD8366 Driver depends on **CONFIG_SPI** | The AD8366 Driver depends on **CONFIG_SPI** | ||
- | </note> | + | </WRAP> |
< | < | ||
Line 86: | Line 86: | ||
{{page> | {{page> | ||
- | < | + | <WRAP box bggreen>< |
< | < | ||
root:/> **cd / | root:/> **cd / | ||
Line 102: | Line 102: | ||
lrwxrwxrwx | lrwxrwxrwx | ||
-rw-r--r-- | -rw-r--r-- | ||
- | </ | + | </ |
=== Show device name === | === Show device name === | ||
- | < | + | <WRAP box bggreen>< |
< | < | ||
root:/> **cd / | root:/> **cd / | ||
root:/> **cat name** | root:/> **cat name** | ||
ad8366 | ad8366 | ||
- | </ | + | </ |
=== Set ChannelY Gain === | === Set ChannelY Gain === | ||
Line 121: | Line 121: | ||
< | < | ||
- | < | + | <WRAP box bggreen>< |
< | < | ||
root:/> **cat out_voltage0_hardwaregain** | root:/> **cat out_voltage0_hardwaregain** | ||
Line 129: | Line 129: | ||
root:/> **cat out_voltage0_hardwaregain** | root:/> **cat out_voltage0_hardwaregain** | ||
9.813000 dB | 9.813000 dB | ||
- | </ | + | </ |