world leader in high performance signal processing
This version (02 Apr 2013 11:59) was approved by larsc.The Previously approved version (18 Feb 2013 15:53) is available.Diff

AD7476A IIO Single Channel Serial ADC Linux Driver

Supported Devices

Reference Circuits

Evaluation Boards

Description

This is a Linux industrial I/O (IIO) subsystem driver, targeting single channel serial interface ADCs. The industrial I/O subsystem provides a unified framework for drivers for many different types of converters and sensors using a number of different physical interfaces (i2c, spi, etc). See IIO for more information.

Source Code

Status

Source Mainlined?
git Yes

Files

Function File
driver drivers/iio/adc/ad7476.c

Example platform device initialization

Specifying reference voltage via the regulator framework

Below example specifies a 3.3 Volt reference for the SPI device 3 on SPI-Bus 0. (spi0.3)

#if defined(CONFIG_REGULATOR_FIXED_VOLTAGE) || defined(CONFIG_REGULATOR_FIXED_VOLTAGE_MODULE)
static struct regulator_consumer_supply ad7476_consumer_supplies[] = {
	REGULATOR_SUPPLY("vcc", "spi0.3"),
};
 
static struct regulator_init_data stamp_avdd_reg_init_data = {
	.constraints	= {
		.name	= "3V3",
		.valid_ops_mask = REGULATOR_CHANGE_STATUS,
	},
	.consumer_supplies = ad7476_consumer_supplies,
	.num_consumer_supplies = ARRAY_SIZE(ad7476_consumer_supplies),
};
 
static struct fixed_voltage_config stamp_vdd_pdata = {
	.supply_name	= "board-3V3",
	.microvolts	= 3300000,
	.gpio		= -EINVAL,
	.enabled_at_boot = 0,
	.init_data	= &stamp_avdd_reg_init_data,
};
static struct platform_device brd_voltage_regulator = {
	.name		= "reg-fixed-voltage",
	.id		= -1,
	.num_resources	= 0,
	.dev		= {
		.platform_data	= &stamp_vdd_pdata,
	},
};
#endif
static struct platform_device *board_devices[] __initdata = {
#if defined(CONFIG_REGULATOR_FIXED_VOLTAGE) || defined(CONFIG_REGULATOR_FIXED_VOLTAGE_MODULE)
	&brd_voltage_regulator
#endif
};
static int __init board_init(void)
{
	[--snip--]
 
	platform_add_devices(board_devices, ARRAY_SIZE(board_devices));
 
	[--snip--]
 
	return 0;
}
arch_initcall(board_init);

Declaring SPI slave devices

Unlike PCI or USB devices, SPI devices are not enumerated at the hardware level. Instead, the software must know which devices are connected on each SPI bus segment, and what slave selects these devices are using. For this reason, the kernel code must instantiate SPI devices explicitly. The most common method is to declare the SPI devices by bus number.

This method is appropriate when the SPI bus is a system bus, as in many embedded systems, wherein each SPI bus has a number which is known in advance. It is thus possible to pre-declare the SPI devices that inhabit this bus. This is done with an array of struct spi_board_info, which is registered by calling spi_register_board_info().

For more information see: Documentation/spi/spi-summary

21 Oct 2010 16:10 · Michael Hennerich

Depending on the converter IC used, you may need to set the modalias accordingly, matching your part name. It may also required to adjust max_speed_hz. Please consult the datasheet, for maximum spi clock supported by the device in question.

static struct spi_board_info board_spi_board_info[] __initdata = {
#if defined(CONFIG_AD7476) || \
 	defined(CONFIG_AD7476_MODULE)
	{
		/* the modalias must be the same as spi device driver name */
		.modalias = "ad7476", /* Name of spi_driver for this device */
		.max_speed_hz = 1000000,     /* max spi clock (SCK) speed in HZ */
		.bus_num = 0, /* Framework bus number */
		.chip_select = 3, /* Framework chip select */
		.mode = SPI_MODE_3,
	},
#endif
};
static int __init board_init(void)
{
	[--snip--]
 
	spi_register_board_info(board_spi_board_info, ARRAY_SIZE(board_spi_board_info));
 
	[--snip--]
 
	return 0;
}
arch_initcall(board_init);

Devicetree

Required devicetree properties:

  • compatible: Needs to be “adi,” followed by the name of the device. E.g. “adi,ad7476a”
  • reg: The chipselect number used for the device
  • spi-max-frequency: Maximum SPI clock frequency.
  • spi-cpha: Needs to be set for the correct SPI mode
  • spi-cpol: Needs to be set for the correct SPI mode
  • vcc-supply: Phandle to the supply regulator
       adc_supply: fixedregulator {
               compatible = "regulator-fixed";
               regulator-name = "fixed-supply";
               regulator-min-microvolt = <3300000>;
               regulator-max-microvolt = <3300000>;
       };

       spi: spi@e0007000 {
               #address-cells = <1>;
               #size-cells = <0>;
               compatible = "xlnx,ps7-spi-1.00.a";
               ...

               ad7476@0 {
                       compatible = "adi,ad7476a";
                       reg = <0>;
                       spi-max-frequency = <1000000>;
                       spi-cpha;
                       spi-cpol;
                       vcc-supply = <&adc_supply>;
               };
        };

Adding Linux driver support

Configure kernel with “make menuconfig” (alternatively use “make xconfig” or “make qconfig”)

The AD7476 Driver depends on CONFIG_SPI

Linux Kernel Configuration
    Device Drivers  --->
        ...
        <*>     Industrial I/O support --->
            --- Industrial I/O support
            ...
            Analog to digital converters  ---> 
                ...
                <*>  Analog Devices AD7476 and similar 1-channel ADCs driver
                ...
            ...
        ...

Hardware configuration

Driver testing

Each and every IIO device, typically a hardware chip, has a device folder under /sys/bus/iio/devices/iio:deviceX. Where X is the IIO index of the device. Under every of these directory folders reside a set of files, depending on the characteristics and features of the hardware device in question. These files are consistently generalized and documented in the IIO ABI documentation. In order to determine which IIO deviceX corresponds to which hardware device, the user can read the name file /sys/bus/iio/devices/iio:deviceX/name. In case the sequence in which the iio device drivers are loaded/registered is constant, the numbering is constant and may be known in advance.

02 Mar 2011 15:16 · Michael Hennerich

This specifies any shell prompt running on the target

root:/> cd /sys/bus/iio/devices/
root:/sys/bus/iio/devices> ls
device0                  device0:buffer0:access0  trigger0
device0:buffer0          device0:buffer0:event0

root:/sys/bus/iio/devices> cd device0

root:/sys/devices/platform/bfin-spi.0/spi0.3/device0> ls -l
drwxr-xr-x    5 root     root             0 Jan  1 00:00 buffer
-r--r--r--    1 root     root          4096 Jan  1 00:00 in_voltage0_raw
-r--r--r--    1 root     root          4096 Jan  1 00:00 in_voltage_scale
-r--r--r--    1 root     root          4096 Jan  1 00:00 name
lrwxrwxrwx    1 root     root             0 Jan  1 00:00 subsystem -> ../../../../../bus/iio
drwxr-xr-x    2 root     root             0 Jan  1 00:00 trigger
-rw-r--r--    1 root     root          4096 Jan  1 00:00 uevent

Show device name

This specifies any shell prompt running on the target

root:/sys/devices/platform/bfin-spi.0/spi0.3/device0> cat name
ad7476

Show scale

Description:
scale to be applied to in_voltage0_raw in order to obtain the measured voltage in millivolts.

This specifies any shell prompt running on the target

root:/sys/devices/platform/bfin-spi.0/spi0.3/device0> cat in_voltage_scale
0.805

Show channel 0 measurement

Description:
Raw unscaled voltage measurement on channel 0

This specifies any shell prompt running on the target

root:/sys/devices/platform/bfin-spi.0/spi0.3/device0> cat in_voltage0_raw
2001

U = in_voltage0_raw * in_voltage_scale = 2001 * 0.805 = 1610,805 mV

Trigger management

If deviceX supports triggered sampling, it’s a so called trigger consumer and there will be an additional folder /sys/bus/iio/device/iio:deviceX/trigger. In this folder there is a file called current_trigger, allowing controlling and viewing the current trigger source connected to deviceX. Available trigger sources can be identified by reading the name file /sys/bus/iio/devices/triggerY/name. The same trigger source can connect to multiple devices, so a single trigger may initialize data capture or reading from a number of sensors, converters, etc.

Trigger Consumers:
Currently triggers are only used for the filling of software ring buffers and as such any device supporting INDIO_RING_TRIGGERED has the consumer interface automatically created.

Description: Read name of triggerY

This specifies any shell prompt running on the target

root:/sys/bus/iio/devices/triggerY/> cat name
irqtrig56

Description: Make irqtrig56 (trigger using system IRQ56, likely a GPIO IRQ), to current trigger of deviceX

This specifies any shell prompt running on the target

root:/sys/bus/iio/devices/iio:deviceX/trigger> echo irqtrig56 > current_trigger

Description: Read current trigger source of deviceX

This specifies any shell prompt running on the target

root:/sys/bus/iio/devices/iio:deviceX/trigger> cat current_trigger
irqtrig56

02 Mar 2011 15:16 · Michael Hennerich

Available standalone trigger drivers

name description
iio-trig-gpio Provides support for using GPIO pins as IIO triggers.
iio-trig-rtc Provides support for using periodic capable real time clocks as IIO triggers.
iio-trig-sysfs Provides support for using SYSFS entry as IIO triggers.
iio-trig-bfin-timer Provides support for using a Blackfin timer as IIO triggers.
02 Mar 2011 15:16 · Michael Hennerich

Buffer management

This specifies any shell prompt running on the target

root:/sys/devices/platform/bfin-spi.0/spi0.3/device0/device0:buffer0> ls
bytes_per_datum          enable                   subsystem
device0:buffer0:access0  length                   uevent
device0:buffer0:event0   scan_elements
root:/sys/devices/platform/bfin-spi.0/spi0.3/device0/device0:buffer0>

The Industrial I/O subsystem provides support for various ring buffer based data acquisition methods. Apart from device specific hardware buffer support, the user can chose between two different software ring buffer implementations. One is the IIO lock free software ring, and the other is based on Linux kfifo. Devices with buffer support feature an additional sub-folder in the /sys/bus/iio/devices/deviceX/ folder hierarchy. Called deviceX:bufferY, where Y defaults to 0, for devices with a single buffer.

Every buffer implementation features a set of files:

length
Get/set the number of sample sets that may be held by the buffer.

enable
Enables/disables the buffer. This file should be written last, after length and selection of scan elements.

scan_elements
The scan_elements directory contains interfaces for elements that will be captured for a single triggered sample set in the buffer.

02 Mar 2011 15:16 · Michael Hennerich

This specifies any shell prompt running on the target

root:/sys/devices/platform/bfin-spi.0/spi0.3/device0/device0:buffer0/scan_elements> ls
in0_en           in_type          timestamp_index
in0_index        timestamp_en     timestamp_type
root:/sys/devices/platform/bfin-spi.0/spi0.3/device0/device0:buffer0/scan_elements>

in_voltageX_en / in_voltageX-voltageY_en / timestamp_en:
Scan element control for triggered data capture. Writing 1 will enable the scan element, writing 0 will disable it

in_voltageX_type / in_voltageX-voltageY_type / timestamp_type:
Description of the scan element data storage within the buffer and therefore in the form in which it is read from user-space. Form is [s|u]bits/storage-bits. s or u specifies if signed (2's complement) or unsigned. bits is the number of bits of data and storage-bits is the space (after padding) that it occupies in the buffer. Note that some devices will have additional information in the unused bits so to get a clean value, the bits value must be used to mask the buffer output value appropriately. The storage-bits value also specifies the data alignment. So u12/16 will be a unsigned 12 bit integer stored in a 16 bit location aligned to a 16 bit boundary. For other storage combinations this attribute will be extended appropriately.

in_voltageX_index / in_voltageX-voltageY_index / timestamp_index:
A single positive integer specifying the position of this scan element in the buffer. Note these are not dependent on what is enabled and may not be contiguous. Thus for user-space to establish the full layout these must be used in conjunction with all _en attributes to establish which channels are present, and the relevant _type attributes to establish the data storage format.

02 Mar 2011 15:16 · Michael Hennerich

More Information