This is a Linux industrial I/O (IIO) subsystem driver, targeting multi channel serial interface ADCs. The industrial I/O subsystem provides a unified framework for drivers for many different types of converters and sensors using a number of different physical interfaces (i2c, spi, etc). See IIO for more information.
| Function | File |
|---|---|
| driver | drivers/staging/iio/adc/ad7291.c |
In case the AD7291 on-chip 2.5V reference is not used, this driver requires specifying the reference voltage, by using the Linux regulator framework.
Below example specifies a 3.3 Volt reference for the I2C device 0-002a on I2C-Bus 0. (0-002a)
#if defined(CONFIG_REGULATOR_FIXED_VOLTAGE) || defined(CONFIG_REGULATOR_FIXED_VOLTAGE_MODULE) static struct regulator_consumer_supply ad7291_consumer_supplies[] = { REGULATOR_SUPPLY("vcc", "0-002a"), }; static struct regulator_init_data board_avdd_reg_init_data = { .constraints = { .name = "3V3", .valid_ops_mask = REGULATOR_CHANGE_STATUS, }, .consumer_supplies = ad7291_consumer_supplies, .num_consumer_supplies = ARRAY_SIZE(ad7291_consumer_supplies), }; static struct fixed_voltage_config board_vdd_pdata = { .supply_name = "board-3V3", .microvolts = 3300000, .gpio = -EINVAL, .enabled_at_boot = 0, .init_data = &board_avdd_reg_init_data, }; static struct platform_device brd_voltage_regulator = { .name = "reg-fixed-voltage", .id = -1, .num_resources = 0, .dev = { .platform_data = &board_vdd_pdata, }, }; #endif
static struct platform_device *board_devices[] __initdata = { #if defined(CONFIG_REGULATOR_FIXED_VOLTAGE) || defined(CONFIG_REGULATOR_FIXED_VOLTAGE_MODULE) &brd_voltage_regulator #endif };
static int __init board_init(void) { [--snip--] platform_add_devices(board_devices, ARRAY_SIZE(board_devices)); [--snip--] return 0; } arch_initcall(board_init);
Unlike PCI or USB devices, I2C devices are not enumerated at the hardware level. Instead, the software must know which devices are connected on each I2C bus segment, and what address these devices are using. For this reason, the kernel code must instantiate I2C devices explicitly. There are different ways to achieve this, depending on the context and requirements. However the most common method is to declare the I2C devices by bus number.
This method is appropriate when the I2C bus is a system bus, as in many embedded systems, wherein each I2C bus has a number which is known in advance. It is thus possible to pre-declare the I2C devices that inhabit this bus. This is done with an array of struct i2c_board_info, which is registered by calling i2c_register_board_info().
So, to enable such a driver one need only edit the board support file by adding an appropriate entry to i2c_board_info.
For more information see: Documentation/i2c/instantiating-devices
Depending on the converter IC used, you may need to set the I2C_BOARD_INFO name accordingly, matching your part name.
static struct i2c_board_info __initdata board_i2c_board_info[] = { #if defined(CONFIG_AD7291) || defined(CONFIG_AD7291_MODULE) { I2C_BOARD_INFO("ad7291", 0x2A), .irq = IRQ_PG14, }, #endif };
static int __init board_init(void) { [--snip--] i2c_register_board_info(0, board_i2c_board_info, ARRAY_SIZE(board_i2c_board_info)); [--snip--] return 0; } arch_initcall(board_init);
Configure kernel with “make menuconfig” (alternatively use “make xconfig” or “make qconfig”)
The driver depends on CONFIG_I2C
Linux Kernel Configuration Device Drivers ---> [*] Staging drivers ---> <*> Industrial I/O support ---> --- Industrial I/O support -*- Enable ring buffer support within IIO -*- Industrial I/O lock free software ring -*- Enable triggered sampling support *** Analog to digital converters *** [--snip--] <*> Analog Devices AD7291 ADC driver [--snip--]
Each and every IIO device, typically a hardware chip, has a device folder under /sys/bus/iio/devices/iio:deviceX. Where X is the IIO index of the device. Under every of these directory folders reside a set of files, depending on the characteristics and features of the hardware device in question. These files are consistently generalized and documented in the IIO ABI documentation. In order to determine which IIO deviceX corresponds to which hardware device, the user can read the name file /sys/bus/iio/devices/iio:deviceX/name. In case the sequence in which the iio device drivers are loaded/registered is constant, the numbering is constant and may be known in advance.
This specifies any shell prompt running on the target
root:/> cd /sys/bus/iio/devices/ root:/sys/bus/iio/devices> ls iio:device0 root:/sys/bus/iio/devices> cd iio:device0 root:/sys/devices/platform/i2c-bfin-twi.0/i2c-0/0-002a/iio:device0> ls -l -r--r--r-- 1 root root 4096 Jan 1 00:38 dev drwxr-xr-x 2 root root 0 Jan 1 00:38 events -rw-r--r-- 1 root root 4096 Jan 1 00:38 in_temp0_mean_raw -r--r--r-- 1 root root 4096 Jan 1 00:38 in_temp0_raw -rw-r--r-- 1 root root 4096 Jan 1 00:38 in_temp0_scale -r--r--r-- 1 root root 4096 Jan 1 00:38 in_voltage0_raw -r--r--r-- 1 root root 4096 Jan 1 00:38 in_voltage1_raw -r--r--r-- 1 root root 4096 Jan 1 00:38 in_voltage2_raw -r--r--r-- 1 root root 4096 Jan 1 00:38 in_voltage3_raw -r--r--r-- 1 root root 4096 Jan 1 00:38 in_voltage4_raw -r--r--r-- 1 root root 4096 Jan 1 00:38 in_voltage5_raw -r--r--r-- 1 root root 4096 Jan 1 00:38 in_voltage6_raw -r--r--r-- 1 root root 4096 Jan 1 00:38 in_voltage7_raw -rw-r--r-- 1 root root 4096 Jan 1 00:38 in_voltage_scale -r--r--r-- 1 root root 4096 Jan 1 00:38 name drwxr-xr-x 2 root root 0 Jan 1 00:38 power --w------- 1 root root 4096 Jan 1 00:38 reset lrwxrwxrwx 1 root root 0 Jan 1 00:38 subsystem -> ../../../../../../bus/iio -rw-r--r-- 1 root root 4096 Jan 1 00:38 uevent
This specifies any shell prompt running on the target
root:/sys/devices/platform/i2c-bfin-twi.0/i2c-0/0-002a/iio:device0> cat name ad7291
Description:
scale to be applied to in_voltageX_raw in order to obtain the measured voltage in millivolts.
This specifies any shell prompt running on the target
root:/sys/devices/platform/i2c-bfin-twi.0/i2c-0/0-002a/iio:device0> cat in_voltage_scale 0.610000
Description:
Raw unscaled voltage measurement on channel 0
| ADC Input | Channel name |
|---|---|
| VIN0 | in_voltage0_raw |
| VIN1 | in_voltage1_raw |
| VIN2 | in_voltage2_raw |
| VIN3 | in_voltage3_raw |
| VIN4 | in_voltage4_raw |
| VIN5 | in_voltage5_raw |
| VIN6 | in_voltage6_raw |
| VIN7 | in_voltage7_raw |
This specifies any shell prompt running on the target
root:/sys/devices/platform/i2c-bfin-twi.0/i2c-0/0-002a/iio:device0> cat in_voltage0_raw 1641
U = in_voltage0_raw * in_voltage_scale = 1641 * 0.610000 = 1001,01 mV
Description: /sys/bus/iio/devices/iio:deviceX/in_temp0_raw
Shows raw unscaled temperature.
| Channel name | Description |
|---|---|
| in_temp0_raw | Current temperature |
| in_temp0_mean_raw | Averaged temperature |
This specifies any shell prompt running on the target
root:/sys/devices/platform/i2c-bfin-twi.0/i2c-0/0-002a/iio:device0> cat in_temp0_raw 107 root:/sys/devices/platform/i2c-bfin-twi.0/i2c-0/0-002a/iio:device0> cat in_temp0_scale 250
T = in_temp0_raw * in_temp0_scale = 107 * 250 = 26750 = 26.75 °C
The Industrial I/O subsystem provides support for passing hardware generated events up to userspace.
In IIO events are not used for passing normal readings from the sensing devices to userspace, but rather for out of band information. Normal data reaches userspace through a low overhead character device - typically via either software or hardware buffer. The stream format is pseudo fixed, so is described and controlled via sysfs rather than adding headers to the data describing what is in it.
Pretty much all IIO events correspond to thresholds on some value derived from one or more raw readings from the sensor. They are provided by the underlying hardware.
Examples include:
Events have timestamps.
The Interface:
The format is:
/** * struct iio_event_data - The actual event being pushed to userspace * @id: event identifier * @timestamp: best estimate of time of event occurrence (often from * the interrupt handler) */ struct iio_event_data { u64 id; s64 timestamp; };
/sys/bus/iio/devices/iio:deviceX/events
Configuration of which hardware generated events are passed up
to user-space.
<type>Z[_name]_thresh[_rising|falling]_en
Event generated when channel passes a threshold in the specified
(_rising|_falling) direction. If the direction is not specified,
then either the device will report an event which ever direction
a single threshold value is called in (e.g.
<type>[Z][_name]_<raw|input>_thresh_value) or
<type>[Z][_name]_<raw|input>_thresh_rising_value and
<type>[Z][_name]_<raw|input>_thresh_falling_value may take
different values, but the device can only enable both thresholds
or neither.
Note the driver will assume the last p events requested are
to be enabled where p is however many it supports (which may
vary depending on the exact set requested. So if you want to be
sure you have set what you think you have, check the contents of
these attributes after everything is configured. Drivers may
have to buffer any parameters so that they are consistent when
a given event type is enabled a future point (and not those for
whatever event was previously enabled).
<type>Z[_name]_thresh[_rising|falling]_value
Specifies the value of threshold that the device is comparing
against for the events enabled by
<type>Z[_name]_thresh[_rising|falling]_en.
If separate attributes exist for the two directions, but
direction is not specified for this attribute, then a single
threshold value applies to both directions.
The raw or input element of the name indicates whether the
value is in raw device units or in processed units (as _raw
and _input do on sysfs direct channel read attributes).
<type>[Z][_name]_roc[_rising|falling]_en
Event generated when channel passes a threshold on the rate of
change (1st differential) in the specified (_rising|_falling)
direction. If the direction is not specified, then either the
device will report an event which ever direction a single
threshold value is called in (e.g.
<type>[Z][_name]_<raw|input>_roc_value) or
<type>[Z][_name]_<raw|input>_roc_rising_value and
<type>[Z][_name]_<raw|input>_roc_falling_value may take
different values, but the device can only enable both rate of
change thresholds or neither.
Note the driver will assume the last p events requested are
to be enabled where p is however many it supports (which may
vary depending on the exact set requested. So if you want to be
sure you have set what you think you have, check the contents of
these attributes after everything is configured. Drivers may
have to buffer any parameters so that they are consistent when
a given event type is enabled a future point (and not those for
whatever event was previously enabled).
<type>[Z][_name]_roc[_rising|falling]_value
Specifies the value of rate of change threshold that the
device is comparing against for the events enabled by
<type>[Z][_name]_roc[_rising|falling]_en.
If separate attributes exist for the two directions,
but direction is not specified for this attribute,
then a single threshold value applies to both directions.
The raw or input element of the name indicates whether the
value is in raw device units or in processed units (as _raw
and _input do on sysfs direct channel read attributes).
<type>Z[_name]_mag[_rising|falling]_en
Similar to in_accel_x_thresh[_rising|_falling]_en, but here the
magnitude of the channel is compared to the threshold, not its
signed value.
<type>Z[_name]_mag[_rising|falling]_value
The value to which the magnitude of the channel is compared. If
number or direction is not specified, applies to all channels of
this type.
<type>[Z][_name][_thresh|_roc][_rising|falling]_period
Period of time (in seconds) for which the condition must be
met before an event is generated. If direction is not
specified then this period applies to both directions.
| Event Attributes |
|---|
| Channel Temp |
| in_temp0_thresh_both_hyst_raw |
| in_temp0_thresh_falling_en |
| in_temp0_thresh_falling_value |
| in_temp0_thresh_rising_en |
| in_temp0_thresh_rising_value |
| Channel VIN0 |
| in_voltage0_thresh_both_hyst_raw |
| in_voltage0_thresh_falling_en |
| in_voltage0_thresh_falling_value |
| in_voltage0_thresh_rising_en |
| in_voltage0_thresh_rising_value |
| Channel VIN1 |
| in_voltage1_thresh_both_hyst_raw |
| in_voltage1_thresh_falling_en |
| in_voltage1_thresh_falling_value |
| in_voltage1_thresh_rising_en |
| in_voltage1_thresh_rising_value |
| Channel VIN2 |
| in_voltage2_thresh_both_hyst_raw |
| in_voltage2_thresh_falling_en |
| in_voltage2_thresh_falling_value |
| in_voltage2_thresh_rising_en |
| in_voltage2_thresh_rising_value |
| Channel VIN3 |
| in_voltage3_thresh_both_hyst_raw |
| in_voltage3_thresh_falling_en |
| in_voltage3_thresh_falling_value |
| in_voltage3_thresh_rising_en |
| in_voltage3_thresh_rising_value |
| Channel VIN4 |
| in_voltage4_thresh_both_hyst_raw |
| in_voltage4_thresh_falling_en |
| in_voltage4_thresh_falling_value |
| in_voltage4_thresh_rising_en |
| in_voltage4_thresh_rising_value |
| Channel VIN5 |
| in_voltage5_thresh_both_hyst_raw |
| in_voltage5_thresh_falling_en |
| in_voltage5_thresh_falling_value |
| in_voltage5_thresh_rising_en |
| in_voltage5_thresh_rising_value |
| Channel VIN6 |
| in_voltage6_thresh_both_hyst_raw |
| in_voltage6_thresh_falling_en |
| in_voltage6_thresh_falling_value |
| in_voltage6_thresh_rising_en |
| in_voltage6_thresh_rising_value |
| Channel VIN7 |
| in_voltage7_thresh_both_hyst_raw |
| in_voltage7_thresh_falling_en |
| in_voltage7_thresh_falling_value |
| in_voltage7_thresh_rising_en |
| in_voltage7_thresh_rising_value |