This is a Linux industrial I/O (IIO) subsystem driver, targeting multi channel serial interface ADCs. The industrial I/O subsystem provides a unified framework for drivers for many different types of converters and sensors using a number of different physical interfaces (i2c, spi, etc). See IIO for more information.
The AD7280A contains all the functions required for general-purpose monitoring of stacked lithium ion batteries as used in hybrid electric vehicles, battery backup applications, and power tools. The part has multiplexed cell voltage and auxiliary ADC measurement channels for up to six cells of battery management. This driver supports the daisy-chain interface allowing up to eight parts to be stacked without the need for individual device isolation.
The driver automatically detects then number of devices present and creates the iio device files accordingly.
| Function | File |
|---|---|
| driver | drivers/staging/iio/adc/ad7280a.c |
| include | drivers/staging/iio/adc/ad7280a.h |
For compile time configuration, it’s common Linux practice to keep board- and application-specific configuration out of the main driver file, instead putting it into the board support file.
For devices on custom boards, as typical of embedded and SoC-(system-on-chip) based hardware, Linux uses platform_data to point to board-specific structures describing devices and how they are connected to the SoC. This can include available ports, chip variants, preferred modes, default initialization, additional pin roles, and so on. This shrinks the board-support packages (BSPs) and minimizes board and application specific #ifdefs in drivers.
Some device parameter may vary between applications and use cases. The platform_data for the device's “struct device” holds this information.
#define AD7280A_ACQ_TIME_400ns 0 #define AD7280A_ACQ_TIME_800ns 1 #define AD7280A_ACQ_TIME_1200ns 2 #define AD7280A_ACQ_TIME_1600ns 3 #define AD7280A_CONV_AVG_DIS 0 #define AD7280A_CONV_AVG_2 1 #define AD7280A_CONV_AVG_4 2 #define AD7280A_CONV_AVG_8 3 #define AD7280A_ALERT_REMOVE_VIN5 (1 << 2) #define AD7280A_ALERT_REMOVE_VIN4_VIN5 (2 << 2) #define AD7280A_ALERT_REMOVE_AUX5 (1 << 0) #define AD7280A_ALERT_REMOVE_AUX4_AUX5 (2 << 0) struct ad7280_platform_data { unsigned acquisition_time; unsigned conversion_averaging; unsigned chain_last_alert_ignore; bool thermistor_term_en; }
In case platform_data is not present or set to NULL, the driver will use following defaults:
static const struct ad7280_platform_data ad7280_default_pdata = { .acquisition_time = AD7280A_ACQ_TIME_400ns, .conversion_averaging = AD7280A_CONV_AVG_DIS, .thermistor_term_en = true, };
Unlike PCI or USB devices, SPI devices are not enumerated at the hardware level. Instead, the software must know which devices are connected on each SPI bus segment, and what slave selects these devices are using. For this reason, the kernel code must instantiate SPI devices explicitly. The most common method is to declare the SPI devices by bus number.
This method is appropriate when the SPI bus is a system bus, as in many embedded systems, wherein each SPI bus has a number which is known in advance. It is thus possible to pre-declare the SPI devices that inhabit this bus. This is done with an array of struct spi_board_info, which is registered by calling spi_register_board_info().
For more information see: Documentation/spi/spi-summary
Depending on the converter IC used, you may need to set the modalias accordingly, matching your part name. It may also required to adjust max_speed_hz. Please consult the datasheet, for maximum spi clock supported by the device in question.
static struct spi_board_info board_spi_board_info[] __initdata = { #if defined(CONFIG_AD7280A) || \ defined(CONFIG_AD7280A_MODULE) { .modalias = "ad7280a", .max_speed_hz = 1000000, /* max spi clock (SCK) speed in HZ */ .bus_num = 0, .chip_select = GPIO_PF10 + MAX_CTRL_CS, /* CS, change it for your board */ .mode = SPI_MODE_1, .irq = IRQ_PF6 }, #endif };
static int __init board_init(void) { [--snip--] spi_register_board_info(board_spi_board_info, ARRAY_SIZE(board_spi_board_info)); [--snip--] return 0; } arch_initcall(board_init);
Configure kernel with “make menuconfig” (alternatively use “make xconfig” or “make qconfig”)
The AD7280A Driver depends on CONFIG_SPI
Linux Kernel Configuration Device Drivers ---> [*] Staging drivers ---> <*> Industrial I/O support ---> --- Industrial I/O support -*- Enable ring buffer support within IIO -*- Industrial I/O lock free software ring -*- Enable triggered sampling support *** Analog to digital converters *** [--snip--] <*> Analog Devices AD7280A Lithium Ion Battery Monitoring System [--snip--]
Each and every IIO device, typically a hardware chip, has a device folder under /sys/bus/iio/devices/iio:deviceX. Where X is the IIO index of the device. Under every of these directory folders reside a set of files, depending on the characteristics and features of the hardware device in question. These files are consistently generalized and documented in the IIO ABI documentation. In order to determine which IIO deviceX corresponds to which hardware device, the user can read the name file /sys/bus/iio/devices/iio:deviceX/name. In case the sequence in which the iio device drivers are loaded/registered is constant, the numbering is constant and may be known in advance.
This specifies any shell prompt running on the target
root:/> cd /sys/bus/iio/devices/ root:/sys/bus/iio/devices> ls device0 device0:event0 root:/sys/bus/iio/devices> cd device0 root:/sys/devices/platform/bfin-spi.0/spi0.18/device0> ls -l drwxr-xr-x 3 root root 0 Mar 14 11:16 device0:event0 -rw-r--r-- 1 root root 4096 Mar 14 11:16 in-in_scale -r--r--r-- 1 root root 4096 Mar 14 11:16 in0-in12_raw -rw-r--r-- 1 root root 4096 Mar 14 11:16 in0-in1_balance_switch_en -rw-r--r-- 1 root root 4096 Mar 14 11:16 in0-in1_balance_timer -r--r--r-- 1 root root 4096 Mar 14 11:16 in0-in1_raw -rw-r--r-- 1 root root 4096 Mar 14 11:16 in1-in2_balance_switch_en -rw-r--r-- 1 root root 4096 Mar 14 11:16 in1-in2_balance_timer -r--r--r-- 1 root root 4096 Mar 14 11:16 in1-in2_raw -rw-r--r-- 1 root root 4096 Mar 14 11:16 in10-in11_balance_switch_en -rw-r--r-- 1 root root 4096 Mar 14 11:16 in10-in11_balance_timer -r--r--r-- 1 root root 4096 Mar 14 11:16 in10-in11_raw -rw-r--r-- 1 root root 4096 Mar 14 11:16 in11-in12_balance_switch_en -rw-r--r-- 1 root root 4096 Mar 14 11:16 in11-in12_balance_timer -r--r--r-- 1 root root 4096 Mar 14 11:16 in11-in12_raw -rw-r--r-- 1 root root 4096 Mar 14 11:16 in2-in3_balance_switch_en -rw-r--r-- 1 root root 4096 Mar 14 11:16 in2-in3_balance_timer -r--r--r-- 1 root root 4096 Mar 14 11:16 in2-in3_raw -rw-r--r-- 1 root root 4096 Mar 14 11:16 in3-in4_balance_switch_en -rw-r--r-- 1 root root 4096 Mar 14 11:16 in3-in4_balance_timer -r--r--r-- 1 root root 4096 Mar 14 11:16 in3-in4_raw -rw-r--r-- 1 root root 4096 Mar 14 11:16 in4-in5_balance_switch_en -rw-r--r-- 1 root root 4096 Mar 14 11:16 in4-in5_balance_timer -r--r--r-- 1 root root 4096 Mar 14 11:16 in4-in5_raw -rw-r--r-- 1 root root 4096 Mar 14 11:16 in5-in6_balance_switch_en -rw-r--r-- 1 root root 4096 Mar 14 11:16 in5-in6_balance_timer -r--r--r-- 1 root root 4096 Mar 14 11:16 in5-in6_raw -rw-r--r-- 1 root root 4096 Mar 14 11:16 in6-in7_balance_switch_en -rw-r--r-- 1 root root 4096 Mar 14 11:16 in6-in7_balance_timer -r--r--r-- 1 root root 4096 Mar 14 11:16 in6-in7_raw -rw-r--r-- 1 root root 4096 Mar 14 11:16 in7-in8_balance_switch_en -rw-r--r-- 1 root root 4096 Mar 14 11:16 in7-in8_balance_timer -r--r--r-- 1 root root 4096 Mar 14 11:16 in7-in8_raw -rw-r--r-- 1 root root 4096 Mar 14 11:16 in8-in9_balance_switch_en -rw-r--r-- 1 root root 4096 Mar 14 11:16 in8-in9_balance_timer -r--r--r-- 1 root root 4096 Mar 14 11:16 in8-in9_raw -rw-r--r-- 1 root root 4096 Mar 14 11:16 in9-in10_balance_switch_en -rw-r--r-- 1 root root 4096 Mar 14 11:16 in9-in10_balance_timer -r--r--r-- 1 root root 4096 Mar 14 11:16 in9-in10_raw -r--r--r-- 1 root root 4096 Mar 14 11:16 name drwxr-xr-x 2 root root 0 Mar 14 11:16 power lrwxrwxrwx 1 root root 0 Mar 14 11:16 subsystem -> ../../../../../bus/iio -r--r--r-- 1 root root 4096 Mar 14 11:16 temp0_raw -r--r--r-- 1 root root 4096 Mar 14 11:16 temp10_raw -r--r--r-- 1 root root 4096 Mar 14 11:16 temp11_raw -r--r--r-- 1 root root 4096 Mar 14 11:16 temp1_raw -r--r--r-- 1 root root 4096 Mar 14 11:16 temp2_raw -r--r--r-- 1 root root 4096 Mar 14 11:16 temp3_raw -r--r--r-- 1 root root 4096 Mar 14 11:16 temp4_raw -r--r--r-- 1 root root 4096 Mar 14 11:16 temp5_raw -r--r--r-- 1 root root 4096 Mar 14 11:16 temp6_raw -r--r--r-- 1 root root 4096 Mar 14 11:16 temp7_raw -r--r--r-- 1 root root 4096 Mar 14 11:16 temp8_raw -r--r--r-- 1 root root 4096 Mar 14 11:16 temp9_raw -rw-r--r-- 1 root root 4096 Mar 14 11:16 temp_scale -rw-r--r-- 1 root root 4096 Mar 14 11:16 uevent root:/sys/devices/platform/bfin-spi.0/spi0.18/device0>
This specifies any shell prompt running on the target
root:/sys/devices/platform/bfin-spi.0/spi0.18/device0> cat name ad7280a
Description:
scale to be applied to inX-inY_raw in order to obtain the measured voltage in millivolts.
This specifies any shell prompt running on the target
root:/sys/devices/platform/bfin-spi.0/spi0.18/device0> cat in-in_scale 0.976000
Description:
Raw unscaled voltage measurement on cell channel in0-in1_raw
This specifies any shell prompt running on the target
root:/sys/devices/platform/bfin-spi.0/spi0.18/device0> cat in0-in1_raw 2254
U = in0-in1_raw * in-in_scale + offset = 2254 * 0.976000 + 1000 = 3199.904 mV
Description:
Raw unscaled voltage measurement on all cell channel in0-inX_raw
This specifies any shell prompt running on the target
root:/sys/devices/platform/bfin-spi.0/spi0.18/device0> cat in0-in12_raw 27048
U = in0-in1_raw * in-in_scale + (cell_num * offset) = 27048 * 0.976000 + (12 * 1000) = 38398.848 mV
Description:
scale to be applied to tempX_raw in order to obtain the measured voltage in millivolts.
This specifies any shell prompt running on the target
root:/sys/devices/platform/bfin-spi.0/spi0.18/device0> cat temp_scale 1.220000
Description:
Shows high accuracy band gap temperature sensor temperature in milli degrees Celsius.
This specifies any shell prompt running on the target
root:/sys/devices/platform/bfin-spi.0/spi0.18/device0> cat temp0_raw 2096
U = temp0_raw * temp_scale = 2096 * 1.220000 = 2557.12 mV
The AD7280A has cell balancing interface outputs designed to control external FET transistors to allow discharging of individual cells.
Description:
Writing 1 enables the cell balance output switch corresponding
to input Y. Writing 0 disables it. If the inY-inZ_balance_timer
is set to a none zero value, the corresponding switch will
enable for the programmed amount of time, before it
automatically disables.
This specifies any shell prompt running on the target
root:/sys/devices/platform/bfin-spi.0/spi0.18/device0> echo 1 > in4-in5_balance_switch_en root:/sys/devices/platform/bfin-spi.0/spi0.18/device0> cat in4-in5_balance_switch_en 1 root:/sys/devices/platform/bfin-spi.0/spi0.18/device0> echo 0 > in4-in5_balance_switch_en root:/sys/devices/platform/bfin-spi.0/spi0.18/device0> cat in4-in5_balance_switch_en 0 root:/sys/devices/platform/bfin-spi.0/spi0.18/device0>
Description:
The inY-inZ_balance_timer file allows the user to program
individual times for each cell balance output. The AD7280A
allows the user to set the timer to a value from 0 minutes to
36.9 minutes. The resolution of the timer is 71.5 sec.
The value written is the on-time in milliseconds. When the
timer value is set 0, the timer is disabled. The cell balance
outputs are controlled only by inY-inZ_balance_switch_en.
This specifies any shell prompt running on the target
root:/sys/devices/platform/bfin-spi.0/spi0.18/device0> echo 150000 > in4-in5_balance_timer root:/sys/devices/platform/bfin-spi.0/spi0.18/device0> cat in4-in5_balance_timer 143000 root:/sys/devices/platform/bfin-spi.0/spi0.18/device0>
This specifies any shell prompt running on the target
root:/> cd /sys/bus/iio/devices/ root:/sys/bus/iio/devices> ls device0 device0:event0 root:/sys/bus/iio/devices> cd device0:event0 root:/sys/devices/platform/bfin-spi.0/spi0.18/device0/device0:event0> ls -l -r--r--r-- 1 root root 4096 Mar 14 13:37 dev -rw-r--r-- 1 root root 4096 Mar 14 13:37 in-in_thresh_high_value -rw-r--r-- 1 root root 4096 Mar 14 13:37 in-in_thresh_low_value drwxr-xr-x 2 root root 0 Mar 14 13:37 power lrwxrwxrwx 1 root root 0 Mar 14 13:37 subsystem -> ../../../../../../bus/iio -rw-r--r-- 1 root root 4096 Mar 14 13:37 temp_thresh_high_value -rw-r--r-- 1 root root 4096 Mar 14 13:37 temp_thresh_low_value -rw-r--r-- 1 root root 4096 Mar 14 13:37 uevent root:/sys/devices/platform/bfin-spi.0/spi0.18/device0/device0:event0>
The AD7280A includes a dynamic alert function that can detect whether the cell voltages or auxiliary ADC inputs exceed an upper or lower limit defined by the user.
Description:
Specifies the value of threshold (_high|_low) that the device is comparing against.
This specifies any shell prompt running on the target
root:/sys/devices/platform/bfin-spi.0/spi0.18/device0/device0:event0> echo 2300 > in-in_thresh_low_value root:/sys/devices/platform/bfin-spi.0/spi0.18/device0/device0:event0> cat in-in_thresh_low_value 2285 root:/sys/devices/platform/bfin-spi.0/spi0.18/device0/device0:event0> echo 4000 > in-in_thresh_high_value root:/sys/devices/platform/bfin-spi.0/spi0.18/device0/device0:event0> cat in-in_thresh_high_value 3994