This is a Linux industrial I/O (IIO) subsystem driver, targeting multi channel serial interface ADCs. The industrial I/O subsystem provides a unified framework for drivers for many different types of converters and sensors using a number of different physical interfaces (i2c, spi, etc). See IIO for more information.
| Function | File |
|---|---|
| driver | drivers/iio/adc/ad7266.c |
| include | include/linux/platform_data/ad7266.h |
For compile time configuration, it’s common Linux practice to keep board- and application-specific configuration out of the main driver file, instead putting it into the board support file.
For devices on custom boards, as typical of embedded and SoC-(system-on-chip) based hardware, Linux uses platform_data to point to board-specific structures describing devices and how they are connected to the SoC. This can include available ports, chip variants, preferred modes, default initialization, additional pin roles, and so on. This shrinks the board-support packages (BSPs) and minimizes board and application specific #ifdefs in drivers.
The AD7265/AD7266 supports different operating modes, which can be configured via external pins. To properly interpret the data from the chip the driver has to know which mode it is configured for. This is done using platform data. If the AD (address) pins of the chip are hook up to GPIOs to be able to change the sampled inputs at runtime the GPIOs can be specified via the platform data as well. If GPIOs are used the `fixed_addr` field must be set to false.
/* * ad7266_range - AD7266 reference voltage range * @AD7266_RANGE_VREF: Device is configured for input range 0V - VREF * (RANGE pin set to low) * @AD7266_RANGE_2VREF: Device is configured for input range 0V - 2VREF * (RANGE pin set to high) */ enum ad7266_range { AD7266_RANGE_VREF, AD7266_RANGE_2VREF, }; /* * ad7266_mode - AD7266 sample mode * @AD7266_MODE_SINGLE_ENDED: Device is configured for single-ended mode * (SGL/DIFF pin set to high) * @AD7266_MODE_PSEUDO_DIFF: Device is configured for pseudo differential mode * (SGL/DIFF pin set to low, AD0 pin set to high) * @AD7266_MODE_PSEUDO_DIFF: Device is configured for full differential mode * (SGL/DIFF pin set to low, AD0 pin set to low) */ enum ad7266_mode { AD7266_MODE_SINGLE_ENDED, AD7266_MODE_PSEUDO_DIFF, AD7266_MODE_DIFF, }; /* * ad7266_platform_data - Platform data for the AD7266 driver * @range: Reference voltage range the device is configured for * @mode: Sample mode the device is configured for * @fixed_addr: Whether the AD pins are hard-wired * @addr_gpios: GPIOs used for controlling the AD pins, only valid if fixed_addr * is set to false. */ struct ad7266_platform_data { enum ad7266_range range; enum ad7266_mode mode; bool fixed_addr; unsigned int addr_gpios[3]; };
static struct ad7266_platform_data pdata = { .range = AD7266_RANGE_2VREF, .mode = AD7266_MODE_SINGLE_ENDED, .fixed_addr = false, .addr_gpios = { GPIO_PF6, GPIO_PF7, GPIO_PF8 }, };
If no platform data is provided the driver assumes differential 0V-VREF operation with a fixed address. This corresponds to the following platform data.
static struct ad7266_platform_data ad7266_pdata_default = { .range = AD7266_RANGE_VREF, .mode = AD7266_MODE_DIFF, .fixed_addr = true, };
Unlike PCI or USB devices, SPI devices are not enumerated at the hardware level. Instead, the software must know which devices are connected on each SPI bus segment, and what slave selects these devices are using. For this reason, the kernel code must instantiate SPI devices explicitly. The most common method is to declare the SPI devices by bus number.
This method is appropriate when the SPI bus is a system bus, as in many embedded systems, wherein each SPI bus has a number which is known in advance. It is thus possible to pre-declare the SPI devices that inhabit this bus. This is done with an array of struct spi_board_info, which is registered by calling spi_register_board_info().
For more information see: Documentation/spi/spi-summary
Depending on the converter IC used, you may need to set the modalias accordingly, matching your part name. It may also required to adjust max_speed_hz. Please consult the datasheet, for maximum spi clock supported by the device in question.
static struct spi_board_info board_spi_board_info[] __initdata = { { .modalias = "ad7266", .max_speed_hz = 1000000, /* max spi clock (SCK) speed in HZ */ .bus_num = 0, .chip_select = GPIO_PF10 + MAX_CTRL_CS, /* CS, change it for your board */ .platform_data = &ad7266_pdata, /* No spi_driver specific config */ .mode = SPI_MODE_2, }, };
static int __init board_init(void) { [--snip--] spi_register_board_info(board_spi_board_info, ARRAY_SIZE(board_spi_board_info)); [--snip--] return 0; } arch_initcall(board_init);
Configure kernel with “make menuconfig” (alternatively use “make xconfig” or “make qconfig”)
The AD7266 Driver depends on CONFIG_SPI
Linux Kernel Configuration
Device Drivers --->
...
<*> Industrial I/O support --->
--- Industrial I/O support
...
Analog to digital converters --->
...
<*> Analog Devices AD7265/AD7266 ADC driver
...
...
...
Each and every IIO device, typically a hardware chip, has a device folder under /sys/bus/iio/devices/iio:deviceX. Where X is the IIO index of the device. Under every of these directory folders reside a set of files, depending on the characteristics and features of the hardware device in question. These files are consistently generalized and documented in the IIO ABI documentation. In order to determine which IIO deviceX corresponds to which hardware device, the user can read the name file /sys/bus/iio/devices/iio:deviceX/name. In case the sequence in which the iio device drivers are loaded/registered is constant, the numbering is constant and may be known in advance.
This specifies any shell prompt running on the target
root:/> cd /sys/bus/iio/devices/ root:/sys/bus/iio/devices> ls iio:device0 trigger0 root:/sys/bus/iio/devices> cd iio:device0 root:/sys/devices/platform/bfin-spi.0/spi0.12/iio:device0> ls -l drwxr-xr-x 2 root root 0 Jan 1 04:03 buffer -r--r--r-- 1 root root 4096 Jan 1 04:03 dev -rw-r--r-- 1 root root 4096 Jan 1 04:03 in_voltage-voltage_scale -r--r--r-- 1 root root 4096 Jan 1 04:03 in_voltage0-voltage1_raw -r--r--r-- 1 root root 4096 Jan 1 04:03 in_voltage2-voltage3_raw -r--r--r-- 1 root root 4096 Jan 1 04:03 in_voltage4-voltage5_raw -r--r--r-- 1 root root 4096 Jan 1 04:03 in_voltage6-voltage7_raw -r--r--r-- 1 root root 4096 Jan 1 04:03 in_voltage8-voltage9_raw -r--r--r-- 1 root root 4096 Jan 1 04:03 in_voltage10-voltage11_raw -r--r--r-- 1 root root 4096 Jan 1 04:03 name drwxr-xr-x 2 root root 0 Jan 1 04:03 power drwxr-xr-x 2 root root 0 Jan 1 04:03 scan_elements lrwxrwxrwx 1 root root 0 Jan 1 04:03 subsystem -> ../../../../../bus/iio drwxr-xr-x 2 root root 0 Jan 1 04:03 trigger -rw-r--r-- 1 root root 4096 Jan 1 04:03 uevent root:/sys/devices/platform/bfin-spi.0/spi0.12/iio:device0>
This specifies any shell prompt running on the target
root:/sys/devices/platform/bfin-spi.0/spi0.12/iio:device0> cat name ad7266
Description:
in_voltage-voltage_scale
Scale to be applied to in_voltageY-voltageZ_raw in order to obtain the measured voltage in millivolts.
This specifies any shell prompt running on the target
root:/sys/devices/platform/bfin-spi.0/spi0.3/device0> cat in_voltage-voltage_scale 0.610350 root:/sys/devices/platform/bfin-spi.0/spi0.3/device0>
Description:
in_voltageY-voltageZ_raw
Raw unscaled voltage measurement on channel pair X-Z in differential mode
| ADC Input Pair | Channel name |
|---|---|
| VA1 - VA2 | in_voltage0-voltage1_raw |
| VB1 - VB2 | in_voltage2-voltage3_raw |
| VA2 - VA3 | in_voltage4-voltage5_raw |
| VB2 - VB3 | in_voltage7-voltage7_raw |
| VA4 - VA5 | in_voltage8-voltage9_raw |
| VB4 - VB5 | in_voltage10-voltage11_raw |
This specifies any shell prompt running on the target
root:/sys/devices/platform/bfin-spi.0/spi0.12/iio:device0> cat in_voltage0-voltage1_raw 100
U = in_voltage0-voltage1_raw * in_voltage-voltage_scale = 100 * 0.610350 = 61.035 mV
Description:
in_voltage_scale
Scale to be applied to in_voltageY in order to obtain the measured voltage in millivolts.
This specifies any shell prompt running on the target
root:/sys/devices/platform/bfin-spi.0/spi0.3/iio:device0> cat in_voltage_scale 0.610350 root:/sys/devices/platform/bfin-spi.0/spi0.3/iio:device0>
Description:
in_voltageY_raw
Raw unscaled voltage measurement on channel in single ended mode
This specifies any shell prompt running on the target
root:/sys/devices/platform/bfin-spi.0/spi0.12/iio:device0> cat in_voltage0_raw 100
U = in_voltage0 * in_voltage_scale = 100 * 0.610350 = 61.035 mV
This specifies any shell prompt running on the target
root:/sys/devices/platform/bfin-spi.0/spi0.3/iio:device0> cat trigger/current_trigger bfintmr3
The Industrial I/O subsystem provides support for various ring buffer based data acquisition methods. Apart from device specific hardware buffer support, the user can chose between two different software ring buffer implementations. One is the IIO lock free software ring, and the other is based on Linux kfifo. Devices with buffer support feature an additional sub-folder in the /sys/bus/iio/devices/deviceX/ folder hierarchy. Called deviceX:bufferY, where Y defaults to 0, for devices with a single buffer.
Every buffer implementation features a set of files:
length
Get/set the number of sample sets that may be held by the buffer.
enable
Enables/disables the buffer. This file should be written last, after length and selection of scan elements.
scan_elements
The scan_elements directory contains interfaces for elements that will be captured for a single triggered sample set in the buffer.
This specifies any shell prompt running on the target
root:/sys/devices/platform/bfin-spi.0/spi0.3/iio:device0/scan_elements> ls in_voltage0-voltage1_en in_voltage2-voltage3_en in_voltage0-voltage1_index in_voltage2-voltage3_index in_voltage0-voltage1_type in_voltage2-voltage3_type root:/sys/devices/platform/bfin-spi.0/spi0.3/iio:device0/scan_elements>
in_voltageX_en / in_voltageX-voltageY_en / timestamp_en:
Scan element control for triggered data capture.
Writing 1 will enable the scan element, writing 0 will disable it
in_voltageX_type / in_voltageX-voltageY_type / timestamp_type:
Description of the scan element data storage within the buffer
and therefore in the form in which it is read from user-space.
Form is [s|u]bits/storage-bits. s or u specifies if signed
(2's complement) or unsigned. bits is the number of bits of
data and storage-bits is the space (after padding) that it
occupies in the buffer. Note that some devices will have
additional information in the unused bits so to get a clean
value, the bits value must be used to mask the buffer output
value appropriately. The storage-bits value also specifies the
data alignment. So u12/16 will be a unsigned 12 bit integer
stored in a 16 bit location aligned to a 16 bit boundary.
For other storage combinations this attribute will be extended
appropriately.
in_voltageX_index / in_voltageX-voltageY_index / timestamp_index:
A single positive integer specifying the position of this
scan element in the buffer. Note these are not dependent on
what is enabled and may not be contiguous. Thus for user-space
to establish the full layout these must be used in conjunction
with all _en attributes to establish which channels are present,
and the relevant _type attributes to establish the data storage
format.