This is a Linux industrial I/O (IIO) subsystem driver, targeting multi channel serial interface ADCs. The industrial I/O subsystem provides a unified framework for drivers for many different types of converters and sensors using a number of different physical interfaces (i2c, spi, etc). See IIO for more information.
| Function | File |
|---|---|
| driver | drivers/staging/iio/adc/ad7192.c |
| include | drivers/staging/iio/adc/ad7192.h |
For compile time configuration, it’s common Linux practice to keep board- and application-specific configuration out of the main driver file, instead putting it into the board support file.
For devices on custom boards, as typical of embedded and SoC-(system-on-chip) based hardware, Linux uses platform_data to point to board-specific structures describing devices and how they are connected to the SoC. This can include available ports, chip variants, preferred modes, default initialization, additional pin roles, and so on. This shrinks the board-support packages (BSPs) and minimizes board and application specific #ifdefs in drivers.
The reference voltage may vary between boards and models. The platform_data for the device's “struct device” holds this information.
/** * struct ad7192_platform_data - platform/board specific information * @vref_mv: the external reference voltage in millivolt * @ext_clk_Hz: the external clock frequency in Hz, if not set * the driver uses the internal clock (16.776 MHz) * @clock_source_sel: [0..3] * 0 External 4.92 MHz clock connected from MCLK1 to MCLK2 * 1 External Clock applied to MCLK2 * 2 Internal 4.92 MHz Clock not available at the MCLK2 pin * 3 Internal 4.92 MHz Clock available at the MCLK2 pin * @refin2_en: REFIN1/REFIN2 Reference Select (AD7190/2 only) * @rej60_en: 50/60Hz notch filter enable * @sinc3_en: SINC3 filter enable (default SINC4) * @chop_en: CHOP mode enable * @buf_en: buffered input mode enable * @unipolar_en: unipolar mode enable * @burnout_curr_en: constant current generators on AIN(+|-) enable */ struct ad7192_platform_data { u16 vref_mv; u32 ext_clk_Hz; u8 clock_source_sel; bool refin2_en; bool rej60_en; bool sinc3_en; bool chop_en; bool buf_en; bool unipolar_en; bool burnout_curr_en; };
static struct ad7192_platform_data ad7192_pdata = { .vref_mv = 3300, .clock_source_sel = 2, .refin2_en = true, .rej60_en = false, .sinc3_en = false, .chop_en = false, .buf_en = false, .unipolar_en = true, .burnout_curr_en = false, };
Unlike PCI or USB devices, SPI devices are not enumerated at the hardware level. Instead, the software must know which devices are connected on each SPI bus segment, and what slave selects these devices are using. For this reason, the kernel code must instantiate SPI devices explicitly. The most common method is to declare the SPI devices by bus number.
This method is appropriate when the SPI bus is a system bus, as in many embedded systems, wherein each SPI bus has a number which is known in advance. It is thus possible to pre-declare the SPI devices that inhabit this bus. This is done with an array of struct spi_board_info, which is registered by calling spi_register_board_info().
For more information see: Documentation/spi/spi-summary
Depending on the converter IC used, you may need to set the modalias accordingly, matching your part name. It may also required to adjust max_speed_hz. Please consult the datasheet, for maximum spi clock supported by the device in question.
static struct spi_board_info board_spi_board_info[] __initdata = { #if defined(CONFIG_AD7192) \ || defined(CONFIG_AD7192_MODULE) { .modalias = "ad7192", .max_speed_hz = 1000000, /* max spi clock (SCK) speed in HZ */ .bus_num = 0, .chip_select = GPIO_PF10 + MAX_CTRL_CS, /* CS, change it for your board */ .platform_data = &ad7192_pdata, .mode = SPI_MODE_3, .irq = IRQ_PF6, }, #endif };
static int __init board_init(void) { [--snip--] spi_register_board_info(board_spi_board_info, ARRAY_SIZE(board_spi_board_info)); [--snip--] return 0; } arch_initcall(board_init);
Configure kernel with “make menuconfig” (alternatively use “make xconfig” or “make qconfig”)
The AD7192 Driver depends on CONFIG_SPI
Linux Kernel Configuration Device Drivers ---> [*] Staging drivers ---> <*> Industrial I/O support ---> --- Industrial I/O support -*- Enable ring buffer support within IIO -*- Industrial I/O lock free software ring -*- Enable triggered sampling support *** Analog to digital converters *** [--snip--] <*> Analog Devices AD7190 AD7192 AD7195 ADC driver [--snip--]
Each and every IIO device, typically a hardware chip, has a device folder under /sys/bus/iio/devices/iio:deviceX. Where X is the IIO index of the device. Under every of these directory folders reside a set of files, depending on the characteristics and features of the hardware device in question. These files are consistently generalized and documented in the IIO ABI documentation. In order to determine which IIO deviceX corresponds to which hardware device, the user can read the name file /sys/bus/iio/devices/iio:deviceX/name. In case the sequence in which the iio device drivers are loaded/registered is constant, the numbering is constant and may be known in advance.
This specifies any shell prompt running on the target
root:/> cd /sys/bus/iio/devices/ root:/sys/bus/iio/devices> ls iio:device0 trigger0 root:/sys/bus/iio/devices> cd iio:device0 root:/sys/devices/platform/bfin-spi.0/spi0.18/iio:device0> ls -l -rw-r--r-- 1 root root 4096 Jan 4 16:59 bridge_switch_en drwxr-xr-x 4 root root 0 Jan 4 16:59 buffer -rw-r--r-- 1 root root 4096 Jan 4 16:59 in_voltage-in_voltage_scale -r--r--r-- 1 root root 4096 Jan 4 16:59 in_voltage-in_voltage_scale_available -r--r--r-- 1 root root 4096 Jan 4 16:59 in_voltage1-in_voltage2_raw -r--r--r-- 1 root root 4096 Jan 4 16:59 in_voltage1_raw -r--r--r-- 1 root root 4096 Jan 4 16:59 in_voltage2-in_voltage2_shorted_raw -r--r--r-- 1 root root 4096 Jan 4 16:59 in_voltage2_raw -r--r--r-- 1 root root 4096 Jan 4 16:59 in_voltage3-in_voltage4_raw -r--r--r-- 1 root root 4096 Jan 4 16:59 in_voltage3_raw -r--r--r-- 1 root root 4096 Jan 4 16:59 in_voltage4_raw -rw-r--r-- 1 root root 4096 Jan 4 16:59 in_voltage_scale -r--r--r-- 1 root root 4096 Jan 4 16:59 in_voltage_scale_available -r--r--r-- 1 root root 4096 Jan 4 16:59 name drwxr-xr-x 2 root root 0 Jan 4 16:59 power -rw-r--r-- 1 root root 4096 Jan 5 11:38 sampling_frequency lrwxrwxrwx 1 root root 0 Jan 4 16:59 subsystem -> ../../../../../bus/iio -r--r--r-- 1 root root 4096 Jan 4 16:59 in_temp0_raw -rw-r--r-- 1 root root 4096 Jan 4 16:59 in_temp0_scale drwxr-xr-x 2 root root 0 Jan 4 16:59 trigger -rw-r--r-- 1 root root 4096 Jan 4 16:59 uevent root:/sys/devices/platform/bfin-spi.0/spi0.18/iio:device0>
This specifies any shell prompt running on the target
root:/sys/devices/platform/bfin-spi.0/spi0.18/iio:device0> cat name ad7192
This specifies any shell prompt running on the target
root:/sys/devices/platform/bfin-spi.0/spi0.18/iio:device0> cat sampling_frequency 10 root:/sys/devices/platform/bfin-spi.0/spi0.18/iio:device0> echo 50 > sampling_frequency root:/sys/devices/platform/bfin-spi.0/spi0.18/iio:device0> cat sampling_frequency 50 root:/sys/devices/platform/bfin-spi.0/spi0.18/iio:device0>
Lists all available scales for the differential input pairs:
| ADC Input Pair | Channel name |
|---|---|
| AIN1(+) - AIN2(-) | in_voltage1-in_voltage2_raw |
| AIN3(+) - AIN4(-) | in_voltage3-in_voltage4_raw |
| AIN2(-) - AIN2(-) | in_voltage2-in_voltage2_shorted_raw |
Setting these directly influences the ADC input range, by altering the GAIN amplifier.
This specifies any shell prompt running on the target
root:/sys/devices/platform/bfin-spi.0/spi0.18/iio:device0> cat in_voltage-in_voltage_scale_available 0.000393390 0.000196690 0.000098340 0.000049170 0.000024580 0.000012290 0.000006140 0.000003070
Lists all available scales for the differential input pairs:
| ADC Input Pair | Channel name |
|---|---|
| AIN1 - AINCOM | in_voltage1_raw |
| AIN2 - AINCOM | in_voltage2_raw |
| AIN3 - AINCOM | in_voltage3_raw |
| AIN4 - AINCOM | in_voltage4_raw |
Setting these directly influences the ADC input range, by altering the GAIN amplifier.
This specifies any shell prompt running on the target
root:/sys/devices/platform/bfin-spi.0/spi0.18/iio:device0> cat in_voltage_scale_available 0.000393390 0.000196690 0.000098340 0.000049170 0.000024580 0.000012290 0.000006140 0.000003070
Scale to be applied to in1-in2_raw, in2-in3_raw in order to obtain the measured voltage in millivolts. Allows the user to select one scale out of the available scales. If the written scale differs from the current scale. The driver performs full and zero offset calibration on all differential input channels.
This specifies any shell prompt running on the target
root:/sys/devices/platform/bfin-spi.0/spi0.18/iio:device0> cat in_voltage-in_voltage_scale 0.000393390 root:/sys/devices/platform/bfin-spi.0/spi0.18/iio:device0> echo 0.000196690 > in_voltage-in_voltage_scale root:/sys/devices/platform/bfin-spi.0/spi0.18/iio:device0> cat in_voltage-in_voltage_scale 0.000196690
Description:
Raw unscaled voltage measurement on channel in_voltage1
| ADC Input Pair | Channel name |
|---|---|
| AIN1(+) - AIN2(-) | in_voltage1-in_voltage2_raw |
| AIN3(+) - AIN4(-) | in_voltage3-in_voltage4_raw |
| AIN2(-) - AIN2(-) | in_voltage2-in_voltage2_shorted_raw |
| AIN1 - AINCOM | in_voltage1_raw |
| AIN2 - AINCOM | in_voltage2_raw |
| AIN3 - AINCOM | in_voltage3_raw |
| AIN4 - AINCOM | in_voltage4_raw |
This specifies any shell prompt running on the target
root:/sys/devices/platform/bfin-spi.0/spi0.18/iio:device0> cat in1_raw -1
U = in_voltage1_raw * in_voltage_scale = 3983772* 0.000393390 = 1567.17606708 mV
Description:
Raw unscaled voltage measurement on channel in_voltage1-in_voltage2
This specifies any shell prompt running on the target
root:/sys/devices/platform/bfin-spi.0/spi0.18/iio:device0> cat in_voltage1-in_voltage2_raw -1
U = in_voltage1-in_voltage3_raw * in_voltage-in_voltage_scale = -1 * 0.000393390 = -0.000393390 mV
Description: /sys/bus/iio/devices/iio:deviceX/in_temp0_raw
Shows raw unscaled temperature.
This specifies any shell prompt running on the target
root:/sys/devices/platform/bfin-spi.0/spi0.18/iio:device0> cat in_temp0_raw -175
Description: /sys/bus/iio/devices/iio:deviceX/bridge_switch_en
Writing 1 closes the bridge switch.
This specifies any shell prompt running on the target
root:/sys/devices/platform/bfin-spi.0/spi0.18/iio:device0> echo 1 > bridge_switch_en root:/sys/devices/platform/bfin-spi.0/spi0.18/iio:device0> cat bridge_switch_en 1 root:/sys/devices/platform/bfin-spi.0/spi0.18/iio:device0> echo 0 > bridge_switch_en
Description: /sys/bus/iio/devices/iio:deviceX/ac_excitation_en
Writing 1 enables AC excitation on the AD7195 ACX strobes.
This specifies any shell prompt running on the target
root:/sys/devices/platform/bfin-spi.0/spi0.18/iio:device0> echo 1 > ac_excitation_en root:/sys/devices/platform/bfin-spi.0/spi0.18/iio:device0> cat ac_excitation_en 1 root:/sys/devices/platform/bfin-spi.0/spi0.18/iio:device0> echo 0 > ac_excitation_en
This driver only supports it's own default trigger source ad7192-dev0
This specifies any shell prompt running on the target
root:/sys/devices/platform/bfin-spi.0/spi0.18/iio:device0> cat trigger/current_trigger ad7192-dev0
This specifies any shell prompt running on the target
root:/sys/devices/platform/bfin-spi.0/spi0.18/device0/iio:buffer> ls enable length
The Industrial I/O subsystem provides support for various ring buffer based data acquisition methods. Apart from device specific hardware buffer support, the user can chose between two different software ring buffer implementations. One is the IIO lock free software ring, and the other is based on Linux kfifo. Devices with buffer support feature an additional sub-folder in the /sys/bus/iio/devices/deviceX/ folder hierarchy. Called deviceX:bufferY, where Y defaults to 0, for devices with a single buffer.
Every buffer implementation features a set of files:
length
Get/set the number of sample sets that may be held by the buffer.
enable
Enables/disables the buffer. This file should be written last, after length and selection of scan elements.
scan_elements
The scan_elements directory contains interfaces for elements that will be captured for a single triggered sample set in the buffer.
This specifies any shell prompt running on the target
root:/sys/devices/platform/bfin-spi.0/spi0.18/iio:device0/scan_elements> ls in_voltage1-in_voltage2_en in_voltage2_en in_voltage4_en in_voltage1-in_voltage2_index in_voltage2_index in_voltage4_index in_voltage1-in_voltage2_type in_voltage2_type in_voltage4_type in_voltage1_en in_voltage3-in_voltage4_en in_temp0_en in_voltage1_index in_voltage3-in_voltage4_index in_temp0_index in_voltage1_type in_voltage3-in_voltage4_type in_temp0_type in_voltage2-in_voltage2_shorted_en in_voltage3_en timestamp_en in_voltage2-in_voltage2_shorted_index in_voltage3_index timestamp_index in_voltage2-in_voltage2_shorted_type in_voltage3_type timestamp_type root:/sys/devices/platform/bfin-spi.0/spi0.18/iio:device0/scan_elements>
in_voltageX_en / in_voltageX-voltageY_en / timestamp_en:
Scan element control for triggered data capture.
Writing 1 will enable the scan element, writing 0 will disable it
in_voltageX_type / in_voltageX-voltageY_type / timestamp_type:
Description of the scan element data storage within the buffer
and therefore in the form in which it is read from user-space.
Form is [s|u]bits/storage-bits. s or u specifies if signed
(2's complement) or unsigned. bits is the number of bits of
data and storage-bits is the space (after padding) that it
occupies in the buffer. Note that some devices will have
additional information in the unused bits so to get a clean
value, the bits value must be used to mask the buffer output
value appropriately. The storage-bits value also specifies the
data alignment. So u12/16 will be a unsigned 12 bit integer
stored in a 16 bit location aligned to a 16 bit boundary.
For other storage combinations this attribute will be extended
appropriately.
in_voltageX_index / in_voltageX-voltageY_index / timestamp_index:
A single positive integer specifying the position of this
scan element in the buffer. Note these are not dependent on
what is enabled and may not be contiguous. Thus for user-space
to establish the full layout these must be used in conjunction
with all _en attributes to establish which channels are present,
and the relevant _type attributes to establish the data storage
format.