This version (09 Nov 2011 11:25) was approved by mhennerich.The Previously approved version (09 Nov 2011 11:25) is available.
This is a Linux industrial I/O (IIO) subsystem driver, targeting serial interface Accelerometer. The industrial I/O subsystem provides a unified framework for drivers for many different types of converters and sensors using a number of different physical interfaces (i2c, spi, etc). See IIO for more information.
| Function | File |
|---|---|
| driver | drivers/staging/iio/accel/adis16240_core.c |
| driver | drivers/staging/iio/accel/adis16240_ring.c |
| driver | drivers/staging/iio/accel/adis16240_trigger.c |
| include | drivers/staging/iio/accel/adis16240.h |
Unlike PCI or USB devices, SPI devices are not enumerated at the hardware level. Instead, the software must know which devices are connected on each SPI bus segment, and what slave selects these devices are using. For this reason, the kernel code must instantiate SPI devices explicitly. The most common method is to declare the SPI devices by bus number.
This method is appropriate when the SPI bus is a system bus, as in many embedded systems, wherein each SPI bus has a number which is known in advance. It is thus possible to pre-declare the SPI devices that inhabit this bus. This is done with an array of struct spi_board_info, which is registered by calling spi_register_board_info().
For more information see: Documentation/spi/spi-summary
Depending on the converter IC used, you may need to set the modalias accordingly, matching your part name. It may also required to adjust max_speed_hz. Please consult the datasheet, for maximum spi clock supported by the device in question.
static struct spi_board_info board_spi_board_info[] __initdata = { #if defined(CONFIG_ADIS16240) \ || defined(CONFIG_ADIS16240_MODULE) { .modalias = "adis16240", .max_speed_hz = 1500000, /* max spi clock (SCK) speed in HZ */ .bus_num = 0, .chip_select = 5, /* CS, change it for your board */ .platform_data = NULL, /* No spi_driver specific config */ .mode = SPI_MODE_3, .irq = IRQ_PF4, }, #endif };
static int __init board_init(void) { [--snip--] spi_register_board_info(board_spi_board_info, ARRAY_SIZE(board_spi_board_info)); [--snip--] return 0; } arch_initcall(board_init);
Configure kernel with “make menuconfig” (alternatively use “make xconfig” or “make qconfig”)
The ADIS16240 Driver depends on CONFIG_SPI
Linux Kernel Configuration Device Drivers ---> [*] Staging drivers ---> <*> Industrial I/O support ---> --- Industrial I/O support -*- Enable ring buffer support within IIO -*- Industrial I/O lock free software ring -*- Enable triggered sampling support *** Accelerometers *** [--snip--] <*> Analog Devices ADIS16240 Programmable Impact Sensor and Recorder [--snip--]
Each and every IIO device, typically a hardware chip, has a device folder under /sys/bus/iio/devices/iio:deviceX. Where X is the IIO index of the device. Under every of these directory folders reside a set of files, depending on the characteristics and features of the hardware device in question. These files are consistently generalized and documented in the IIO ABI documentation. In order to determine which IIO deviceX corresponds to which hardware device, the user can read the name file /sys/bus/iio/devices/iio:deviceX/name. In case the sequence in which the iio device drivers are loaded/registered is constant, the numbering is constant and may be known in advance.
This specifies any shell prompt running on the target
root:/> cd /sys/bus/iio/devices/ root:/sys/bus/iio/devices> ls iio:device0 trigger0 root:/sys/bus/iio/devices> cd iio:device0 root:/sys/devices/platform/bfin-spi.0/spi0.5/iio:device0> ls -l -r--r--r-- 1 root root 4096 Jan 4 04:15 accel_xyz_squared_peak_raw drwxr-xr-x 2 root root 0 Jan 4 04:15 buffer -r--r--r-- 1 root root 4096 Jan 4 04:15 dev -rw-r--r-- 1 root root 4096 Jan 4 04:15 in_accel_x_calibbias -r--r--r-- 1 root root 4096 Jan 4 04:15 in_accel_x_raw -rw-r--r-- 1 root root 4096 Jan 4 04:15 in_accel_x_scale -rw-r--r-- 1 root root 4096 Jan 4 04:15 in_accel_y_calibbias -r--r--r-- 1 root root 4096 Jan 4 04:15 in_accel_y_raw -rw-r--r-- 1 root root 4096 Jan 4 04:15 in_accel_y_scale -rw-r--r-- 1 root root 4096 Jan 4 04:15 in_accel_z_calibbias -r--r--r-- 1 root root 4096 Jan 4 04:15 in_accel_z_raw -rw-r--r-- 1 root root 4096 Jan 4 04:15 in_accel_z_scale -r--r--r-- 1 root root 4096 Jan 4 04:15 in_temp0_raw -rw-r--r-- 1 root root 4096 Jan 4 04:15 in_temp0_scale -r--r--r-- 1 root root 4096 Jan 4 04:15 in_voltage0_supply_raw -rw-r--r-- 1 root root 4096 Jan 4 04:15 in_voltage0_supply_scale -r--r--r-- 1 root root 4096 Jan 4 04:15 in_voltage1_raw -r--r--r-- 1 root root 4096 Jan 4 04:15 name drwxr-xr-x 2 root root 0 Jan 4 04:15 power --w------- 1 root root 4096 Jan 4 04:15 reset -r--r--r-- 1 root root 4096 Jan 4 04:15 sampling_frequency_available drwxr-xr-x 2 root root 0 Jan 4 04:15 scan_elements lrwxrwxrwx 1 root root 0 Jan 4 04:15 subsystem -> ../../../../../bus/iio drwxr-xr-x 2 root root 0 Jan 4 04:15 trigger -rw-r--r-- 1 root root 4096 Jan 4 04:15 uevent
This specifies any shell prompt running on the target
root:/sys/devices/platform/bfin-spi.0/spi0.5/iio:device0> cat name adis16240
For a detailed description please see: drivers/staging/iio/Documentation/sysfs-bus-iio
| Device files |
|---|
| accel_xyz_squared_peak_raw |
| in_accel_x_calibbias |
| in_accel_x_raw |
| in_accel_x_scale |
| in_accel_y_calibbias |
| in_accel_y_raw |
| in_accel_y_scale |
| in_accel_z_calibbias |
| in_accel_z_raw |
| in_accel_z_scale |
| in_temp0_raw |
| in_temp0_scale |
| in_voltage0_supply_raw |
| in_voltage0_supply_scale |
| in_voltage1_raw |
| name |
| reset |
| sampling_frequency_available |
This driver only supports it's own default trigger source adis16240-dev0
This specifies any shell prompt running on the target
root:/sys/devices/platform/bfin-spi.0/spi0.5/iio:device0> cat trigger/current_trigger adis16240-dev0
This specifies any shell prompt running on the target
root:/sys/devices/platform/bfin-spi.0/spi0.5/iio:device0/buffer> ls bytes_per_datum enable length
The Industrial I/O subsystem provides support for various ring buffer based data acquisition methods. Apart from device specific hardware buffer support, the user can chose between two different software ring buffer implementations. One is the IIO lock free software ring, and the other is based on Linux kfifo. Devices with buffer support feature an additional sub-folder in the /sys/bus/iio/devices/deviceX/ folder hierarchy. Called deviceX:bufferY, where Y defaults to 0, for devices with a single buffer.
Every buffer implementation features a set of files:
length
Get/set the number of sample sets that may be held by the buffer.
enable
Enables/disables the buffer. This file should be written last, after length and selection of scan elements.
scan_elements
The scan_elements directory contains interfaces for elements that will be captured for a single triggered sample set in the buffer.
This specifies any shell prompt running on the target
root:/sys/devices/platform/bfin-spi.0/spi0.5/iio:device0/scan_elements>ls in_accel_x_en in_accel_z_index in_timestamp_type in_accel_x_index in_accel_z_type in_voltage0_supply_en in_accel_x_type in_temp0_en in_voltage0_supply_index in_accel_y_en in_temp0_index in_voltage0_supply_type in_accel_y_index in_temp0_type in_voltage1_en in_accel_y_type in_timestamp_en in_voltage1_index in_accel_z_en in_timestamp_index in_voltage1_type
in_voltageX_en / in_voltageX-voltageY_en / timestamp_en:
Scan element control for triggered data capture.
Writing 1 will enable the scan element, writing 0 will disable it
in_voltageX_type / in_voltageX-voltageY_type / timestamp_type:
Description of the scan element data storage within the buffer
and therefore in the form in which it is read from user-space.
Form is [s|u]bits/storage-bits. s or u specifies if signed
(2's complement) or unsigned. bits is the number of bits of
data and storage-bits is the space (after padding) that it
occupies in the buffer. Note that some devices will have
additional information in the unused bits so to get a clean
value, the bits value must be used to mask the buffer output
value appropriately. The storage-bits value also specifies the
data alignment. So u12/16 will be a unsigned 12 bit integer
stored in a 16 bit location aligned to a 16 bit boundary.
For other storage combinations this attribute will be extended
appropriately.
in_voltageX_index / in_voltageX-voltageY_index / timestamp_index:
A single positive integer specifying the position of this
scan element in the buffer. Note these are not dependent on
what is enabled and may not be contiguous. Thus for user-space
to establish the full layout these must be used in conjunction
with all _en attributes to establish which channels are present,
and the relevant _type attributes to establish the data storage
format.