This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:tools-software:linux-drivers:gpio:adp5588-gpio [09 Nov 2011 11:54] – [Supported Devices] Michael Hennerich | resources:tools-software:linux-drivers:gpio:adp5588-gpio [05 Sep 2012 11:24] – ch Michael Hennerich | ||
---|---|---|---|
Line 8: | Line 8: | ||
===== Evaluation Boards ===== | ===== Evaluation Boards ===== | ||
- | * [[adi> | + | * [[adi> |
- | * [[adi> | + | * [[adi> |
- | * [[adi> | + | * [[adi> |
===== Description ===== | ===== Description ===== | ||
Line 28: | Line 28: | ||
^ Source | ^ Source | ||
- | | [[bfgit>linux-kernel?drivers/ | + | | [[git.linux.org>drivers/ |
===== Files ===== | ===== Files ===== | ||
Line 66: | Line 66: | ||
< | < | ||
The ADP5588 Driver depends on **CONFIG_I2C**\\ | The ADP5588 Driver depends on **CONFIG_I2C**\\ | ||
- | IRQ-Chip interrupt controller support is not available in case this driver is build as Module | + | IRQ-Chip interrupt controller support is not available in case this driver is build as Module |
</ | </ | ||
< | < | ||
- | Device Drivers | + | Device Drivers |
- | [*] GPIO Support | + | [*] GPIO Support |
--- GPIO Support | --- GPIO Support | ||
Line 109: | Line 109: | ||
<note tip> | <note tip> | ||
On the ADP5588 Demo Mother Board replace R30 (10kOhm PULL-UP resistor on /INTB strobe) with a 1-3kOhm resistor. | On the ADP5588 Demo Mother Board replace R30 (10kOhm PULL-UP resistor on /INTB strobe) with a 1-3kOhm resistor. | ||
- | The 10kOhm resistor is too weak - Blackfin might see an additional falling edge interrupt on the rising edge of / | + | The 10kOhm resistor is too weak - Blackfin might see an additional falling edge interrupt on the rising edge of /INTB. |
</ | </ | ||