No renderer 'pdf' found for mode 'pdf'
ADAS1000 - Blackfin Framework
Supported Devices
Evaluation Boards
Overview
The EVAL-ADAS1000SDZ is a fully featured evaluation kit for the ADAS1000. The evaluation kit consists of an evaluation board kitted with 2 ADAS1000 devices capable of demonstrating ECG capture up to 12 leads.
This evaluation board is provided for silicon evaluation purposes and is not designed to be connected directly to animal or human.
This board can be operated in conjunction with the System Development Platform (SDP) or alternatively may be interfaced to directly via a dedicated serial interface connector (J4).
The SDP controller board connects to the PC via USB 2.0. The evaluation board connects to the SDP-B controller board. The ADAS1000 evaluation board cannot be connected directly to the PC. The evaluation software running on the PC will communicate with the evaluation board through the SDP-B Controller board. The SDP Controller board is a separate list item in the ordering guide below (EVAL-SDP-CB1Z). If you have not previously purchased an SDP-B Controller board, please do so to ensure a full evaluation setup.
Framework Functional Description
This project demonstrates a framework developed for Visual DSP Visual DSP to interface the ADAS1000 to the ADSP-BF527 on the SDP-B controller board.
The software has been developed to
Requirements:
VisualDSP++ 5.0 Update 10
ADAS1000 Eval Board setup, EVAL-ADAS1000SDZ
SDP-B Rev 1.3 (with Emulator to connect to VisualDSP++),
Breakout board for SDP-B (If Hardware DRDY is used)
ECG cables and simulator (if required)
Framework Files
The attached zip file contains the relevant files for this project
Zip File Contents & description:
ADAS1000_SDP_v1.c Main function which can be used to develop the application
ADAS1K_Functions.c All the functions related to ADAS1000, which can be used by the application to read/write ADAS1000 registers,and to read data frame from ADAS1000
ADAS1K_DataProcess.c Functions to process the data read from ADAS1000
ADAS1K_DataDisplay.c Functions used to initialize the display unit and used to display/plot processed data from ADAS1000
SPORT_Functions.c
PLL configuration and all the SPORT1 functions used for Serial Interface with ADAS1000
ADAS1000_SDP_v1.ldf Linker Description file, defining all the memory sections used by the processor
ADAS1K_Functions.h Declaration of all functions related to ADAS1000, and Hardware DRDY pin definitions
ADAS1K_RegValue.h Definitions of values for ADAS1000 registers which can be directly used during ADAS1000 register configuration. The values is calculated according to definitions in User_Config.h
cdefADAS1K.h - Definitions of registers of ADAS1000, BIT Map, BIT Value and BIT Position definitions of all the fields of registers of ADAS1000 and other constant definitions and variable typdefs related to ADAS1000
cdefBF527_new.h - System
MMR register addresses for PORT registers of BF527 Blackfin on SDP)
SPORT_Functions.h - Declaration of all the SPORT1 functions used for Serial Interface with ADAS1000
User_Config.h - All the user definable parameters for various functionalities of (ADAS1000 + SDP) system
LA.vps -
VDSP++ plot for LA data
LL.vps -
VDSP++ plot for LL data
RA.vps -
VDSP++ plot for RA data
V1.vps -
VDSP++ plot for V1 data
V2.vps -
VDSP++ plot for V2 data
Implementation Description:
'Reg_Config_Table' is an array which is updated with required ADAS1000 register configuration
'ADAS1000_Open' will initialize
ADSP-BF527
Software reset of ADAS1000
Use 'Reg_Config_Table' and initialize the registers of ADAS1000
Read back the register values from ADAS1000 and confirm the values are correctly configured
Initialize the data buffers (Input and processed data)
In an infinite loop
Capture data frames from ADAS1000
Process the captured frames
Display the processed data
Procedure:
Hardware Setup
Connect J4 of SDP-B Rev 1.3 to J2 of ADAS1000 Eval board
Connect the ECG probe to J1 of ADAS1000 Eval board
Connect the Emulator to
JTAG pins (J3) of SDP-B
If Hardware DRDY is used, Connect Probing Card of SDP-B to J2 conector of SDP-B. Connect 'DRDY' pin of ADAS1000 (J4-11) to PH8 pin of
ADSP-BF527 coming on Probing Card of SDP-B (J2.85)
Open the project (ADAS1000_SDP_v1.dpj) in Visual
DSP++ 5.0 Update 10
Modify UserConfig.h file for required operation
Create and Connect to BF527 Emulator Session in Visual
DSP++
Build the project
Run the code. BF527 configures ADAS1000 and data is received continuously from it.
Plot the data
Menu > View > Debug Windows > Plot > Restore
Browse and open LA.vps and other plot files (.vps files)
Right click on the plot > Configure > Modify 'Count' for number of samples
Halt the code, to see the latest 'Count' number of samples plotted
Zip file