This is an old revision of the document!
GENERAL DESCRIPTION With the RPG2 evaluation kit, there is a need to have a host processor initialize/interact with the evaluation kit.
The ni-example-app source code does just this. It interacts with RPG2 as a sample host processor. This is literally a starting point for interacting with RPG2. The end user is by no means limited to just the PC acting as the host, or the STM32 acting as the host.
The actual app can be run on any processor once the LPL has been created for the host processor with a given link type.
What this guide is going to walk a user through is how to build and interact with the ni-example-app out of the box. Customizations are expected but those topics are covered in detail in other documents(the RPG2 Unified Interface User Guide and the RPG2 IO Configuration Tool User Guide).
Once the ni-example-app has been built either for the PC , the app can be used from the PC as the host to do the corresponding quickstart guides for RPG2.
Initial Release
Ni-example-app is distributed with both a version for a windows executable and an STM32 example. Any platform can work as the layers common to the Unified Interface are the same both for RPG2 and the host platform. Figure 1 shows the breakdown of layers in ni-example-app.
Figure 1:Network Applications IO Suite General Use Case
The ni-example-app software suite basically constructs what is known as a host processor application with the following high level tasks being done for a given platform/system.
• Calls to ui-init o This initializes the ui-stk on the host platform. • Link type initialization o This sets up the link type that shall be used.
• Set the response timeout
o This sets up the link between the host and RPG2. o This can vary from platform to platform. • Wait for the signal SDONE to go high. o This signal goes high when RPG2 is ready to receive commands. o This one may or may not be needed but it is highly recommended to install between RPG2 and the host processor. • Send out the NI-Discover message o This expects an echo of the discover almost like a ping. • Send out the NI-Init message o This tells RPG2 to initialize and be ready for further communication. o There is some warning in the ni-example-app for ui-stk compatibility. • Resets RPG2 from the Host Processor side. o This is done for the purposes of reprogramming RPG2. Finalized devices might be able to do well without this command. • Enable profile o This is usually for specific Industrial Ethernet Profile not discussed in this guide. • Enter the Event Handler o This is a while 1 loop where events are continuously processed.
Inside of the Event handler, there are several different events that need to be handled.
• UI Synch State • UI System Event • UI Config Request • UI Item out Data • UI Item in Data Latch • UI Http Tunnel Request • UI Acyclic out Data • UI IO mapping request • UI Device State Change
What all of this does is the following tasks:
• Makes use of a Host Processor to initialize RPG2 regardless of the protocol in place. o This allows for the QSG to be run. • Once it is “network initialized” it will take the output data written to it from the PLC and echo it back on the input o This is for the example application. The user’s actual application will operate differently.
Item Number | Output size | Input size |
---|---|---|
500 | 2 | 2 |
501 | 4 | 4 |
502 | 2 | 0 |
This allows for basic ladder logic construction and all of the QSGs essentially make an echo routine from host out to the network and back again.
Table 1 shows a user how to hook up miscellaneous pins to use a given link type when having the PC act as the Applications Processor.
Signal | Connector | Pin Number | Notes |
---|---|---|---|
UART - RX | 604 | 9 | Dual purpose. If UART is selected it will be UART-RX. If SPI is selected this will be the BUSY Signal. |
UART TX | 604 | 10 | - |
SPI MOSI | 604 | 1 | - |
SPI MISO | 604 | 2 | - |
SPI CLK | 604 | 3 | - |
SPI SS | 604 | 4 | - |
SPI - RREQ | 604 | 7 | - |
SPI-BUSY | 604 | 9 | - |
Ethernet | 302 | - | This is an Ethernet Cable. |
SDONE | 604 | 12 | This signal goes high the moment RPG2 is ready to receive commands over the given link type. |
Reset | 604 | 13 | This is the reset in pin for the ADIN2299. |
3.3 V | 603 | 7 | - |
5 V | 603 | 11 | - |
GND | 602 | 14 | Not all grounds are needed. |
GND | 602 | 15 | - |
GND | 602 | 16 | - |
GND | 603 | 10 | - |
GND | 604 | 11 | - |
GND | 605 | 15 | - |
GND | 605 | 16 | - |
Link Type 0 | JP600 | - | Link Types 0-2 are done to select which Link type is being used by RPG2. A user can also specify this with the Link Configuration File. The software will use the pins unless it is directed by means of an installed link configuration file. The default for the board is to use the Ethernet link type. |
Link Type 1 | JP601 | - | |
Link Type 2 | JP602 | - |
Table 1: Pins for using the PC as the Applications Processor
For the purposes of running this example on the PC, the user will either use the UART or Ethernet link type.
The pre-distributed ni-example-app runs on a PC out of the box. There are many different options that can be done as part of the ni-example-app on a command line. This can be done by navigating on a command line to the location of ni-example-app and putting in the -h in order to get the options.
Figure 2: Navigating to location for ni-example-app
Seeing the options shown by this command sends out the following configuration options.
Syntax | Command | Argument | Result |
---|---|---|---|
-l | Link Type | UART / ETH | The link type will be either Ethernet or UART. |
-c | COM Port | X where X is the com port number | The UART is used on the given USB/UART. |
-n | devString | The syntax for the Ethernet Host Interface | The Ethernet traffic goes out on the given RJ-45 connection. |
-h | Help | - | Displays the help section. |
-b | Use the example Basket for configuration | The Basket in place from the IO configuration Tool | The Host will use the “add Basket” method to configure RPG2.(Note that this basket is 1000. If another basket is in place, make sure to use that number. |
--no-reset | There is no reset sent from the Host Processor | - | The Host will not send a reset to RPG2 during initialization. |
--no-configure | Don’t Configure RPG2 | - | The Host will not do any configuration of RPG2 upon usage. |
--file-save | Update or create the file on the file system | --file-save “Module path” “Local path” | This basically allows the user to put files onto the file system from the host processor. There are many applications to this. More is discussed in the ADIN2299 User's Guide |
--file-get | Get file system content. | --file-get “Module path” “Local path” | This allows the user to get content as it exists on the file system. |
--file-delete | Remove a file from the file system | --file-delete “module path” | Deletes a file from the file system. |
--file-mark | Mark a file for an update on the file system | --file-mark “module path” | Use this as a mark to update upon reset of RPG2. |
--file-listing | Get the contents of the file system | --file-listing “” | Gets the contents of the file system as they appear. |
--tcp-server | Opens a TCP Server on the ADIN2299 | Local Port | Open's a TCP Server on the local port. |
--tcp-client | Opens a TCP Client on the ADIN2299 | Local Port | Open's a TCP Client on the local port. |
--udp-server | Opens a UDP Server on the ADIN2299 | Local Port | Open's a UDP Server on the local port. |
--udp-client | Opens a UDP Client on the ADIN2299 | Local Port | Open's a UDP Client on the local port. |
--enable-dhcp | Enables DHCP | - | Makes the device use DHCP |
--static-ip | Gives a static IP address | IP Address, Subnet, Gateway, DNS1, DNS2, Domain | The IP address is mandatory but the others are all optional. |
Table 2: Command Line Help Display
There is more information associated with how to connect this device in the following Quickstart Guides.
• RPG2 EtherCAT Quickstart Guide • RPG2 Profinet Quickstart Guide • RPG2 Ethernet/IP Quickstart Guide • RPG2 Modbus/TCP Quickstart Guide
Please refer to these documents for how to use them from the network perspective.
Shown below are two of the ways that this can be connected for evaluation.
Figure 3: Setup fora UART interface with ni-example-app.
Figure 4: Setup for an Ethernet interface with ni-example-app
The example application for Windows is called ni-example-app. This application is an application processor simulator that contains the needed API calls to interact with the Communications Controller. The ni-example-app application can be downloaded from the Analog Devices, Inc., Chronous Developer Portal. Extract the zipped file to a local directory and navigate to ..\ni-example-app\project\vs\ni-example-app. Open ni-example-app.sln with Visual Studio 2015 or later. The Solution Explorer will show the following five projects:
• ni-api-srv • ni-example-app • ni-windows-support-srv • ui-stk • ui-windows-lpl-srv
If not already selected, select ×86 as the Solution Platform. Specifying the Endianness To specify the endianness, take the following steps:
The default definition is UI_LITTLE_ENDIAN. A preprocessor definition is required either UI_LITTLE_ENDIAN or UI_BIG_ENDIAN. For a Windows platform, little endian is expected. For an embedded processor, endianness is something that varies depending on the application processor chosen.
Figure 5: Specifying the Endianness of the Applications processor
To set the Command Arguments, take the following steps:
Click the dropdown arrow and select <Edit…>.
To set the Ethernet as an application processor interface, take the following steps:
Take the following steps to set the Ethernet Command Arguments:
Figure 6: Setting arguments for the Ethernet Application processor interface.
To set the UART as an application processor interface, take the following steps:
Figure 7: UART Command Line Arguments
The item and device constructs are the default values for the predistributed sample industrial Ethernet configuration database. For more information, see the ADIN2299 User Guide for more details on this.. While not in the Console display, once the user has called the configuration complete in the application processor code, the user then must make calls specific to the inputs and outputs as shown in Table 3 (NI_SetInputData and NI_GetOutputData). The program then continuously calls the NI_ProcessEvents() function to process events. Inside of NI_ProcessEvents() there is an input data subroutine and an output data subroutine.
The ni-example-app suite can be built for any particular host processor. This set of instructions walks a user through how to do this for the STM32 CUBE.
The signals to connect when running the ni-example-app on the PC are shown in the table below.
EVAL Signal | EVAL Connector | EVAL Pin No. | STM32 Signal | STM32 Connector | STM32 Pin No. |
---|---|---|---|---|---|
UART-RX | 604 | 9 | UART-RX | C9 | 25 |
UART-TX | 604 | 10 | UART-TX | C9 | 27 |
SPI-MOSI | 604 | 1 | SPI-MOSI | CN-7 | 12 |
SPI-MISO | 604 | 2 | SPI-MISO | CN-7 | 14 |
SPI-CLK | 604 | 3 | SPI-CLK | CN-7 | 15 |
SPI-SS | 604 | 4 | SPI-SS | CN-7 | 17 |
SPI-RREQ | 604 | 7 | CN-9 | 7 | |
SPI-BUSY | 604 | 9 | CN-9 | 9 | |
Ethernet | 302 | - | Ethernet | CN-14 | - |
SDONE | 604 | 12 | SDONE | CN-8 | 14 |
RESET | 604 | 13 | RESET | CN-9 | 29 |
LINK TYPE | JP600 | 0 or 1 | CN-9 | 4 | |
LINK TYPE | JP601 | 0 or 1 | CN-9 | 6 | |
LINK TYPE | JP602 | 0 or 1 | CN-9 | 8 | |
Ground | 602 | 14 | Ground | CN-7 | 8 |
Ground | 602 | 15 | Ground | CN-8 | 11 |
Ground | 602 | 16 | Ground | CN-8 | 13 |
Ground | 603 | 10 | Ground | CN-9 | 12 |
Ground | 604 | 11 | Ground | CN-9 | 23 |
Ground | 605 | 15 | Ground | CN-10 | 5 |
Ground | 605 | 16 | Ground | CN-10 | 17 |
- | - | - | Ground | CN-10 | 22 |
- | - | - | Ground | CN-10 | 27 |
3.3V | 603 | 7 | 3.3V | CN-8 | 7 |
5V | 603 | 11 | 5V | CN-8 | 9 |
This version of ni-example-app can run for any link type between RPG2 and the STM32. Connections required for a given link type are shown (as an example) for three different types below.
EVAL Signal | EVAL Connector | EVAL Pin No. | STM32 Signal | STM32 Connector | STM32 Pin No. |
---|---|---|---|---|---|
Ethernet | 302 | - | Ethernet | CN-14 | - |
SDONE | 604 | 12 | SDONE | CN-8 | 14 |
RESET | 604 | 13 | RESET | CN-9 | 29 |
3.3V | 603 | 7 | 3.3V | CN-8 | 7 |
5V | 603 | 11 | 5V | CN-8 | 9 |
Ground | 602 | 14 | Ground | CN-7 | 8 |
Ground | 602 | 15 | Ground | CN-8 | 11 |
Ground | 602 | 16 | Ground | CN-8 | 13 |
The link type is determined by setting the pins as shown in figure 8.
Figure 8: Pin Setting for the Ethernet Interface.
Link Type | JP600 | 0 |
Link Type | JP601 | 0 |
Link Type | JP602 | 0 |
EVAL Signal | EVAL Connector | EVAL Pin No. | STM32 Signal | STM32 Connector | STM32 Pin No. |
---|---|---|---|---|---|
UART-RX | 604 | 9 | UART-RX | C9 | 25 |
UART-TX | 604 | 10 | UART-TX | C9 | 27 |
SDONE | 604 | 12 | SDONE | CN-8 | 14 |
RESET | 604 | 13 | RESET | CN-9 | 29 |
3.3V | 603 | 7 | 3.3V | CN-8 | 7 |
5V | 603 | 11 | 5V | CN-8 | 9 |
Ground | 602 | 14 | Ground | CN-7 | 8 |
Ground | 602 | 15 | Ground | CN-8 | 11 |
Ground | 602 | 16 | Ground | CN-8 | 13 |
The link type is determined by setting the pins as shown in figure 9.
Figure 9: Pin Setting for the UART Interface.
Link Type | JP600 | 1 |
Link Type | JP601 | 0 |
Link Type | JP602 | 0 |
EVAL Signal | EVAL Connector | EVAL Pin No. | STM32 Signal | STM32 Connector | STM32 Pin No. |
---|---|---|---|---|---|
SPI-MOSI | 604 | 1 | SPI-MOSI | CN-7 | 12 |
SPI-MISO | 604 | 2 | SPI-MISO | CN-7 | 14 |
SPI-CLK | 604 | 3 | SPI-CLK | CN-7 | 15 |
SPI-SS | 604 | 4 | SPI-SS | CN-7 | 17 |
SPI-RREQ | 604 | 7 | CN-9 | 7 | |
SPI-BUSY | 604 | 9 | CN-9 | 9 | |
SDONE | 604 | 12 | SDONE | CN-8 | 14 |
RESET | 604 | 13 | RESET | CN-9 | 29 |
3.3V | 603 | 7 | 3.3V | CN-8 | 7 |
5V | 603 | 11 | 5V | CN-8 | 9 |
Ground | 602 | 14 | Ground | CN-7 | 8 |
Ground | 602 | 15 | Ground | CN-8 | 11 |
Ground | 602 | 16 | Ground | CN-8 | 13 |
The link type is determined by setting the pins as shown in figure 10.
Figure 10: SPI Pin Strapping
Link Type | JP600 | 0 |
Link Type | JP601 | 1 |
Link Type | JP602 | 0 |
When you have checked out the STM32 example application, the software needs to be built to run on the STM32 on the user’s environment. The first step is to checkout the ni-example-app and set up the environment.
From the main screen as shown below, the user will click on the debug symbol.
Figure 11: Host Processor root directory
Open a Git Bash where the project is located.
Figure 12: Opening a Git Bash
Type the following into the GIT Bash to checkout project files for the STM32. git clone -b v1.16.2 https://github.com/STMicroelectronics/STM32CubeF7.git
Figure 13: Entering Commands into the Git Bash.
This particular step takes a while, but once it is done you will see the project directory as shown.
Figure 14: Directory after running the git bash.
Open the STMCUBE IDE. Navigate to “C:\Users\cstelmar\Desktop\Documentation\RapID_NI_Example_Applications_Software_Suite-Rel6.0.2\example-application\ni-example-app\project\cubeide\STM32F767ZI” Or equivalent depending on where you have decided to store the project.
Figure 15: Select Workspace Directory.
Click “Select Folder”
Figure 16: Navigating to the Project.
Click on “Launch”
Click on the “Information Center” tab at the top.
Figure 18: Selecting file import options.
From this point go to “File/Import”. Figure 19: Import Wizard.
From here click on “General\Existing Projects into Workspace” Figure 20: Import Projects Options.
From here click on the “browse” method by the select root directory option. Then navigate to where the STMCubeF7 location with ni-example-app is located.
This will then bring a large number of projects into the main screen. Figure 21: Projects to import.
Click on the “Deselect All” and then add the following pages to the project and click Finish. Figure 22: Importing of Projects.
ni-api-srv ni-example-app ni-stm32xx-support-srv ui-stk ui-stm32f7xx-lpl-srv Download them all into the project page.
Figure 23: Project view with all needed projects downloaded.
Specify the Link Type in PLAT_Platform.c. It can be either SPI, UART or ETH from a hard coding standpoint.
Figure 24: Defining link parameters.
Now save the file and the build process can begin.
Start by building in the following way:
• DBG ui-stk
Figure 25: Building the UI-stack.
• DBG ui-stm32f7xx-lpl-srv
Figure 26: Building the lpl srv.
• DBG – ni-stm32f7xx-support-srv
Figure 27: Building the STM32 support service.
• DBG – ni-api-srv
Figure 28: Building the ni-api-srv
• DBG – ni-example-app
Figure 29: Building the ni-api-srv
The example project is now built. The next step will be to build and then use the built project. To Build, first go to the debug symbol and select “Debug Configurations”. Then navigate as shown below to the ni-example-app-debug location.
Figure 30: Building the debug configuration.
The user then proceeds as shown below: Figure 31: ni-example-app STM32 debug parameters.
Then click on “Debug”. Ni-example-app is now running fully on the STM32F7 platform. It can be used to interract with networks the same way the ni-example-app on the PC does.
Following the completion of this document, there are other places a user can go to use ni-example-app in more real world PLC conditions.
• RPG2 EtherCAT Quickstart Guide – Walks through the EtherCAT protocol and how to make PDO data be reflected between the host and RPG2. • RPG2 Profinet Quickstart Guide – Walks through the EtherCAT protocol and how to make inputs and output data be reflected by the PLC. • RPG2 EtherNet/IP Quickstart Guide – Walks through the Ethernet/IP protocol and how to make class1 data be reflected between the host and RPG2. • RPG2 EtherCAT Semi Profile User Guide – Walks a user through how EtherCAT can be used for the Semi Profile with minor application changes. • RPG2 Unified Interface User Guide – This walks a user through the API in detail for the Unified Interface on RPG2.