This is an old revision of the document!
Figure 2. 24-Lead LFCSP Pin Configuration
Table 1. Function Descriptions for Quick Start
Mnemonic | Description |
---|---|
VOUT | Analog output voltage. |
VREFP | Positive reference voltage input. Connect a voltage in the range of 5 V to VDD - 2.5 V. |
VDD | Positive analog supply connection. Connect a voltage in the range of 7.5 V to 16.5 V. VDD must be decoupled to AGND. |
Active low reset. Asserting this pin returns the DAC to its power-on status. | |
Active low input. Asserting this pin sets the DAC register to a user defined value and updates the DAC output. | |
Active low load DAC logic input. This is used to update the DAC register and, consequently, the analog output. | |
VCC | Digital supply. Connect a voltage in the range of 2.7 V to 5.5 V. VCC must be decoupled to DGND. |
IOVCC | Digital interface supply. Voltage range is from 1.71 V to 5.5 V. |
SDO | Serial data output. |
SDIN | Serial data input. |
SCLK | Serial clock input. |
Level-triggered control input (active low). This is the frame synchronization signal for the input data. | |
DGND | Ground reference for digital circuitry. |
VREFN | Negative reference voltage input. Connect a voltage in the range of VSS + 2.5 V to 0 V. |
VSS | Negative analog supply connection. Connect a voltage in the range of -16.5 V to -2.5 V. VSS must be decoupled to AGND. |
AGND | Ground reference for analog circuitry. |
RFB | Feedback connection for external amplifier. |
INV | Inverting input connection for external amplifier. |
Table 2. Hardware Control Pins Truth Table
/LDAC | /CLR | /RESET | Function |
---|---|---|---|
X1 | X1 | 0 | DAC in reset mode. The device cannot be programmed. |
X1 | X1 | ⇑2 | DAC is turned to its power-on state. All registers are set to their default values. |
0 | 0 | 1 | DAC register loaded with the clearcode register value and output set accordingly. |
0 | 1 | 1 | Output set according to the DAC register value. |
1 | 0 | 1 | DAC register loaded with the clearcode register value and output set accordingly. |
⇓3 | 1 | 1 | Output set according to the DAC register value. |
⇓3 | 0 | 1 | Output remains at the clearcode register value. |
⇑2 | 1 | 1 | Output remains set according to the DAC register value. |
⇑2 | 0 | 1 | Output remains at the clearcode register value. |
1 | ⇓3 | 1 | DAC register loaded with the clearcode register value and output set accordingly. |
0 | ⇓3 | 1 | DAC register loaded with the clearcode register value and output set accordingly. |
1 | ⇑2 | 1 | Output remains at the clearcode register value. |
0 | ⇑2 | 1 | Output set according to the DAC register value. |
1 X is don't care.
2 ⇑ is rising edge.
3 ⇓ is falling edge.
Table 3. Register Address Definitions
Read/Write | Register Address | |||
---|---|---|---|---|
R/W | C2 | C1 | C0 | Description |
X1 | 0 | 0 | 0 | No operation |
0 | 0 | 0 | 1 | Write to the DAC register |
0 | 0 | 1 | 0 | Write to the control register |
0 | 0 | 1 | 1 | Write to the clearcode register |
0 | 1 | 0 | 0 | Write to the software control register |
1 | 0 | 0 | 1 | Read from the DAC register |
1 | 0 | 1 | 0 | Read from the control register |
1 | 0 | 1 | 1 | Read from the clearcode register |
1 X = don't care.
Table 4. Control Register Functions
Bit Name | Description | |
---|---|---|
RBUF | Output amplifier configuration control. | |
Setting | Function | |
0 | Internal amplifier powered up. | |
1 (default) | Internal amplifier powered down. | |
OPGND | Output ground clamp control. | |
Setting | Function | |
0 | DAC output clamp to ground removed and DAC placed in normal mode. | |
1 (default) | DAC output clamped to ground and DAC placed in tristate mode. | |
DACTRI | DAC tristate control. | |
Setting | Function | |
0 | DAC in normal operating mode. | |
1 (default) | DAC in tristate mode. | |
BIN/2sC | DAC register coding selection. | |
Setting | Function | |
0 (default) | AC register uses twos complement coding. | |
1 | DAC register uses offset binary coding. | |
SDODIS | SDO pin enable/disable control. | |
Setting | Function | |
0 (default) | SDO pin enabled. | |
1 | SDO pin disabled (tristate). | |
R/ | Read/write select bit. | |
Setting | Function | |
0 | AD5760/AD5780/AD5790 addressed for a write operation. | |
1 | AD5760/AD5780/AD5790 addressed for a read operation. |
Table 5. Software Control Register Functions
Bit Name | Description |
---|---|
LDAC1 | Setting this bit to 1 updates the DAC register and consequently the DAC output. |
CLR2 | Setting this bit to 1 sets the DAC register to a user defined value and updates the DAC output. |
RESET | Setting this bit to 1 returns the AD5760/AD5780/AD5790 device to its power-on state. |
1 The LDAC function has no effect when the pin is low. Refer to Table 2 in the Hardware Control Pins Truth Table section for further details.
2 The CLR function has no effect when the pin is low. Refer to Table 2 in the Hardware Control Pins Truth Table section for further detail.
where:
VREFN is the negative voltage applied at the VREFN input pin.
VREFP is the positive voltage applied at the VREFP input pin.
D is the decimal equivalent.
N is the number of bits.
To initialize the part,
Write the following over the serial interface: 0010 0000 0000 0000 0001 0010 (Read/Write bit, three register address bits, 20 data bits).
To write in binary coding select BIN/2sC = “1”.
The default coding is the offset binary, the same 24-bit data will impact in a different way depending on the coding selected. The user will need to ensure the coding used by writing to the control register or reading back from it.
Figure 6. Initializing the part
To write a midscale code to the DAC register, select the write option from the read/write bit (R/W = “0”), the correspondent register address (C2C1C0 = “001”) and the data bits for a midscale code.
The 24-bit data to write over the serial interface is:
16-bit AD5760: 0001 1000 0000 0000 0000 XXXX
18-bit AD5780: 0001 1000 0000 0000 0000 00XX
20-bit AD5790: 0001 1000 0000 0000 0000 0000
Figure 7. Write to the DAC Register)
To define the value at which the DAC output is set when the CLR pin or CLR bit in the software control register is asserted, write the desired code to the clearcode register.
For a full scale clear code, write the following over the serial interface:
16-bit AD5760: 0011 1111 1111 1111 1111 XXXX
18-bit AD5780: 0011 1111 1111 1111 1111 11XX
20-bit AD5790: 0011 1111 1111 1111 1111 1111
Figure 8. Write Full Scale code to the Clearcode Register
To set the DAC register to a user defined value and update the DAC output set the CLR bit to a logic “1”.
Write the following over the serial interface: 0100 0000 0000 0000 0000 0010
The user should see the DAC output value change to full scale code.
Figure 9. Clear the part to a user defined value
To confirm the clearcode value written to the part, read the data on the clearcode register (Full scale for this example). Write the following over the serial interface: 1011 XXXX XXXX XXXX XXXX XXXX.
Remember that this action is a read function, so the R/ bit is set to “1”.
The data bits are don't care, as the aim is to read from the part and not a write function.
Figure 10. Readback from the clearcode register